<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic perl and imagemagick in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/perl-and-imagemagick/m-p/273603#M29962</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried to install imagemagick on linux imx6 baseline.&lt;/P&gt;&lt;P&gt;So, i added x11 and perl packages. But when installing imagemagick package, there's the following error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find -lperl&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see perl-5.8.8-2 package is installed but it seems to me i should see other entries like libperl-dev ,...&lt;/P&gt;&lt;P&gt;I suppose perl package is not enough. &lt;/P&gt;&lt;P&gt;Does someone know what packages profile to use ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rgds,&lt;/P&gt;&lt;P&gt;Christophe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Dec 2013 08:18:13 GMT</pubDate>
    <dc:creator>christophe</dc:creator>
    <dc:date>2013-12-20T08:18:13Z</dc:date>
    <item>
      <title>perl and imagemagick</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/perl-and-imagemagick/m-p/273603#M29962</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried to install imagemagick on linux imx6 baseline.&lt;/P&gt;&lt;P&gt;So, i added x11 and perl packages. But when installing imagemagick package, there's the following error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find -lperl&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see perl-5.8.8-2 package is installed but it seems to me i should see other entries like libperl-dev ,...&lt;/P&gt;&lt;P&gt;I suppose perl package is not enough. &lt;/P&gt;&lt;P&gt;Does someone know what packages profile to use ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rgds,&lt;/P&gt;&lt;P&gt;Christophe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Dec 2013 08:18:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/perl-and-imagemagick/m-p/273603#M29962</guid>
      <dc:creator>christophe</dc:creator>
      <dc:date>2013-12-20T08:18:13Z</dc:date>
    </item>
    <item>
      <title>Re: perl and imagemagick</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/perl-and-imagemagick/m-p/273604#M29963</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the -dev package is usually for headers files, needed for development. Is libperl.so somewhere on your filesystem? if yes, you may use the -L to indicate the folder where it resides.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Dec 2013 15:10:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/perl-and-imagemagick/m-p/273604#M29963</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-12-20T15:10:37Z</dc:date>
    </item>
    <item>
      <title>Re: perl and imagemagick</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/perl-and-imagemagick/m-p/273605#M29964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In ltib/rootfs/usr/lib, i've a perl5 directory with many directories and .pm files. But i can't locate libperl.so wheter in perl5 or another lib directory.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Dec 2013 15:54:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/perl-and-imagemagick/m-p/273605#M29964</guid>
      <dc:creator>christophe</dc:creator>
      <dc:date>2013-12-20T15:54:34Z</dc:date>
    </item>
    <item>
      <title>Re: perl and imagemagick</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/perl-and-imagemagick/m-p/273606#M29965</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Chris&lt;/P&gt;&lt;P&gt;Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Feb 2014 06:45:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/perl-and-imagemagick/m-p/273606#M29965</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-21T06:45:54Z</dc:date>
    </item>
    <item>
      <title>Re: perl and imagemagick</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/perl-and-imagemagick/m-p/273607#M29966</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Chris&lt;/P&gt;&lt;P&gt;This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Feb 2014 07:19:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/perl-and-imagemagick/m-p/273607#M29966</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-28T07:19:56Z</dc:date>
    </item>
  </channel>
</rss>