<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6 CSI -&amp;gt; VDIC path in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-CSI-gt-VDIC-path/m-p/273244#M29829</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The VDI_SRC_SEL should be set as 01b (CSI direct(cb7)).&lt;/P&gt;&lt;P&gt;The CSI0_DATA_DEST should be set as CSI0_DATA_DEST[2] - destination is IDMAC via SMFC.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Dec 2013 09:35:43 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2013-12-24T09:35:43Z</dc:date>
    <item>
      <title>i.MX6 CSI -&gt; VDIC path</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-CSI-gt-VDIC-path/m-p/273242#M29827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We want to use de-interlacing for the image from CSI as attached path.&lt;/P&gt;&lt;P&gt;Then, we think we have to set VDI_SRC_SEL field to 01b (CSI direct(cb7)) in chapter 37.5.34 in IMX6DQRM (Rev.1) for using the attached path, isn't it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other hand, there is no setting to set CSI destination = VDIC in CSI0_DATA_DEST field in chapter 37.5.152.&lt;/P&gt;&lt;P&gt;What value should we set to CSI0_DATA_DEST in this case?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And if more setting is needed to use the attached de-interlacing path, could you let us know also?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Dec 2013 08:09:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-CSI-gt-VDIC-path/m-p/273242#M29827</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2013-12-20T08:09:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 CSI -&gt; VDIC path</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-CSI-gt-VDIC-path/m-p/273243#M29828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Anybody can reply?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact, our dead line is close, so I appreciate if you give me a reply soon.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Dec 2013 08:18:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-CSI-gt-VDIC-path/m-p/273243#M29828</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2013-12-24T08:18:16Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 CSI -&gt; VDIC path</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-CSI-gt-VDIC-path/m-p/273244#M29829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The VDI_SRC_SEL should be set as 01b (CSI direct(cb7)).&lt;/P&gt;&lt;P&gt;The CSI0_DATA_DEST should be set as CSI0_DATA_DEST[2] - destination is IDMAC via SMFC.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Dec 2013 09:35:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-CSI-gt-VDIC-path/m-p/273244#M29829</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-12-24T09:35:43Z</dc:date>
    </item>
  </channel>
</rss>