<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Unknown Monitor in Ubuntu FS</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Unknown-Monitor-in-Ubuntu-FS/m-p/273190#M29796</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a custom i.MX6Q device which is using the L3.0.35_1.1.0_oneiric file system. When I select the "Displays..." option on the Ubuntu menu, the display is marked as unknown. I ahve searched the web for a solution with no luck so far. Anybody know the answer? Do I need to edit the xorg.conf file? My monitor is 1280x720 HDMI.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Apr 2013 22:34:33 GMT</pubDate>
    <dc:creator>PaulDeMetrotion</dc:creator>
    <dc:date>2013-04-17T22:34:33Z</dc:date>
    <item>
      <title>Unknown Monitor in Ubuntu FS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unknown-Monitor-in-Ubuntu-FS/m-p/273190#M29796</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a custom i.MX6Q device which is using the L3.0.35_1.1.0_oneiric file system. When I select the "Displays..." option on the Ubuntu menu, the display is marked as unknown. I ahve searched the web for a solution with no luck so far. Anybody know the answer? Do I need to edit the xorg.conf file? My monitor is 1280x720 HDMI.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2013 22:34:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unknown-Monitor-in-Ubuntu-FS/m-p/273190#M29796</guid>
      <dc:creator>PaulDeMetrotion</dc:creator>
      <dc:date>2013-04-17T22:34:33Z</dc:date>
    </item>
    <item>
      <title>Re: Unknown Monitor in Ubuntu FS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unknown-Monitor-in-Ubuntu-FS/m-p/273191#M29797</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think you can try this:&lt;/P&gt;&lt;P&gt;&lt;A href="http://anhe51.wordpress.com/2012/01/30/change-resolution-of-unknown-monitor-in-ubuntu-11-10/"&gt;http://anhe51.wordpress.com/2012/01/30/change-resolution-of-unknown-monitor-in-ubuntu-11-10/&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Apr 2013 05:45:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unknown-Monitor-in-Ubuntu-FS/m-p/273191#M29797</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2013-04-23T05:45:42Z</dc:date>
    </item>
    <item>
      <title>Re: Unknown Monitor in Ubuntu FS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unknown-Monitor-in-Ubuntu-FS/m-p/273192#M29798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried this suggestion and it did add additional resolution choices in the setup screen. But the monitor is still identified as "Unknown". I am using a Samsung SyncMaster HDMI monitor and have verified that EDID information is being sent from the device. Any idea why Ubuntu still has no idea what the monitor is???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 May 2013 18:08:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unknown-Monitor-in-Ubuntu-FS/m-p/273192#M29798</guid>
      <dc:creator>PaulDeMetrotion</dc:creator>
      <dc:date>2013-05-02T18:08:28Z</dc:date>
    </item>
  </channel>
</rss>