<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How to disable screensaver</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-disable-screensaver/m-p/273047#M29747</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your reply, this did not stop the screensaver from turning on it seems to 'wake up' the display if the screensaver has come on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It led me onto finding this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;echo -e '\033[9;0]' &amp;gt; /dev/tty1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used this in a start up script and it seems to work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Oct 2013 10:40:09 GMT</pubDate>
    <dc:creator>contra</dc:creator>
    <dc:date>2013-10-11T10:40:09Z</dc:date>
    <item>
      <title>How to disable screensaver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-disable-screensaver/m-p/273045#M29745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the IMX28 build from LTIB to play video on the LCD. After approximately 10 minutes the screen goes blank but I can see through the console output that the video is still running. I believe that a screensaver is turning the display off. Is there a way to disable this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Oct 2013 07:58:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-disable-screensaver/m-p/273045#M29745</guid>
      <dc:creator>contra</dc:creator>
      <dc:date>2013-10-10T07:58:12Z</dc:date>
    </item>
    <item>
      <title>Re: How to disable screensaver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-disable-screensaver/m-p/273046#M29746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try the following :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;echo 0 &amp;gt; /sys/class/graphics/fb0/blank&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;frame buffer number (0 in the example) may differ. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Oct 2013 09:14:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-disable-screensaver/m-p/273046#M29746</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-10-10T09:14:50Z</dc:date>
    </item>
    <item>
      <title>Re: How to disable screensaver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-disable-screensaver/m-p/273047#M29747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your reply, this did not stop the screensaver from turning on it seems to 'wake up' the display if the screensaver has come on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It led me onto finding this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;echo -e '\033[9;0]' &amp;gt; /dev/tty1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used this in a start up script and it seems to work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Oct 2013 10:40:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-disable-screensaver/m-p/273047#M29747</guid>
      <dc:creator>contra</dc:creator>
      <dc:date>2013-10-11T10:40:09Z</dc:date>
    </item>
  </channel>
</rss>