<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RTC clock forward in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RTC-clock-forward/m-p/272720#M29718</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am running imx28 processor on Technologic System's TS-7400-V2 hardware. Have linux kernel 2.6.35.3 on it. I have about 14sec of drift per day in the system time. But the RTC more or less remains accurate over a day if I am not syncing my RTC from system time or vice versa. In other words if I leave them running independently, the system time moves forward. But the RTC doesn't. Wondering if you are doing a sync from system to RTC as a cron job of some sort.&lt;/P&gt;&lt;P&gt;Another funny thing to notice, if I run ntpdate back to back, it keeps making adjustments in the order of 0.6-1sec every time I run it. Seems like I can never have an accuracy of &amp;lt; 0.5s in system time. Does not make sense. This could only mean the ntp client is not properly working on this system. On a different linux base hardware the ntpdate works just fine, and makes adjustments in the order of 0.03-0.05seconds in six hours interval, which is normal.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Mar 2015 20:48:22 GMT</pubDate>
    <dc:creator>siddiquis</dc:creator>
    <dc:date>2015-03-19T20:48:22Z</dc:date>
    <item>
      <title>RTC clock forward</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-clock-forward/m-p/272715#M29713</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a problem related to the RTC imx28.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When connecting a source in VBAT we have a consumption of 18mA when the power is off (operating system off), after that just this battery keeps the RTC board with this consumption.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After some time off and keeping VBAT powered by this source (4.2 V), we connect the equipment back to normal font and see the clock forward than it should be.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using the Yocto denzil to compile linux for the product, the default settings of kernel already linked items pertaining to RTC.&lt;/P&gt;&lt;P&gt;The kernel is the linux-imx-2.6.35.3-r24.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have you seen any behavior like this?&lt;/P&gt;&lt;P&gt;Does it still lacks enable or configure anything on linux?&lt;/P&gt;&lt;P&gt;I am sending also. Config kernel.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now appreciate the help.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336531"&gt;config.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jul 2013 11:22:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-clock-forward/m-p/272715#M29713</guid>
      <dc:creator>munoz0raul</dc:creator>
      <dc:date>2013-07-15T11:22:14Z</dc:date>
    </item>
    <item>
      <title>Re: RTC clock forward</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-clock-forward/m-p/272716#M29714</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have also seen an issue with both the Linux system time and the RTC running fast.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On an EVK running a Yocto build with Linux 2.6.35 kernel, with both system clock and RTC running off 24 MHz crystal, we've seen both clocks drift forwards by about 12 s per day. That's about 140 ppm error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On our own hardware with a Linux 2.6.35 kernel (Timesys build, not Yocto), with system clock from 24 MHz crystal and RTC from 32.768 kHz crystal, the system clock drifts forward by about 12 s per day, while the hardware clock drifts forwards by about 14 s per day. That's about 140 and 160 ppm error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please see the attached logs and graphs. The logs were obtained by the attached script &lt;STRONG&gt;time.sh&lt;/STRONG&gt; that obtained PC time from a Linux PC from the &lt;A class="external-link" href="https://en.wikipedia.org/wiki/Daytime_Protocol" rel="nofollow"&gt;Daytime Protocol server&lt;/A&gt; on port 13. The graphs were obtained with the attached Python program.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jul 2014 03:42:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-clock-forward/m-p/272716#M29714</guid>
      <dc:creator>CraigMcQueen</dc:creator>
      <dc:date>2014-07-09T03:42:44Z</dc:date>
    </item>
    <item>
      <title>Re: Re: RTC clock forward</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-clock-forward/m-p/272717#M29715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have further results obtained when the EVK is configured to use the 32.768 kHz crystal for its RTC. I've improved my time logging method to decrease the granularity from 1 s to a smaller value. See the attached graph. It's showing a clock drift of about 66 s per day (about 760 ppm) for the RTC running on the 32.768 kHz crystal. It's showing a clock drift of about 11 s (about 125 ppm) for the system clock running on the 24 MHz crystal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These drift rates seem well out of the spec for the crystals. What might be causing these high drift rates?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jul 2014 07:25:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-clock-forward/m-p/272717#M29715</guid>
      <dc:creator>CraigMcQueen</dc:creator>
      <dc:date>2014-07-10T07:25:07Z</dc:date>
    </item>
    <item>
      <title>Re: RTC clock forward</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-clock-forward/m-p/272718#M29716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are discussing internally this issue, we will respond as soon as we have an answer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jul 2014 19:42:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-clock-forward/m-p/272718#M29716</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2014-07-15T19:42:19Z</dc:date>
    </item>
    <item>
      <title>Re: RTC clock forward</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-clock-forward/m-p/272719#M29717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The load capacitors for 32k crystal have not been optimized on EVK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The load capacitance of the crystal on EVK is 12.5pF. Ideally, we need to use 15pF load capacitors if we assume a stray capacitance of 5pF. Since we are using 10pF capacitors on EVK, the crystal would be running slightly faster than the nominal frequency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On customer's design, they should use load capacitors that matches the crystal they are using.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jul 2014 15:33:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-clock-forward/m-p/272719#M29717</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2014-07-30T15:33:19Z</dc:date>
    </item>
    <item>
      <title>Re: RTC clock forward</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-clock-forward/m-p/272720#M29718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am running imx28 processor on Technologic System's TS-7400-V2 hardware. Have linux kernel 2.6.35.3 on it. I have about 14sec of drift per day in the system time. But the RTC more or less remains accurate over a day if I am not syncing my RTC from system time or vice versa. In other words if I leave them running independently, the system time moves forward. But the RTC doesn't. Wondering if you are doing a sync from system to RTC as a cron job of some sort.&lt;/P&gt;&lt;P&gt;Another funny thing to notice, if I run ntpdate back to back, it keeps making adjustments in the order of 0.6-1sec every time I run it. Seems like I can never have an accuracy of &amp;lt; 0.5s in system time. Does not make sense. This could only mean the ntp client is not properly working on this system. On a different linux base hardware the ntpdate works just fine, and makes adjustments in the order of 0.03-0.05seconds in six hours interval, which is normal.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2015 20:48:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-clock-forward/m-p/272720#M29718</guid>
      <dc:creator>siddiquis</dc:creator>
      <dc:date>2015-03-19T20:48:22Z</dc:date>
    </item>
  </channel>
</rss>