<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 2nd Ethernet using i.MX6? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/2nd-Ethernet-using-i-MX6/m-p/272467#M29620</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to implement a 2nd ethernet port along with 10/100 Mbps feature (rgmii) on my design based on i.MX6 processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I thought I could use one of the integrated USB Host Controllers for this purpose. I do not want to use USB Host1 Core since&lt;/P&gt;&lt;P&gt;I already have USB ports on my design using this core. Host2 and Host3 cores seemed perfect for me since they directly have HSIC interface.&lt;/P&gt;&lt;P&gt;And with a HSIC-to-Ethernet converter like LAN9730, it would be easy. But then I realized that USB Host2 and Host3 signals (data and strobe)&lt;/P&gt;&lt;P&gt;share the same pads with RGMII_TXC, RGMII_TX_CTL, RGMII_RXC and RGMII_RX_CTL signals which are used in RGMII interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I still somehow implement a 2nd ethernet port with the above method? Or maybe are there any other methods you can suggest to implement&lt;/P&gt;&lt;P&gt;a 2nd ethernet port?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Mar 2014 16:05:43 GMT</pubDate>
    <dc:creator>durmus</dc:creator>
    <dc:date>2014-03-03T16:05:43Z</dc:date>
    <item>
      <title>2nd Ethernet using i.MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/2nd-Ethernet-using-i-MX6/m-p/272467#M29620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to implement a 2nd ethernet port along with 10/100 Mbps feature (rgmii) on my design based on i.MX6 processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I thought I could use one of the integrated USB Host Controllers for this purpose. I do not want to use USB Host1 Core since&lt;/P&gt;&lt;P&gt;I already have USB ports on my design using this core. Host2 and Host3 cores seemed perfect for me since they directly have HSIC interface.&lt;/P&gt;&lt;P&gt;And with a HSIC-to-Ethernet converter like LAN9730, it would be easy. But then I realized that USB Host2 and Host3 signals (data and strobe)&lt;/P&gt;&lt;P&gt;share the same pads with RGMII_TXC, RGMII_TX_CTL, RGMII_RXC and RGMII_RX_CTL signals which are used in RGMII interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I still somehow implement a 2nd ethernet port with the above method? Or maybe are there any other methods you can suggest to implement&lt;/P&gt;&lt;P&gt;a 2nd ethernet port?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Mar 2014 16:05:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/2nd-Ethernet-using-i-MX6/m-p/272467#M29620</guid>
      <dc:creator>durmus</dc:creator>
      <dc:date>2014-03-03T16:05:43Z</dc:date>
    </item>
    <item>
      <title>Re: 2nd Ethernet using i.MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/2nd-Ethernet-using-i-MX6/m-p/272468#M29621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately it is as you mentioned: The PADS for the ENET module and HSIC are shared and thus you cannot use both the Ethernet Module and the HSIC module simultaneously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would suggest using one of the available uSDHC interfaces or even a regular USB interface to add a second Ethernet module.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Mar 2014 21:35:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/2nd-Ethernet-using-i-MX6/m-p/272468#M29621</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2014-03-14T21:35:09Z</dc:date>
    </item>
  </channel>
</rss>