<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Get the linux kernel headers in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Get-the-linux-kernel-headers/m-p/272258#M29591</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you did some changes on your kernel? If yes, build the whole system (./ltib) and flash the rootfs again. The problem is that one you have a rootfs (with certain modules on it) and&amp;nbsp; later you update the kernel (and boot with it), you can see the directory name mismatch as the one you are seen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hack: If you did not do any change on the module area, you can do a just create a soft link on the modules where link's name is the uname -r one and points to the current module's folder...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Feb 2014 03:39:24 GMT</pubDate>
    <dc:creator>LeonardoSandova</dc:creator>
    <dc:date>2014-02-04T03:39:24Z</dc:date>
    <item>
      <title>Get the linux kernel headers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Get-the-linux-kernel-headers/m-p/272256#M29589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the freescale imx6 SD board and I have the LTIB ubuntu running on it. When I did a "uname&amp;nbsp; -r" , here is what I see:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.0.35-2666-gbdde708&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However under /lib/modules, I only see the headers for&amp;nbsp; 3.0.35-2508-g54750ff&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How/where do I download the kernel headers for 3.0.35-2666-gbdde708 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;tera&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Feb 2014 10:44:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Get-the-linux-kernel-headers/m-p/272256#M29589</guid>
      <dc:creator>terateller</dc:creator>
      <dc:date>2014-02-03T10:44:03Z</dc:date>
    </item>
    <item>
      <title>Re: Get the linux kernel headers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Get-the-linux-kernel-headers/m-p/272257#M29590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;3.0.35 is a Linux version, 2666 - local changes and gbdde708 - git hash.&lt;/P&gt;&lt;P&gt;I think you get similar version after compiling Linux from LTIB, but major only Linux version, local changes and git revision may be difference.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Feb 2014 17:42:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Get-the-linux-kernel-headers/m-p/272257#M29590</guid>
      <dc:creator>BrilliantovKiri</dc:creator>
      <dc:date>2014-02-03T17:42:15Z</dc:date>
    </item>
    <item>
      <title>Re: Get the linux kernel headers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Get-the-linux-kernel-headers/m-p/272258#M29591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you did some changes on your kernel? If yes, build the whole system (./ltib) and flash the rootfs again. The problem is that one you have a rootfs (with certain modules on it) and&amp;nbsp; later you update the kernel (and boot with it), you can see the directory name mismatch as the one you are seen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hack: If you did not do any change on the module area, you can do a just create a soft link on the modules where link's name is the uname -r one and points to the current module's folder...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Feb 2014 03:39:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Get-the-linux-kernel-headers/m-p/272258#M29591</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2014-02-04T03:39:24Z</dc:date>
    </item>
    <item>
      <title>Re: Get the linux kernel headers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Get-the-linux-kernel-headers/m-p/272259#M29592</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;so should I get headers for 3.0.35 via the apt-get command? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Feb 2014 13:21:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Get-the-linux-kernel-headers/m-p/272259#M29592</guid>
      <dc:creator>terateller</dc:creator>
      <dc:date>2014-02-05T13:21:46Z</dc:date>
    </item>
    <item>
      <title>Re: Get the linux kernel headers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Get-the-linux-kernel-headers/m-p/272260#M29593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I wanted to compile an application. It asked for the kernel headers. Also I was searching for "tcrypt.c" crypto test program which happens to be under /crypto/ folder in my main LTIB kernel sources. However I don't find it in the booted IMX board with this kernel. I wanted to run this test program so wondered about compiling the kernel with sources&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Feb 2014 13:25:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Get-the-linux-kernel-headers/m-p/272260#M29593</guid>
      <dc:creator>terateller</dc:creator>
      <dc:date>2014-02-05T13:25:18Z</dc:date>
    </item>
  </channel>
</rss>