<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX6q SPDIF Tx driver</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6q-SPDIF-Tx-driver/m-p/272177#M29557</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My hardware uses IMX6Q.&lt;/P&gt;&lt;P&gt;My source code is based on L3.0.35_12.09.01.01.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Jun 2013 03:44:04 GMT</pubDate>
    <dc:creator>johnturnur</dc:creator>
    <dc:date>2013-06-13T03:44:04Z</dc:date>
    <item>
      <title>IMX6q SPDIF Tx driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6q-SPDIF-Tx-driver/m-p/272173#M29553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In our custom board audio is routed through SPDIF interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am getting some signals on SPDIF port but no audio is heard.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions?&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SPDIF Register values are as&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;STCSCH: 0x304000&lt;/P&gt;&lt;P&gt;STCSCL: 0x000000&lt;/P&gt;&lt;P&gt;SCR: 0x00030417&lt;/P&gt;&lt;P&gt;SIE: 0x00040000&lt;/P&gt;&lt;P&gt;STC: 0x00000196&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;-John&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jun 2013 06:32:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6q-SPDIF-Tx-driver/m-p/272173#M29553</guid>
      <dc:creator>johnturnur</dc:creator>
      <dc:date>2013-06-04T06:32:27Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6q SPDIF Tx driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6q-SPDIF-Tx-driver/m-p/272174#M29554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi John,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SPDIF is a data stream, if you are playing and audio file on IMX6 and the sink (output) is SPDIF, you need a device that will receive SPDIF and converted it to an audible format.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We use devices similar to Transit M-Audio to generate a SPDIF stream and capture (record) in iMX6 into SPDIF Rx; in your case connect the SPDIF Tx line to an audio receiver (probably you will need a coxial to optical converter).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2013 22:53:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6q-SPDIF-Tx-driver/m-p/272174#M29554</guid>
      <dc:creator>adrian_alonso</dc:creator>
      <dc:date>2013-06-11T22:53:01Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6q SPDIF Tx driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6q-SPDIF-Tx-driver/m-p/272175#M29555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I have connected converter at output side.&lt;/P&gt;&lt;P&gt;So it should work, This setup is working with other SPDIF source.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2013 04:00:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6q-SPDIF-Tx-driver/m-p/272175#M29555</guid>
      <dc:creator>johnturnur</dc:creator>
      <dc:date>2013-06-12T04:00:49Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6q SPDIF Tx driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6q-SPDIF-Tx-driver/m-p/272176#M29556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi John,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which board are you using?&lt;/P&gt;&lt;P&gt;And are you using latest public release L3.0.35_4.0.0._130424?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2013 22:19:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6q-SPDIF-Tx-driver/m-p/272176#M29556</guid>
      <dc:creator>adrian_alonso</dc:creator>
      <dc:date>2013-06-12T22:19:59Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6q SPDIF Tx driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6q-SPDIF-Tx-driver/m-p/272177#M29557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My hardware uses IMX6Q.&lt;/P&gt;&lt;P&gt;My source code is based on L3.0.35_12.09.01.01.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2013 03:44:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6q-SPDIF-Tx-driver/m-p/272177#M29557</guid>
      <dc:creator>johnturnur</dc:creator>
      <dc:date>2013-06-13T03:44:04Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6q SPDIF Tx driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6q-SPDIF-Tx-driver/m-p/272178#M29558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi John,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately non of Freescale iMX6 boards has an SPDIF TX;&lt;/P&gt;&lt;P&gt;In some iMX6 boards HDMI uses SPDIF TX for handling audio, so interface is known to work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will suggest to try latest release as we don't typically provide support for previous releases.&lt;/P&gt;&lt;P&gt;Latest release L3.0.5_4.0.0_130424&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2013 15:56:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6q-SPDIF-Tx-driver/m-p/272178#M29558</guid>
      <dc:creator>adrian_alonso</dc:creator>
      <dc:date>2013-06-13T15:56:32Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6q SPDIF Tx driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6q-SPDIF-Tx-driver/m-p/272179#M29559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks i will try with L3.0.5_4.0.0_130424.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2013 03:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6q-SPDIF-Tx-driver/m-p/272179#M29559</guid>
      <dc:creator>johnturnur</dc:creator>
      <dc:date>2013-06-14T03:37:28Z</dc:date>
    </item>
  </channel>
</rss>