<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Problem which cannot reboot by WDT</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problem-which-cannot-reboot-by-WDT/m-p/271836#M29496</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi t_kaz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;difference between WDT and POR resets is given in Chapter&lt;/P&gt;&lt;P&gt;System Reset Controller (SRC) Reference Manual.&lt;/P&gt;&lt;P&gt;POR disables (resets) all chip completely, while WDT not.&lt;/P&gt;&lt;P&gt;For example WDT does not disable DDR controler and DDR memories,&lt;/P&gt;&lt;P&gt;so after WDT reset they are reinitialized again.&lt;/P&gt;&lt;P&gt;One can try to disable DDR controler then perform WDT reset.&lt;/P&gt;&lt;P&gt;Also one flush and disable MMU and arm core caches.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Mar 2014 23:30:40 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-03-12T23:30:40Z</dc:date>
    <item>
      <title>Problem which cannot reboot by WDT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-which-cannot-reboot-by-WDT/m-p/271835#M29495</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When WDT was enabled, software stopped(kernel console froze), but u-boot does not restart. &lt;/P&gt;&lt;P&gt;Is there something that is considered to be the cause of this?&lt;/P&gt;&lt;P&gt;and What would be a good way to performing reset like POR by software?&lt;/P&gt;&lt;P&gt;please let me know. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;warm_reset_enable="0", so I think that cold reset is performed by WDT and a new boot sequence starts. &lt;/P&gt;&lt;P&gt;However, it has problem. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;WDT reg settings&lt;/P&gt;&lt;P&gt;WDOG1_WCR:0x14 (or 0x4)&lt;/P&gt;&lt;P&gt;WDOG1_WICR:0x4 &lt;/P&gt;&lt;P&gt;WDOG1_WMCR:0x0&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Mar 2014 12:16:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-which-cannot-reboot-by-WDT/m-p/271835#M29495</guid>
      <dc:creator>t_kaz</dc:creator>
      <dc:date>2014-03-03T12:16:35Z</dc:date>
    </item>
    <item>
      <title>Re: Problem which cannot reboot by WDT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-which-cannot-reboot-by-WDT/m-p/271836#M29496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi t_kaz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;difference between WDT and POR resets is given in Chapter&lt;/P&gt;&lt;P&gt;System Reset Controller (SRC) Reference Manual.&lt;/P&gt;&lt;P&gt;POR disables (resets) all chip completely, while WDT not.&lt;/P&gt;&lt;P&gt;For example WDT does not disable DDR controler and DDR memories,&lt;/P&gt;&lt;P&gt;so after WDT reset they are reinitialized again.&lt;/P&gt;&lt;P&gt;One can try to disable DDR controler then perform WDT reset.&lt;/P&gt;&lt;P&gt;Also one flush and disable MMU and arm core caches.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Mar 2014 23:30:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-which-cannot-reboot-by-WDT/m-p/271836#M29496</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-03-12T23:30:40Z</dc:date>
    </item>
  </channel>
</rss>