<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCamera and Co</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Camera-and-Co/m-p/271505#M29419</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi There!,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this is my first Post, since I didnt find a place to introduce, I'll do a quick one here.&lt;/P&gt;&lt;P&gt;My Name is Timo and I'm a Software developer who quickjumped into the Hardware development... :smileywink:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm part of a StartUp (we didnt start up yet) - and we have a very slow Prototype on Arduino but we want to Upgrade to more "professional" Parts like Freescale. Initial Production Value is planned 10K but we hope it could be more. &lt;STRONG&gt;With these numbers, most Manufacturer are not interested in us.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Intention:&lt;/STRONG&gt; We developed something like a IP Camera with a micro on Arduino, since the Arduino is too weak to handle more then a FEW FPS we needed a solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the Journes began developing with Arduino and after a a few talks with our FAB and Arrow we came up that the Freescale Lines maybe something for us!&lt;/P&gt;&lt;P&gt;AND now we got a KWIKSTIK as suggested but the information on it is very low everything we find is related to the i.MX Family.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I'm here and I may a explain a bit of our needs and you may know a similar Project or related.&lt;/P&gt;&lt;P&gt;We would appreciate any help, somewhat!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We need to build a device which has WiFi, a Micro and Camera onboard also a WebServer should be implemented.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The Camera&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;· We dont need a Full HD Camera, even 720p is too much - VGA would do it and would be alright.&lt;/P&gt;&lt;P&gt;· Since we need to stream, it should be able to deliver 15FPS +&lt;/P&gt;&lt;P&gt;· We would love to have a ready shield or Breakout Board as solution.&lt;/P&gt;&lt;P&gt;· Camera should be then purchased that we can Plug it onto our Design Board on FAB Processing. Like C329-SPI&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Price:&lt;/STRONG&gt; &amp;lt; 30 USD / EUR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;WiFi&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;it would be sweet to have a WiFi Board for the Tower, which then can be redesigned to work in our Product&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Microphone&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently this is a fixed thing on the KWIKSTIK, if that won't work, is there a TOWER ES with a Micro?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What would be the right components for it?&lt;/P&gt;&lt;P&gt;We are not able to use something like plug and play and external Products since we want to create batch / mass product out of it.&lt;/P&gt;&lt;P&gt;ITS SO HARD TO FIND INFORMATION - but I dont want to give up :smileywink:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;THANK YOU VERY MUCH - your help is appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S. Sorry my technical EN is not that brilliant :smileywink:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Feb 2013 14:07:45 GMT</pubDate>
    <dc:creator>sleeper</dc:creator>
    <dc:date>2013-02-25T14:07:45Z</dc:date>
    <item>
      <title>Camera and Co</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Camera-and-Co/m-p/271505#M29419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi There!,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this is my first Post, since I didnt find a place to introduce, I'll do a quick one here.&lt;/P&gt;&lt;P&gt;My Name is Timo and I'm a Software developer who quickjumped into the Hardware development... :smileywink:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm part of a StartUp (we didnt start up yet) - and we have a very slow Prototype on Arduino but we want to Upgrade to more "professional" Parts like Freescale. Initial Production Value is planned 10K but we hope it could be more. &lt;STRONG&gt;With these numbers, most Manufacturer are not interested in us.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Intention:&lt;/STRONG&gt; We developed something like a IP Camera with a micro on Arduino, since the Arduino is too weak to handle more then a FEW FPS we needed a solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the Journes began developing with Arduino and after a a few talks with our FAB and Arrow we came up that the Freescale Lines maybe something for us!&lt;/P&gt;&lt;P&gt;AND now we got a KWIKSTIK as suggested but the information on it is very low everything we find is related to the i.MX Family.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I'm here and I may a explain a bit of our needs and you may know a similar Project or related.&lt;/P&gt;&lt;P&gt;We would appreciate any help, somewhat!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We need to build a device which has WiFi, a Micro and Camera onboard also a WebServer should be implemented.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The Camera&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;· We dont need a Full HD Camera, even 720p is too much - VGA would do it and would be alright.&lt;/P&gt;&lt;P&gt;· Since we need to stream, it should be able to deliver 15FPS +&lt;/P&gt;&lt;P&gt;· We would love to have a ready shield or Breakout Board as solution.&lt;/P&gt;&lt;P&gt;· Camera should be then purchased that we can Plug it onto our Design Board on FAB Processing. Like C329-SPI&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Price:&lt;/STRONG&gt; &amp;lt; 30 USD / EUR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;WiFi&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;it would be sweet to have a WiFi Board for the Tower, which then can be redesigned to work in our Product&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Microphone&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently this is a fixed thing on the KWIKSTIK, if that won't work, is there a TOWER ES with a Micro?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What would be the right components for it?&lt;/P&gt;&lt;P&gt;We are not able to use something like plug and play and external Products since we want to create batch / mass product out of it.&lt;/P&gt;&lt;P&gt;ITS SO HARD TO FIND INFORMATION - but I dont want to give up :smileywink:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;THANK YOU VERY MUCH - your help is appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Timo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S. Sorry my technical EN is not that brilliant :smileywink:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Feb 2013 14:07:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Camera-and-Co/m-p/271505#M29419</guid>
      <dc:creator>sleeper</dc:creator>
      <dc:date>2013-02-25T14:07:45Z</dc:date>
    </item>
  </channel>
</rss>