<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: USB on START-R Board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-on-START-R-Board/m-p/159282#M2927</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fillipo,&lt;/P&gt;&lt;P&gt;I am facing a similar problem with Freescale iMX21 eval board. I am trying to boot with linux kernel 3.2 we observed that USB-HCD and storage driver is registered properly. However USB UDC driver is not properly initializaed. During platform specific code initialization, during probe, UDC&amp;nbsp;driver returns ENODEV. Due to no device is detected in the system. The same is the case with rtc driver.&lt;/P&gt;&lt;P&gt;Could you please help me out.&lt;/P&gt;&lt;P&gt;&amp;nbsp;boot logs attached:&lt;/P&gt;&lt;P&gt;cs89x0:cs89x0_probe(0x0)&lt;BR /&gt;cs89x0.c: v2.4.3-pre1 Russell Nelson &amp;lt;&lt;A href="mailto:nelson@crynwr.com"&gt;nelson@crynwr.com&lt;/A&gt;&amp;gt;, Andrew Morton&lt;BR /&gt;eth0: cs8900 rev K found at 0xf5000000 [Cirrus EEPROM]&lt;BR /&gt;cs89x0 media RJ-45, IRQ 203, programmed I/O, MAC 00:04:9f:00:5c:07&lt;BR /&gt;cs89x0_probe1() successful&lt;BR /&gt;cs89x0:cs89x0_probe(0x0)&lt;BR /&gt;cs89x0: request_region(0xf5000000, 0x10) failed&lt;BR /&gt;cs89x0: no cs8900 or cs8920 detected.&amp;nbsp; Be sure to disable PnP with SETUP&lt;BR /&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;BR /&gt;IMX21 USB Host Controller&lt;BR /&gt;*** imx21_probe: res_start = 0xc192a0e4, res-&amp;gt;start&lt;BR /&gt;imx21-hcd imx21-hcd.0: Hardware HC revision: 0x20&lt;BR /&gt;imx21-hcd imx21-hcd.0: IMX21 USB Host Controller&lt;BR /&gt;imx21-hcd imx21-hcd.0: new USB bus registered, assigned bus number 1&lt;BR /&gt;imx21-hcd imx21-hcd.0: irq 55, io base 0x10024000&lt;BR /&gt;hub 1-0:1.0: USB hub found&lt;BR /&gt;hub 1-0:1.0: 3 ports detected&lt;BR /&gt;Initializing USB Mass Storage driver...&lt;BR /&gt;usbcore: registered new interface driver usb-storage&lt;BR /&gt;USB Mass Storage support registered.&lt;BR /&gt;Satyajeeeeeeeet: enterred in udc_init&lt;BR /&gt;imx_udc: Return value is 0&lt;BR /&gt;imx_udc: Return value is -19&lt;BR /&gt;mxc_rtc: Return value is 0&lt;BR /&gt;mxc_rtc: Return value is -19&lt;BR /&gt;i2c /dev entries driver&lt;BR /&gt;Software Watchdog Timer: 0.07 initialized. soft_noboot=0 soft_margin=60 sec soft_panic=0 (nowayout= 0)&lt;BR /&gt;TCP cubic registered&lt;BR /&gt;drivers/rtc/hctosys.c: unable to open rtc device (rtc0)&lt;BR /&gt;imx21-hcd imx21-hcd.0: Hub status changed&lt;BR /&gt;usb 1-2: new full speed USB device number 2 using imx21-hcd&lt;BR /&gt;usb 1-2: device not accepting address 2, error -110&lt;BR /&gt;In udev-&amp;gt;wusb logic&lt;BR /&gt;imx21-hcd imx21-hcd.0: Hub status changed&lt;BR /&gt;usb 1-2: new full speed USB device number 3 using imx21-hcd&lt;BR /&gt;eth0: using half-duplex 10Base-T (RJ-45)&lt;BR /&gt;IP-Config: Complete:&lt;/P&gt;&lt;P&gt;&lt;CITE&gt;Filippo said:&lt;/CITE&gt;&lt;/P&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/usb-on-start-r-board?groupUrl=imx53quickstartboard&amp;amp;#4103961Comment69209"&gt;&lt;DIV&gt;&lt;DIV class="xg_user_generated"&gt;&lt;P&gt;SOLVED&lt;/P&gt;&lt;P&gt;After removing the OTG stuff from the kernel .config, everything is ok, and the serial port too. I guess my problems on the serial port were from the board, after a powerup they are gone, and I'm pretty sure there are no relationship with OTG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Aug 2012 11:31:45 GMT</pubDate>
    <dc:creator>Satya1z</dc:creator>
    <dc:date>2012-08-02T11:31:45Z</dc:date>
    <item>
      <title>USB on START-R Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-on-START-R-Board/m-p/159278#M2923</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm currently using ltib with the patch linux-2.6.35.3-imx_11.09.01_201112 applied, as per MX53_LINUX_BSP_201112_Patch_release.pdf document. Maybe I'm doing something really wrong, but I can't have usb running, and dmesg tells me:&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.765806] Warning: unable to open an initial console.&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.766228] RAMDISK: ext2 filesystem found at block 0&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.766291] RAMDISK: Loading 5703KiB [1 disk] into ram disk... \&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.873475] mmc0: new high speed SD card at address 0007&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.874120] mmcblk0: mmc0:0007 SD01G 972 MiB &lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.874538]&amp;nbsp; mmcblk0: p1 p2&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.878777] /&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.943605] usb 1-1: device descriptor read/64, error -71&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.944282] done.&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.128608] VFS: Mounted root (ext2 filesystem) on device 1:0.&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.128885] devtmpfs: mounted&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.129006] Freeing init memory: 180K&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.263448] usb 1-1: device descriptor read/64, error -71&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.493424] usb 1-1: new low speed USB device using fsl-ehci and address 3&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.546226] eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=0:00, irq=-1)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.803314] usb 1-1: device descriptor read/64, error -71&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.223299] usb 1-1: device descriptor read/64, error -71&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.453318] usb 1-1: new low speed USB device using fsl-ehci and address 4&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.993266] usb 1-1: device not accepting address 4, error -71&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 5.113349] usb 1-1: new low speed USB device using fsl-ehci and address 5&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 5.543518] PHY: 0:00 - Link is Up - 100/Full&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 5.653288] usb 1-1: device not accepting address 5, error -71&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 5.653379] hub 1-0:1.0: unable to enumerate USB device on port 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 8.093355] ehci_fsl_bus_suspend, Host 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 8.094262] there is a device on the port&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;After that, I have the prompt but the usb keyboard is not running.&lt;BR /&gt;I'm seeing that the first usb error is printed before the initrd is loaded, too.&lt;BR /&gt; The board runs fine with the original mmc ( the one with Ubuntu factory loaded ).&lt;BR /&gt;Additionally, on the START Board ( the Dialog based one ) the same kernel runs fine, and usb is ok.&lt;/P&gt;&lt;P&gt;I have the same results using a kernel built outside ltib, with all the patches applied.&lt;BR /&gt;I'm stuck on this from yesterday, any guy has some hints, or a running .config file if this is the case?&lt;BR /&gt; Thank you in advance&lt;BR /&gt;Filippo&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 May 2012 13:38:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-on-START-R-Board/m-p/159278#M2923</guid>
      <dc:creator>Filippo</dc:creator>
      <dc:date>2012-05-04T13:38:35Z</dc:date>
    </item>
    <item>
      <title>Re: USB on START-R Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-on-START-R-Board/m-p/159279#M2924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Ubuntu 12.04 release has the same problem; see&amp;nbsp;&lt;A href="https://bugs.launchpad.net/ubuntu/+source/linux-linaro-lt-mx5/+bug/943058"&gt;https://bugs.launchpad.net/ubuntu/+source/linux-linaro-lt-mx5/+bug/943058&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do hope it gets fixed soon: my iMX53QSB is gathering dust until it does.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 May 2012 09:49:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-on-START-R-Board/m-p/159279#M2924</guid>
      <dc:creator>RobertBrown</dc:creator>
      <dc:date>2012-05-07T09:49:58Z</dc:date>
    </item>
    <item>
      <title>Re: USB on START-R Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-on-START-R-Board/m-p/159280#M2925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Somehow SOLVED&lt;/P&gt;&lt;P&gt;I've rebuilt ltib from start, I've applied all the patches and I've created a new mmc : usb runs, maybe I had some environment problems.&lt;/P&gt;&lt;P&gt;Then I've used a stock 2.6.35.3 kernel patched with all the patches from Freescale, built from a crosstool generated compiler and a buildroot created file system. Apart from some junk on the serial port until the login appears, everything runs fine too.&lt;/P&gt;&lt;P&gt;The junk appears after the dmesg line&lt;BR /&gt;mxcintuart.0: ttymxc0 at MMIO 0x53fbc000 (irq = 31) is a Freescale i.MX&lt;BR /&gt;until the prompt, but the prompt is correct.I will investigate further.&lt;/P&gt;&lt;P&gt;Anyway I still have that note that complains about USB_OTG and others, I will investigate this too.&lt;/P&gt;&lt;P&gt;So, Robert, I thank you very much for the info, is exactly what I was seeing in my wrong ltib.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 May 2012 11:13:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-on-START-R-Board/m-p/159280#M2925</guid>
      <dc:creator>Filippo</dc:creator>
      <dc:date>2012-05-07T11:13:25Z</dc:date>
    </item>
    <item>
      <title>Re: USB on START-R Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-on-START-R-Board/m-p/159281#M2926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SOLVED&lt;/P&gt;&lt;P&gt;After removing the OTG stuff from the kernel .config, everything is ok, and the serial port too. I guess my problems on the serial port were from the board, after a powerup they are gone, and I'm pretty sure there are no relationship with OTG.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 May 2012 15:38:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-on-START-R-Board/m-p/159281#M2926</guid>
      <dc:creator>Filippo</dc:creator>
      <dc:date>2012-05-07T15:38:09Z</dc:date>
    </item>
    <item>
      <title>Re: USB on START-R Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-on-START-R-Board/m-p/159282#M2927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fillipo,&lt;/P&gt;&lt;P&gt;I am facing a similar problem with Freescale iMX21 eval board. I am trying to boot with linux kernel 3.2 we observed that USB-HCD and storage driver is registered properly. However USB UDC driver is not properly initializaed. During platform specific code initialization, during probe, UDC&amp;nbsp;driver returns ENODEV. Due to no device is detected in the system. The same is the case with rtc driver.&lt;/P&gt;&lt;P&gt;Could you please help me out.&lt;/P&gt;&lt;P&gt;&amp;nbsp;boot logs attached:&lt;/P&gt;&lt;P&gt;cs89x0:cs89x0_probe(0x0)&lt;BR /&gt;cs89x0.c: v2.4.3-pre1 Russell Nelson &amp;lt;&lt;A href="mailto:nelson@crynwr.com"&gt;nelson@crynwr.com&lt;/A&gt;&amp;gt;, Andrew Morton&lt;BR /&gt;eth0: cs8900 rev K found at 0xf5000000 [Cirrus EEPROM]&lt;BR /&gt;cs89x0 media RJ-45, IRQ 203, programmed I/O, MAC 00:04:9f:00:5c:07&lt;BR /&gt;cs89x0_probe1() successful&lt;BR /&gt;cs89x0:cs89x0_probe(0x0)&lt;BR /&gt;cs89x0: request_region(0xf5000000, 0x10) failed&lt;BR /&gt;cs89x0: no cs8900 or cs8920 detected.&amp;nbsp; Be sure to disable PnP with SETUP&lt;BR /&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;BR /&gt;IMX21 USB Host Controller&lt;BR /&gt;*** imx21_probe: res_start = 0xc192a0e4, res-&amp;gt;start&lt;BR /&gt;imx21-hcd imx21-hcd.0: Hardware HC revision: 0x20&lt;BR /&gt;imx21-hcd imx21-hcd.0: IMX21 USB Host Controller&lt;BR /&gt;imx21-hcd imx21-hcd.0: new USB bus registered, assigned bus number 1&lt;BR /&gt;imx21-hcd imx21-hcd.0: irq 55, io base 0x10024000&lt;BR /&gt;hub 1-0:1.0: USB hub found&lt;BR /&gt;hub 1-0:1.0: 3 ports detected&lt;BR /&gt;Initializing USB Mass Storage driver...&lt;BR /&gt;usbcore: registered new interface driver usb-storage&lt;BR /&gt;USB Mass Storage support registered.&lt;BR /&gt;Satyajeeeeeeeet: enterred in udc_init&lt;BR /&gt;imx_udc: Return value is 0&lt;BR /&gt;imx_udc: Return value is -19&lt;BR /&gt;mxc_rtc: Return value is 0&lt;BR /&gt;mxc_rtc: Return value is -19&lt;BR /&gt;i2c /dev entries driver&lt;BR /&gt;Software Watchdog Timer: 0.07 initialized. soft_noboot=0 soft_margin=60 sec soft_panic=0 (nowayout= 0)&lt;BR /&gt;TCP cubic registered&lt;BR /&gt;drivers/rtc/hctosys.c: unable to open rtc device (rtc0)&lt;BR /&gt;imx21-hcd imx21-hcd.0: Hub status changed&lt;BR /&gt;usb 1-2: new full speed USB device number 2 using imx21-hcd&lt;BR /&gt;usb 1-2: device not accepting address 2, error -110&lt;BR /&gt;In udev-&amp;gt;wusb logic&lt;BR /&gt;imx21-hcd imx21-hcd.0: Hub status changed&lt;BR /&gt;usb 1-2: new full speed USB device number 3 using imx21-hcd&lt;BR /&gt;eth0: using half-duplex 10Base-T (RJ-45)&lt;BR /&gt;IP-Config: Complete:&lt;/P&gt;&lt;P&gt;&lt;CITE&gt;Filippo said:&lt;/CITE&gt;&lt;/P&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/usb-on-start-r-board?groupUrl=imx53quickstartboard&amp;amp;#4103961Comment69209"&gt;&lt;DIV&gt;&lt;DIV class="xg_user_generated"&gt;&lt;P&gt;SOLVED&lt;/P&gt;&lt;P&gt;After removing the OTG stuff from the kernel .config, everything is ok, and the serial port too. I guess my problems on the serial port were from the board, after a powerup they are gone, and I'm pretty sure there are no relationship with OTG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Aug 2012 11:31:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-on-START-R-Board/m-p/159282#M2927</guid>
      <dc:creator>Satya1z</dc:creator>
      <dc:date>2012-08-02T11:31:45Z</dc:date>
    </item>
  </channel>
</rss>