<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MCIMX53-START-R board can't boot up</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146804#M292</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i have not done like that,The image&lt;SPAN style="font-family: mceinline;"&gt; &lt;/SPAN&gt;that came with it&amp;nbsp; is broken,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Oct 2012 13:28:39 GMT</pubDate>
    <dc:creator>caoping</dc:creator>
    <dc:date>2012-10-24T13:28:39Z</dc:date>
    <item>
      <title>MCIMX53-START-R board can't boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146798#M286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello everyone!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; now i have two boards,they are both IMX53 quick starts board,one power chip is DA9053(1 GB DDR3/800) and the other is PC34708VM(1 GB DDR3/800 MXIMX53-START-R), when i download u-boot image using Mfgtools,the board with DA9053 power-chip works OK!but the other board with PC34708VM power-chip can't boot after the stage "Jumping to OS image" ,Mfgtools&amp;nbsp; stops, the error code is "-65534",&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; And when&amp;nbsp; i set the two boards at Serial Downloader by linking pin11 of SW1 to pin10 of SW1, when i send 0x05 0x05,they both can response,and the value is the same!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; but i still can't boot the MXIMX53-START-R after i got u-boot.bin file from my supplier,who said the boot file is latest!&amp;nbsp; Before this,i put u-boot.bin at the location that u-boot-mx53-loco.bin located,and renamed the u-boot.bin for&amp;nbsp; u-boot-mx53-loco.bin&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2012 02:05:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146798#M286</guid>
      <dc:creator>caoping</dc:creator>
      <dc:date>2012-10-23T02:05:53Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX53-START-R board can't boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146799#M287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use the &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;IMX_MFG_TOOL&lt;/A&gt; &lt;STRONG&gt;Rev #: &lt;/STRONG&gt;1.6.2.042 which is downloaded from the "Downloads" page of i.MX53QSB web page here :&lt;/P&gt;&lt;P&gt;&amp;lt; &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&lt;/A&gt; &amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried it can program the Start-R board with the micro SD card..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2012 05:58:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146799#M287</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2012-10-23T05:58:50Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX53-START-R board can't boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146800#M288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;SPAN class="j-post-author"&gt;&lt;STRONG&gt;&lt;A href="https://community.nxp.com/people/jimmychan"&gt;jimmychan&lt;/A&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;it still can't boot up, i suspect that there are some problems on the hardware,i will proceed to find the reason of that,Thank you for you share.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2012 10:25:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146800#M288</guid>
      <dc:creator>caoping</dc:creator>
      <dc:date>2012-10-24T10:25:45Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX53-START-R board can't boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146801#M289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you use uboot that came with the tool download or uboot that you had been using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2012 11:43:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146801#M289</guid>
      <dc:creator>RandyKrakora</dc:creator>
      <dc:date>2012-10-24T11:43:51Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX53-START-R board can't boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146802#M290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes,i use uboot that came with the tool download.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2012 13:14:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146802#M290</guid>
      <dc:creator>caoping</dc:creator>
      <dc:date>2012-10-24T13:14:00Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX53-START-R board can't boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146803#M291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It sounds like the mfg. kernel that is used during reprogramming is not compatible with the START-R board. Can you boot the START-R board with the Ubuntu uSD card that came with it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2012 13:20:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146803#M291</guid>
      <dc:creator>RandyKrakora</dc:creator>
      <dc:date>2012-10-24T13:20:16Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX53-START-R board can't boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146804#M292</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i have not done like that,The image&lt;SPAN style="font-family: mceinline;"&gt; &lt;/SPAN&gt;that came with it&amp;nbsp; is broken,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2012 13:28:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146804#M292</guid>
      <dc:creator>caoping</dc:creator>
      <dc:date>2012-10-24T13:28:39Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX53-START-R board can't boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146805#M293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What errors are there when you boot the board with the card that came with it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2012 15:10:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146805#M293</guid>
      <dc:creator>RandyKrakora</dc:creator>
      <dc:date>2012-10-24T15:10:37Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX53-START-R board can't boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146806#M294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;when i use the Mfgtools version 1.6.2.042,it will stop at the "Jumping to OS image" stage&lt;/P&gt;&lt;P&gt;the error information in the mfgtol.log&amp;nbsp; is :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thursday, October 25, 2012 09:02:56&lt;/P&gt;&lt;P&gt;1 - Panel A Start processing MX53LOCO-SD &amp;lt;LIST/&amp;gt;. Panel A Start &amp;lt;CMD/&amp;gt; type="boot" body="BootStrap" file="u-boot-mx53-loco.bin" timeout="10" onError="" text="Read from DDR script from U-Boot to init DDR Memory.".&lt;/P&gt;&lt;P&gt;1 - Panel A Finished &amp;lt;CMD/&amp;gt; type="boot" body="BootStrap" file="u-boot-mx53-loco.bin" timeout="10" onError="" text="Read from DDR script from U-Boot to init DDR Memory." SUCCESS code=0. Panel A Start &amp;lt;CMD/&amp;gt; type="load" body="" file="uImage" timeout="10" onError="" text="Doing Kernel.". &lt;/P&gt;&lt;P&gt;1 - Panel A Finished &amp;lt;CMD/&amp;gt; type="load" body="" file="uImage" timeout="10" onError="" text="Doing Kernel." SUCCESS code=0. Panel A Start &amp;lt;CMD/&amp;gt; type="load" body="" file="initramfs.cpio.gz.uboot" timeout="10" onError="" text="Doing Initramfs.". &lt;/P&gt;&lt;P&gt;1 - Panel A Finished &amp;lt;CMD/&amp;gt; type="load" body="" file="initramfs.cpio.gz.uboot" timeout="10" onError="" text="Doing Initramfs." SUCCESS code=0. Panel A Start &amp;lt;CMD/&amp;gt; type="jump" body="" file="" timeout="10" onError="" text=" Jumping to OS image. ". &lt;/P&gt;&lt;P&gt;1 - Panel A Finished &amp;lt;CMD/&amp;gt; type="jump" body="" file="" timeout="10" onError="" text=" Jumping to OS image. " SUCCESS code=0. Panel A Start &amp;lt;CMD/&amp;gt; type="find" body="Updater" file="" timeout="180" onError="" text="". Panel A UtpUpdate Event: DeviceRemoval Msg: (null) DevState: Disconnected OpState: WAITING_FOR_DEVICE Panel A UtpUpdate Event: DeviceArrival Msg: (null) DevState: BootStrap OpState: WAITING_FOR_DEVICE&lt;/P&gt;&lt;P&gt;1 - Panel A Finished &amp;lt;CMD/&amp;gt; type="find" body="Updater" file="" timeout="180" onError="" text="" FAIL code=-65530. Panel A: failed to run command: type="find" body="Updater" file="" timeout="180" onError="" text="" ,, Error code:-65530 2 - Panel A Finished processing MX53LOCO-SD &amp;lt;LIST/&amp;gt; : FAIL code=-65530. Panel A: &lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Oct 2012 01:22:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146806#M294</guid>
      <dc:creator>caoping</dc:creator>
      <dc:date>2012-10-25T01:22:50Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX53-START-R board can't boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146807#M295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not 100% certain on the terminology used, but in my experience "loco" refers to old QSB ( DA9053 ) and START-R refers to newer QSB - QSB-R ( &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #f8f8f8;"&gt;PC34708VM&lt;/SPAN&gt; ). The uboot file you are downloading is named with "loco" so I wonder it that file and the kernel with it are both for the older QSB and therefore will not work on newer QSB-R. I would try to find a "qsb-r" or "start-r" uboot and kernel and modify the mfg. tool scripts to use those ( or create another target ) for programming the QSB-R.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Oct 2012 16:35:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146807#M295</guid>
      <dc:creator>RandyKrakora</dc:creator>
      <dc:date>2012-10-29T16:35:20Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX53-START-R board can't boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146808#M296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you everyone! The problem has &lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN&gt;been resolved，When i change another board from my supplier,who said it worked well. All things are right! and the version that I used now is that &lt;A href="https://community.nxp.com/people/jimmychan"&gt;jimmychan&lt;/A&gt; has said. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN&gt;The&amp;nbsp; &lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;IMX_MFG_TOOL&lt;/A&gt; &lt;STRONG&gt;Rev #: &lt;/STRONG&gt;1.6.2.042&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN&gt;&amp;lt; &lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&lt;/A&gt; &amp;gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN&gt;thank you,everyone.and there exists some problem on the version I think.different board should use different version.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Oct 2012 13:59:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX53-START-R-board-can-t-boot-up/m-p/146808#M296</guid>
      <dc:creator>caoping</dc:creator>
      <dc:date>2012-10-30T13:59:05Z</dc:date>
    </item>
  </channel>
</rss>