<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MCIMX6Q4AVT10AC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX6Q4AVT10AC/m-p/270662#M29161</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why not ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Mar 2014 06:10:46 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2014-03-03T06:10:46Z</dc:date>
    <item>
      <title>MCIMX6Q4AVT10AC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX6Q4AVT10AC/m-p/270661#M29160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; text-indent: 0px; color: #222222;"&gt;(question)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; text-indent: 0px; color: #222222;"&gt;Can '1GHZ' CPU be used by '800MHZ '&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Mar 2014 05:57:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX6Q4AVT10AC/m-p/270661#M29160</guid>
      <dc:creator>hiroshitakahash</dc:creator>
      <dc:date>2014-03-03T05:57:16Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX6Q4AVT10AC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX6Q4AVT10AC/m-p/270662#M29161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why not ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Mar 2014 06:10:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX6Q4AVT10AC/m-p/270662#M29161</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-03-03T06:10:46Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX6Q4AVT10AC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX6Q4AVT10AC/m-p/270663#M29162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hiroshi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If my understanding is correct, you want to run a 1GHz i.MX6 processor at 800MHz (core frequency), right? If so, the answer is yes, you just have to configure the clocks (see reference manual chapter 18) so the resulting frequency is the one you desire. If you are using an OS like Linux, this is done automatically by configuring some settings. I'm mainly focused on HW, but a SW person can help you with this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;Jorge.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Mar 2014 19:29:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX6Q4AVT10AC/m-p/270663#M29162</guid>
      <dc:creator>JorgeRama_rezRi</dc:creator>
      <dc:date>2014-03-03T19:29:36Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX6Q4AVT10AC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX6Q4AVT10AC/m-p/270664#M29163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hiroshi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If your BSP is Android or Linux, you can add "arm_freq=800" into your bootloader parameters. Lets CPU work at special frequency (MHz).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Carl&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Mar 2014 06:06:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX6Q4AVT10AC/m-p/270664#M29163</guid>
      <dc:creator>CarlChien</dc:creator>
      <dc:date>2014-03-04T06:06:32Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX6Q4AVT10AC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX6Q4AVT10AC/m-p/270665#M29164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Adding &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;"arm_freq=800"&lt;/SPAN&gt; is only working for L3.0.35, to make it work for all kernel, I think you can change the /sys/devices/system/cpu/cpu0/cpufreq/scaling_max_freq to 792000. just "echo 792000 &amp;gt; /sys/devices/system/cpu/cpu0/cpufreq/scaling_max_freq" after linux kernel boot up. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Mar 2014 06:55:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX6Q4AVT10AC/m-p/270665#M29164</guid>
      <dc:creator>AnsonHuang</dc:creator>
      <dc:date>2014-03-04T06:55:32Z</dc:date>
    </item>
  </channel>
</rss>