<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX233 and SDIO multiplex in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX233-and-SDIO-multiplex/m-p/270532#M29128</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="text-align: left;"&gt;Would it be possible to have both an SDIO wireless device and an SDHC card on one SSP of the i.MX233, using a multiplexer like&lt;A href="http://www.ti.com/product/ts3a27518e-q1" title="http://www.ti.com/product/ts3a27518e-q1"&gt; TS3A27518E-Q1 &lt;/A&gt;or &lt;A href="http://www.maximintegrated.com/datasheet/index.mvp/id/5763" title="http://www.maximintegrated.com/datasheet/index.mvp/id/5763"&gt;MAX4996&lt;/A&gt;? Also, could you do it simply by connecting the data lines together for the two cards and having separate CMD lines for each device?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 23 Feb 2013 19:36:09 GMT</pubDate>
    <dc:creator>daveshah</dc:creator>
    <dc:date>2013-02-23T19:36:09Z</dc:date>
    <item>
      <title>i.MX233 and SDIO multiplex</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX233-and-SDIO-multiplex/m-p/270532#M29128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="text-align: left;"&gt;Would it be possible to have both an SDIO wireless device and an SDHC card on one SSP of the i.MX233, using a multiplexer like&lt;A href="http://www.ti.com/product/ts3a27518e-q1" title="http://www.ti.com/product/ts3a27518e-q1"&gt; TS3A27518E-Q1 &lt;/A&gt;or &lt;A href="http://www.maximintegrated.com/datasheet/index.mvp/id/5763" title="http://www.maximintegrated.com/datasheet/index.mvp/id/5763"&gt;MAX4996&lt;/A&gt;? Also, could you do it simply by connecting the data lines together for the two cards and having separate CMD lines for each device?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Feb 2013 19:36:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX233-and-SDIO-multiplex/m-p/270532#M29128</guid>
      <dc:creator>daveshah</dc:creator>
      <dc:date>2013-02-23T19:36:09Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX233 and SDIO multiplex</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX233-and-SDIO-multiplex/m-p/270533#M29129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Quote from "SD Specifications Part 1 Physical Layer Specification Version 2.00"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.5 Bus Topology&lt;/P&gt;&lt;P&gt;... &lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Common bus signals for multiple card slots are not recommended.&lt;/SPAN&gt; A single SD bus should&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN class="GRcorrect"&gt;connect&lt;/SPAN&gt; a single SD card.&lt;/STRONG&gt; &lt;/P&gt;&lt;P&gt;..&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jacky&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Feb 2013 07:50:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX233-and-SDIO-multiplex/m-p/270533#M29129</guid>
      <dc:creator>JackyAtFreescal</dc:creator>
      <dc:date>2013-02-26T07:50:57Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX233 and SDIO multiplex</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX233-and-SDIO-multiplex/m-p/270534#M29130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David, did Jacky's answer helps you. If yes, please mark it as Correct Answer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Mar 2013 03:22:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX233-and-SDIO-multiplex/m-p/270534#M29130</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2013-03-06T03:22:15Z</dc:date>
    </item>
  </channel>
</rss>