<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic set ethernet address on usb0 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/set-ethernet-address-on-usb0/m-p/159206#M2912</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an imx51 evk board. I have the freescale android image running on it(R.10.3).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have two DHCP networks. I have one normally connected over ethernet port of the board. The other via usb port. How do I set the MAC address in my U-boot command?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did a normal setenv ethaddr xx.xx.xx.xx.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However both the ethernet and usb0 seem to be polling their respective dhcp servers without reply.&lt;/P&gt;&lt;P&gt;Can the ethaddr overwrite the previous addresS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I get the two dhcp-based network interfaces runing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 May 2012 12:30:20 GMT</pubDate>
    <dc:creator>patrickimmling</dc:creator>
    <dc:date>2012-05-04T12:30:20Z</dc:date>
    <item>
      <title>set ethernet address on usb0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/set-ethernet-address-on-usb0/m-p/159206#M2912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an imx51 evk board. I have the freescale android image running on it(R.10.3).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have two DHCP networks. I have one normally connected over ethernet port of the board. The other via usb port. How do I set the MAC address in my U-boot command?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did a normal setenv ethaddr xx.xx.xx.xx.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However both the ethernet and usb0 seem to be polling their respective dhcp servers without reply.&lt;/P&gt;&lt;P&gt;Can the ethaddr overwrite the previous addresS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I get the two dhcp-based network interfaces runing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 May 2012 12:30:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/set-ethernet-address-on-usb0/m-p/159206#M2912</guid>
      <dc:creator>patrickimmling</dc:creator>
      <dc:date>2012-05-04T12:30:20Z</dc:date>
    </item>
  </channel>
</rss>