<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SoC selection dilemma in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SoC-selection-dilemma/m-p/159156#M2906</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I want to design a custom board, the system is going to be a prototype Smartphone with: 512MB mDDR, 2G/3G modem, WiFi+BT, 4" AMOLED, 5MP camera,...almost everything!.&amp;nbsp;Superior graphics performance, high quality image/video, low power consumption and low price are all critical.&lt;/P&gt;&lt;P&gt;I got best SoCs from TI and Qualcom, but the package is not suitable for prototyping - &amp;nbsp;will cost me more than money&lt;/P&gt;&lt;P&gt;Now, here I come, I see all the imx family (I've experience with imx23, imx27 and imx28). Finally the chice is between imx51 or imx53; only these can qualify for the competition.&lt;/P&gt;&lt;P&gt;imx53 has superior performance clearly, but how about power. I couldn't find a power benchmark. also memory interface - DDR2 suffices for my purpose, but imx53 seems to have a DDR3 F/F&lt;/P&gt;&lt;P&gt;Finally, leaving all the unused features (like FEC, CAN, HDMI, AUX display,...) would it be possible to manage to fit the PCB to 6-layers?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;-Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 26 Jun 2011 09:23:31 GMT</pubDate>
    <dc:creator>danix</dc:creator>
    <dc:date>2011-06-26T09:23:31Z</dc:date>
    <item>
      <title>SoC selection dilemma</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SoC-selection-dilemma/m-p/159156#M2906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I want to design a custom board, the system is going to be a prototype Smartphone with: 512MB mDDR, 2G/3G modem, WiFi+BT, 4" AMOLED, 5MP camera,...almost everything!.&amp;nbsp;Superior graphics performance, high quality image/video, low power consumption and low price are all critical.&lt;/P&gt;&lt;P&gt;I got best SoCs from TI and Qualcom, but the package is not suitable for prototyping - &amp;nbsp;will cost me more than money&lt;/P&gt;&lt;P&gt;Now, here I come, I see all the imx family (I've experience with imx23, imx27 and imx28). Finally the chice is between imx51 or imx53; only these can qualify for the competition.&lt;/P&gt;&lt;P&gt;imx53 has superior performance clearly, but how about power. I couldn't find a power benchmark. also memory interface - DDR2 suffices for my purpose, but imx53 seems to have a DDR3 F/F&lt;/P&gt;&lt;P&gt;Finally, leaving all the unused features (like FEC, CAN, HDMI, AUX display,...) would it be possible to manage to fit the PCB to 6-layers?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;-Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 26 Jun 2011 09:23:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SoC-selection-dilemma/m-p/159156#M2906</guid>
      <dc:creator>danix</dc:creator>
      <dc:date>2011-06-26T09:23:31Z</dc:date>
    </item>
    <item>
      <title>Re: SoC selection dilemma</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SoC-selection-dilemma/m-p/159157#M2907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i.MX53 is good for Smartphone and some big mobile phone companies are using it. You can use i.MX53 PoP + LPDDR2 to get both&amp;nbsp;small board area and low power when you design Smartphone.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Oct 2011 03:02:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SoC-selection-dilemma/m-p/159157#M2907</guid>
      <dc:creator>KarlLu</dc:creator>
      <dc:date>2011-10-27T03:02:25Z</dc:date>
    </item>
  </channel>
</rss>