<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic AUDMUX internal network mode does not work on IMX6 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/AUDMUX-internal-network-mode-does-not-work-on-IMX6/m-p/270072#M28924</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am currently working with the IMX6SLEVK attempting to capture audio from 2 CODECs (TDM mode) using a single SSI controller. I have the master and slave CODECs connected to external AUDMUX4 &amp;amp; AUDMUX5 ports. The SSI controller being used is on the AUDMUX1 port. When the AUDUMX1 port is configured to RX data using “internal network mode” and the INMMASK is set to receive data from AUD4 AND AUD5, I get no data. However, if the INMMASK is configured&amp;nbsp; to only receive AUD4 or only receive AUD5, data is received correctly. It seems that when multiple ports are selected in the INMMASK, all the data received is 0’s.&amp;nbsp;&amp;nbsp; Individually the channels look fine. How do you receive data from 2 external ports to a single SSI interface?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The clock and frame sync lines are all being routed correctly. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 Jan 2014 20:06:33 GMT</pubDate>
    <dc:creator>RobHawksFan</dc:creator>
    <dc:date>2014-01-31T20:06:33Z</dc:date>
    <item>
      <title>AUDMUX internal network mode does not work on IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AUDMUX-internal-network-mode-does-not-work-on-IMX6/m-p/270072#M28924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am currently working with the IMX6SLEVK attempting to capture audio from 2 CODECs (TDM mode) using a single SSI controller. I have the master and slave CODECs connected to external AUDMUX4 &amp;amp; AUDMUX5 ports. The SSI controller being used is on the AUDMUX1 port. When the AUDUMX1 port is configured to RX data using “internal network mode” and the INMMASK is set to receive data from AUD4 AND AUD5, I get no data. However, if the INMMASK is configured&amp;nbsp; to only receive AUD4 or only receive AUD5, data is received correctly. It seems that when multiple ports are selected in the INMMASK, all the data received is 0’s.&amp;nbsp;&amp;nbsp; Individually the channels look fine. How do you receive data from 2 external ports to a single SSI interface?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The clock and frame sync lines are all being routed correctly. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jan 2014 20:06:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AUDMUX-internal-network-mode-does-not-work-on-IMX6/m-p/270072#M28924</guid>
      <dc:creator>RobHawksFan</dc:creator>
      <dc:date>2014-01-31T20:06:33Z</dc:date>
    </item>
    <item>
      <title>Re: AUDMUX internal network mode does not work on IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AUDMUX-internal-network-mode-does-not-work-on-IMX6/m-p/270073#M28925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rob,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you check if you setup follows this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;With internal network mode, single point-to-multipoint network configuration with&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;an arbitrary number of slaves can be supported if the external slaves are put into the&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;high-impedance state (as defined in the SSI network mode protocol) and have pull-up&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;resistors on their TxD pins. (Alternatively, this can be viewed as requiring a pull-up&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;resistor on the corresponding AUDMUX RxD pin.)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Feb 2014 21:44:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AUDMUX-internal-network-mode-does-not-work-on-IMX6/m-p/270073#M28925</guid>
      <dc:creator>adrian_alonso</dc:creator>
      <dc:date>2014-02-28T21:44:43Z</dc:date>
    </item>
  </channel>
</rss>