<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Yocto - Working with the Toolchain in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270005#M28910</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried this, on your suggestion, unfortunately it led to the same result. &lt;/P&gt;&lt;P&gt;I truly appreciate your help. Do you happen to have any other possible ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 23 Feb 2013 07:56:52 GMT</pubDate>
    <dc:creator>jparrish88</dc:creator>
    <dc:date>2013-02-23T07:56:52Z</dc:date>
    <item>
      <title>Yocto - Working with the Toolchain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270002#M28907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just started using Yocto by Following &lt;A href="https://community.nxp.com/docs/DOC-93844"&gt;How to test yocto for imx6&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;Now I'd like to build another project with the build-derived toolchain or the ADT installer toolchain.&lt;/P&gt;&lt;P&gt;I'd also like to use eclipse and the Yocto plugin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the first thing I tried was the ADT, it looked like it would be the easier method.&lt;/P&gt;&lt;P&gt;I followed the steps here: &lt;A href="http://www.yoctoproject.org/docs/1.3/adt-manual/adt-manual.html#adt-intro-section" title="http://www.yoctoproject.org/docs/1.3/adt-manual/adt-manual.html#adt-intro-section"&gt;http://www.yoctoproject.org/docs/1.3/adt-manual/adt-manual.html#adt-intro-section&lt;/A&gt;&lt;A href="http://www.yoctoproject.org/docs/1.3/adt-manual/adt-manual.html#adt-intro-section" title="http://www.yoctoproject.org/docs/1.3/adt-manual/adt-manual.html#adt-intro-section"&gt;http://www.yoctoproject.org/docs/1.3/adt-manual/adt-manual.html#adt-intro-section&lt;/A&gt;&lt;A href="http://www.yoctoproject.org/docs/1.3/adt-manual/adt-manual.html#adt-intro-section"&gt;http://www.yoctoproject.org/docs/1.3/adt-manual/adt-manual.html#adt-intro-section&lt;/A&gt;&lt;/P&gt;&lt;P&gt;In doing so I typed the commands bitbake adt-installer then the log showed that it had succeeded.&lt;/P&gt;&lt;P&gt;So I found the ADT installer tarball in /build/tmp/deploy/sdk&lt;/P&gt;&lt;P&gt;Extracted that to a folder in my ~/. then I ran the adt-installer script. I didn't change the configuration.&lt;/P&gt;&lt;P&gt;That installed files to /opt/poky/1.3/.&lt;/P&gt;&lt;P&gt;From there I should have been set to use the eclipse yocto plugin.&lt;/P&gt;&lt;P&gt;In order to set up Eclipse and the Yocto plugin I followed these directions: &lt;A href="http://www.yoctoproject.org/docs/1.3/dev-manual/dev-manual.html#adt-eclipse" title="http://www.yoctoproject.org/docs/1.3/dev-manual/dev-manual.html#adt-eclipse"&gt;http://www.yoctoproject.org/docs/1.3/dev-manual/dev-manual.html#adt-eclipse&lt;/A&gt;&lt;A href="http://www.yoctoproject.org/docs/1.3/dev-manual/dev-manual.html#adt-eclipse"&gt;http://www.yoctoproject.org/docs/1.3/dev-manual/dev-manual.html#adt-eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I went with Juno and I installed the pre-built yocto plugin (I thought it would be the safest).&lt;/P&gt;&lt;P&gt;After everything was installed, and two restarts later... I went into window -&amp;gt; preferences -&amp;gt; Yocto Project ADT&lt;/P&gt;&lt;P&gt;This window let me set where my toolchain was being pulled from.&lt;/P&gt;&lt;P&gt;I entered /opt/poky/1.3/ into both the toolchain root and the sysroot.&lt;/P&gt;&lt;P&gt;In the drop down I'm suppose to select my toolchain.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38739i89CB555611FEC1A8/image-size/large?v=v2&amp;amp;px=999" title="Screenshot-Preferences-ADT.png" alt="Screenshot-Preferences-ADT.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Here is where I found out I should have changed the adt install scripts configuration.&lt;/P&gt;&lt;P&gt;It only showed that I could select either ARMv5te or i586.&lt;/P&gt;&lt;P&gt;Obviously I screwed up. But I should be able to build using this toolchain. So I started a new project as the directions state.&lt;/P&gt;&lt;P&gt;I build the project and it gives me this output:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38740iFF8C7633E3072507/image-size/large?v=v2&amp;amp;px=999" title="Screenshot-C-C++ - Eclipse-ADT.png" alt="Screenshot-C-C++ - Eclipse-ADT.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Okay so I messed up the ADT install. Turns out the configuration built for the wrong platform.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So then I tried to redirect eclipse to use my build derived toolchain.&lt;/P&gt;&lt;P&gt;So I entered in bitbake: bitbake meta-ide-support&lt;/P&gt;&lt;P&gt;It completed successfully and I saw a sysroot folder and an environment-setup file be placed in the /build/tmp directory.&lt;/P&gt;&lt;P&gt;So I go back into the eclipse and I I reconfigure it for a build derived toolchain.&lt;/P&gt;&lt;P&gt;But nothing appears in the toolchain drop down.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38803iFB9A1D46DE2D11D1/image-size/large?v=v2&amp;amp;px=999" title="Screenshot-Preferences-BD.png" alt="Screenshot-Preferences-BD.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If I try to hit ok, even though my target arch is greyed out I get this.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38805i5EAED4E227B675CA/image-size/large?v=v2&amp;amp;px=999" title="Screenshot-Yocto Project Configuration Error.png" alt="Screenshot-Yocto Project Configuration Error.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the weird part, if I select standalone pre-built I get a toolchain in the drop down.&lt;/P&gt;&lt;P&gt;However, I can't select apply or ok.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38742iD32DA3A298E46C03/image-size/large?v=v2&amp;amp;px=999" title="Screenshot-Preferences-BD-SA.png" alt="Screenshot-Preferences-BD-SA.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That said, I'm not sure what else I can do to get the Yocto plug in to work.&lt;/P&gt;&lt;P&gt;I then tried to just to use the environment-setup file now located in the /build/tmp directory to build a Makefile based project - Uboot.&lt;/P&gt;&lt;P&gt;It failed by saying that the project was not setup. (Most likely this error is from my inexperience with compling uboot)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help or advice would be well received. Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I couldn't share it without you having to follow me.&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/DaianeAngolini"&gt;DaianeAngolini&lt;/A&gt; and &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/OtavioSalvador"&gt;OtavioSalvador&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Feb 2013 18:07:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270002#M28907</guid>
      <dc:creator>jparrish88</dc:creator>
      <dc:date>2013-02-22T18:07:27Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto - Working with the Toolchain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270003#M28908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/OtavioSalvador"&gt;OtavioSalvador&lt;/A&gt; don´t you have a movie showing how to configure it? Where is it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think the missing step would be to create the toolchain&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #222222; font-family: arial, sans-serif; background-color: #ffffff;"&gt;bitbake meta-toolchain&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Feb 2013 18:51:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270003#M28908</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2013-02-22T18:51:44Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto - Working with the Toolchain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270004#M28909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, we do; check at: &lt;A _jive_internal="true" href="https://community.nxp.com/message/304395"&gt;https://community.freescale.com/message/304395&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Feb 2013 19:16:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270004#M28909</guid>
      <dc:creator>OtavioSalvador</dc:creator>
      <dc:date>2013-02-22T19:16:57Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto - Working with the Toolchain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270005#M28910</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried this, on your suggestion, unfortunately it led to the same result. &lt;/P&gt;&lt;P&gt;I truly appreciate your help. Do you happen to have any other possible ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Feb 2013 07:56:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270005#M28910</guid>
      <dc:creator>jparrish88</dc:creator>
      <dc:date>2013-02-23T07:56:52Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto - Working with the Toolchain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270006#M28911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am sorry but I don't. We have customers using it in their customized BSPs so it works fine for all us.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Eclipse error about meta-ide-support might be because it does not know where your build system is locate. I never used it this way as we build the toolchain for the customers and they use it with Eclipse but I'd try to open Eclipse from same terminal you did the environment setup to bitbake (after sourcing it).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Feb 2013 14:47:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270006#M28911</guid>
      <dc:creator>OtavioSalvador</dc:creator>
      <dc:date>2013-02-23T14:47:57Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto - Working with the Toolchain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270007#M28912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Find a script(*.sh) in tmp. Then it will install toolchain in /opt. Select toochain/sysroot in there. Good Luck.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2013 04:13:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270007#M28912</guid>
      <dc:creator>thomaslin</dc:creator>
      <dc:date>2013-03-26T04:13:26Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto - Working with the Toolchain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270008#M28913</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry Thomas but I didn't get you; did it work for you?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2013 11:28:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270008#M28913</guid>
      <dc:creator>OtavioSalvador</dc:creator>
      <dc:date>2013-03-26T11:28:37Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto - Working with the Toolchain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270009#M28914</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, please check 2nd pic of &lt;A _jive_internal="true" href="https://community.nxp.com/thread/305027"&gt;https://community.freescale.com/thread/305027&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;I can create a "hello world!" code by esclipse and execute in TTY debug mode ok.&lt;/P&gt;&lt;P&gt;After that, system crash by Ubuntu kernel upgrade. :smileysad:&lt;/P&gt;&lt;P&gt;Try to fix so far. I will try to do similar job in Qt.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2013 14:39:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270009#M28914</guid>
      <dc:creator>thomaslin</dc:creator>
      <dc:date>2013-03-26T14:39:41Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto - Working with the Toolchain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270010#M28915</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to first fix your host or you'll have a bad time working on all this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2013 12:54:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270010#M28915</guid>
      <dc:creator>OtavioSalvador</dc:creator>
      <dc:date>2013-03-28T12:54:43Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto - Working with the Toolchain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270011#M28916</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I am using ubuntu 12.04, eclipse indigo, and have bitbaked rootfs &amp;amp; toolchain from yocto 'dylan (v1.4.1)'.&lt;/P&gt;&lt;P&gt;I then went on to setup eclipse for yocto devel &amp;amp; debug. followed the procedures from : &lt;A href="http://www.yoctoproject.org/docs/1.4/dev-manual/dev-manual.html#adt-eclipse" title="http://www.yoctoproject.org/docs/1.4/dev-manual/dev-manual.html#adt-eclipse"&gt;Yocto Project Development Manual&lt;/A&gt;&amp;nbsp; (section 4.2.2.1.3.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try to install the yocto ADT plugin it whines saying that:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;Cannot complete the install because one or more required items could not be found.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Software being installed: Yocto Project ADT Plug-in 1.4.0.201304182148 (org.yocto.sdk.feature.group 1.4.0.201304182148)&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Missing requirement: Yocto Project ADT Plug-in 1.4.0.201304182148 (org.yocto.sdk.feature.group 1.4.0.201304182148) requires 'org.eclipse.cdt.autotools.core 1.1.0' but it could not be found&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;well the Autotools are definitely installed already, but the version that is stated next to the installed version is "Autotools support for CDT (Incubation)&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.0.1.201202152032"&lt;/P&gt;&lt;P&gt;I also built the yocto-eclipse plugin from source and tried installing that too. Same thing happens.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone has seen that? how could I go about this problem ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2013 15:28:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Working-with-the-Toolchain/m-p/270011#M28916</guid>
      <dc:creator>synthnassizer</dc:creator>
      <dc:date>2013-06-12T15:28:25Z</dc:date>
    </item>
  </channel>
</rss>