<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Mounting a firewire drive</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Mounting-a-firewire-drive/m-p/269785#M28805</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a maxtor external harddrive with both USB and firewire ports.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I connect the drive using the usb port, the drive is mounted and I can browse the drive. When I try using the firewire port nothing is mounted. I I type:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;grep . /sys/bus/firewire/devices/fw*/*&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I get the output in the attached file. The drive is obviously being detected, but not mounted. I have tried the same drive on an x86 system and it mounts without any problems so I know the drive is working correctly.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Has anyone managed to mount a firewire drive successfully?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the kernel build, I have enabled Firewire driver stack, OHCI-1394 controllers and storagedevices (SBP-2 protocol). They are all built into the kernel.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336495"&gt;firewire.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Apr 2013 16:35:54 GMT</pubDate>
    <dc:creator>andrewellis</dc:creator>
    <dc:date>2013-04-16T16:35:54Z</dc:date>
    <item>
      <title>Mounting a firewire drive</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mounting-a-firewire-drive/m-p/269785#M28805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a maxtor external harddrive with both USB and firewire ports.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I connect the drive using the usb port, the drive is mounted and I can browse the drive. When I try using the firewire port nothing is mounted. I I type:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;grep . /sys/bus/firewire/devices/fw*/*&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I get the output in the attached file. The drive is obviously being detected, but not mounted. I have tried the same drive on an x86 system and it mounts without any problems so I know the drive is working correctly.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Has anyone managed to mount a firewire drive successfully?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the kernel build, I have enabled Firewire driver stack, OHCI-1394 controllers and storagedevices (SBP-2 protocol). They are all built into the kernel.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336495"&gt;firewire.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Apr 2013 16:35:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mounting-a-firewire-drive/m-p/269785#M28805</guid>
      <dc:creator>andrewellis</dc:creator>
      <dc:date>2013-04-16T16:35:54Z</dc:date>
    </item>
    <item>
      <title>Re: Mounting a firewire drive</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mounting-a-firewire-drive/m-p/269786#M28806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This problem seems to be an intermittent one, I have started the system again, and the firewire drive was mounted. On subsequent power cycles the drive was not mounted everytime. When the drive is mounted, there is an entry /dev/sdb1. When the drive is not mounted there is no entry in /dev/ for a hard drive.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm thinking the drive itself my be flakey?&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2013 12:26:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mounting-a-firewire-drive/m-p/269786#M28806</guid>
      <dc:creator>andrewellis</dc:creator>
      <dc:date>2013-04-17T12:26:12Z</dc:date>
    </item>
    <item>
      <title>Re: Mounting a firewire drive</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mounting-a-firewire-drive/m-p/269787#M28807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;which board are you using? which BSP are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Apr 2013 04:07:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mounting-a-firewire-drive/m-p/269787#M28807</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2013-04-19T04:07:10Z</dc:date>
    </item>
    <item>
      <title>Re: Mounting a firewire drive</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mounting-a-firewire-drive/m-p/269788#M28808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jimmy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the SabreSD with an i.MX6Q processor, and using BSP L3.0.35_1.1.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Apr 2013 08:58:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mounting-a-firewire-drive/m-p/269788#M28808</guid>
      <dc:creator>andrewellis</dc:creator>
      <dc:date>2013-04-19T08:58:57Z</dc:date>
    </item>
    <item>
      <title>Re: Mounting a firewire drive</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mounting-a-firewire-drive/m-p/269789#M28809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We don't support firewire on i.MX6Q&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 May 2013 08:41:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mounting-a-firewire-drive/m-p/269789#M28809</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2013-05-02T08:41:44Z</dc:date>
    </item>
  </channel>
</rss>