<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX6Q Target Description File for GDB 4.7.3 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Target-Description-File-for-GDB-4-7-3/m-p/269408#M28664</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to know what Target Description File to use for GDB 4.7.3. I have tried arm-with-neon.xml from &lt;A href="https://sourceware.org/git/gitweb.cgi?p=binutils-gdb.git;a=tree;f=gdb/features;hb=HEAD" title="https://sourceware.org/git/gitweb.cgi?p=binutils-gdb.git;a=tree;f=gdb/features;hb=HEAD"&gt;https://sourceware.org/git/gitweb.cgi?p=binutils-gdb.git;a=tree;f=gdb/features;hb=HEAD&lt;/A&gt; but I get errors when GDB reads FP registers and the CPSR is not correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anybody know which file is correct? And what file do I use if NEON is disabled?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If there are some issues with what has to be enabled by code for it to work, please express the answer in terms of the SDK, as that is the code I am using.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Dec 2013 15:19:33 GMT</pubDate>
    <dc:creator>MikeJones</dc:creator>
    <dc:date>2013-12-18T15:19:33Z</dc:date>
    <item>
      <title>iMX6Q Target Description File for GDB 4.7.3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Target-Description-File-for-GDB-4-7-3/m-p/269408#M28664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to know what Target Description File to use for GDB 4.7.3. I have tried arm-with-neon.xml from &lt;A href="https://sourceware.org/git/gitweb.cgi?p=binutils-gdb.git;a=tree;f=gdb/features;hb=HEAD" title="https://sourceware.org/git/gitweb.cgi?p=binutils-gdb.git;a=tree;f=gdb/features;hb=HEAD"&gt;https://sourceware.org/git/gitweb.cgi?p=binutils-gdb.git;a=tree;f=gdb/features;hb=HEAD&lt;/A&gt; but I get errors when GDB reads FP registers and the CPSR is not correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anybody know which file is correct? And what file do I use if NEON is disabled?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If there are some issues with what has to be enabled by code for it to work, please express the answer in terms of the SDK, as that is the code I am using.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Dec 2013 15:19:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Target-Description-File-for-GDB-4-7-3/m-p/269408#M28664</guid>
      <dc:creator>MikeJones</dc:creator>
      <dc:date>2013-12-18T15:19:33Z</dc:date>
    </item>
  </channel>
</rss>