<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Sabre Lite Terminal Keyboard Input Error in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Sabre-Lite-Terminal-Keyboard-Input-Error/m-p/269094#M28584</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem with the Temrinal emulation (putty) with my Sabre Lite board.&lt;/P&gt;&lt;P&gt;The output from the boot process ist correct, but I can`t make any input...&lt;SPAN class="emoticon_sad emoticon-inline"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The OS on my PC ist Windows 7 64-bit&lt;/P&gt;&lt;P&gt;The settings of the terminal emulation seems to be okay:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;115.2 kbaud, 8 data bits, 1 stop bit, no parity, no flow control.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used the cables from the kit: 1 Custom Serial cable, 6-pin female to dual DB9 mal connectos an 1 DB9 female to DB9 female cable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What ist wrong? Where is my mistake?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Feb 2014 21:29:00 GMT</pubDate>
    <dc:creator>chrisgeilker</dc:creator>
    <dc:date>2014-02-28T21:29:00Z</dc:date>
    <item>
      <title>Sabre Lite Terminal Keyboard Input Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sabre-Lite-Terminal-Keyboard-Input-Error/m-p/269094#M28584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem with the Temrinal emulation (putty) with my Sabre Lite board.&lt;/P&gt;&lt;P&gt;The output from the boot process ist correct, but I can`t make any input...&lt;SPAN class="emoticon_sad emoticon-inline"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The OS on my PC ist Windows 7 64-bit&lt;/P&gt;&lt;P&gt;The settings of the terminal emulation seems to be okay:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;115.2 kbaud, 8 data bits, 1 stop bit, no parity, no flow control.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used the cables from the kit: 1 Custom Serial cable, 6-pin female to dual DB9 mal connectos an 1 DB9 female to DB9 female cable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What ist wrong? Where is my mistake?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Feb 2014 21:29:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sabre-Lite-Terminal-Keyboard-Input-Error/m-p/269094#M28584</guid>
      <dc:creator>chrisgeilker</dc:creator>
      <dc:date>2014-02-28T21:29:00Z</dc:date>
    </item>
    <item>
      <title>Re: Sabre Lite Terminal Keyboard Input Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sabre-Lite-Terminal-Keyboard-Input-Error/m-p/269095#M28585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chris,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your settings are correct (115200,8,N,1, no flow control).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The dual-DB-9 to Molex cable we ship is configured as DCE, to allow direct connection to a PC serial port or USB serial adapter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not sure what you're referring to regarding the DB9 female-female cable and the "custom serial cable".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you take a photo?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From your description of the symptoms, it appears that the Tx line from your PC isn't making it to the board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Feb 2014 22:28:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sabre-Lite-Terminal-Keyboard-Input-Error/m-p/269095#M28585</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-02-28T22:28:18Z</dc:date>
    </item>
    <item>
      <title>Re: Sabre Lite Terminal Keyboard Input Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sabre-Lite-Terminal-Keyboard-Input-Error/m-p/269096#M28586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The DB9 cable&amp;nbsp; ist a standard serial cable Sub D&lt;/P&gt;&lt;P&gt;The other cable is a Molex to 2 x Sub D (one for Debug).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Cables ar in the Kit from element14.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the pho&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42931i607D23A888FA8E9C/image-size/large?v=v2&amp;amp;px=999" title="IMG_20140301_084439082[1].jpg" alt="IMG_20140301_084439082[1].jpg" /&gt;&lt;/span&gt;to:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Mar 2014 13:56:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sabre-Lite-Terminal-Keyboard-Input-Error/m-p/269096#M28586</guid>
      <dc:creator>chrisgeilker</dc:creator>
      <dc:date>2014-03-01T13:56:33Z</dc:date>
    </item>
    <item>
      <title>Re: Sabre Lite Terminal Keyboard Input Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sabre-Lite-Terminal-Keyboard-Input-Error/m-p/269097#M28587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chris,&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;Chris Geilker wrote:d&lt;/P&gt;
&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;... &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;The Cables ar in the Kit from element14.&lt;/P&gt;
&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I have no idea how you need to cable things. You might need to put a meter on the cable to verify that pin 3 on your DB-9 from your PC is connected to Pin 5 of J17 on the SABRE Lite.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Mar 2014 16:35:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sabre-Lite-Terminal-Keyboard-Input-Error/m-p/269097#M28587</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-03-01T16:35:34Z</dc:date>
    </item>
  </channel>
</rss>