<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Command interpreter for iMX28</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Command-interpreter-for-iMX28/m-p/268697#M28452</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, mike&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; For register read/write, there is already tools, such as "md" and "mw" command in uboot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; In linux kernel, our BSP rootfs has a tool called "memtool", it is in /unit_tests/, you can use it to read/write register directly in kernel.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; These tools are only for register read/write.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Jul 2013 08:46:16 GMT</pubDate>
    <dc:creator>AnsonHuang</dc:creator>
    <dc:date>2013-07-12T08:46:16Z</dc:date>
    <item>
      <title>Command interpreter for iMX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Command-interpreter-for-iMX28/m-p/268695#M28450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;for starting-up with my own hardware and later for testing I want to implement a command interpreter with functions like read/write CPU registers, read/write I/Os, reading ADC-value and so on.&lt;/P&gt;&lt;P&gt;Does anyone know whether one is already available?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jul 2013 08:31:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Command-interpreter-for-iMX28/m-p/268695#M28450</guid>
      <dc:creator>michaelkoelbl</dc:creator>
      <dc:date>2013-07-12T08:31:42Z</dc:date>
    </item>
    <item>
      <title>Re: Command interpreter for iMX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Command-interpreter-for-iMX28/m-p/268696#M28451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;U-boot is not bad candidate.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jul 2013 08:43:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Command-interpreter-for-iMX28/m-p/268696#M28451</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-07-12T08:43:00Z</dc:date>
    </item>
    <item>
      <title>Re: Command interpreter for iMX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Command-interpreter-for-iMX28/m-p/268697#M28452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, mike&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; For register read/write, there is already tools, such as "md" and "mw" command in uboot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; In linux kernel, our BSP rootfs has a tool called "memtool", it is in /unit_tests/, you can use it to read/write register directly in kernel.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; These tools are only for register read/write.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jul 2013 08:46:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Command-interpreter-for-iMX28/m-p/268697#M28452</guid>
      <dc:creator>AnsonHuang</dc:creator>
      <dc:date>2013-07-12T08:46:16Z</dc:date>
    </item>
  </channel>
</rss>