<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: &amp;quot;FSL gnome release package&amp;quot; build fails at python build stage</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/quot-FSL-gnome-release-package-quot-build-fails-at-python-build/m-p/158841#M2844</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Mar 2013 05:28:32 GMT</pubDate>
    <dc:creator>zhiyancao</dc:creator>
    <dc:date>2013-03-20T05:28:32Z</dc:date>
    <item>
      <title>"FSL gnome release package" build fails at python build stage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/quot-FSL-gnome-release-package-quot-build-fails-at-python-build/m-p/158838#M2841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to build a minimal gnome environment using the "FSL gnome release package" build option in ltib.&lt;/P&gt;&lt;P&gt;However, my build is failing at the python build stage.&amp;nbsp; I did some digging and found a similar problem with fontconfig but attempting to apply the solution to my python.spec proved unsuccessful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the relevant output:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;creating Makefile&lt;BR /&gt;+ make python Parser/pgen&lt;BR /&gt;gcc -pthread -DNDEBUG -g -O3 -Wall -Wstrict-prototypes&amp;nbsp;&amp;nbsp; Parser/acceler.o Parser/grammar1.o Parser/listnode.o Parser/node.o Parser/parser.o Parser/parsetok.o Parser/bitset.o Parser/metagrammar.o Parser/firstsets.o Parser/grammar.o Parser/pgen.o Objects/obmalloc.o Python/mysnprintf.o Parser/tokenizer_pgen.o Parser/printgrammar.o Parser/pgenmain.o -lpthread -ldl&amp;nbsp; -lutil -o Parser/pgen&lt;BR /&gt;gcc -pthread -c -fno-strict-aliasing -DNDEBUG -g -O3 -Wall -Wstrict-prototypes -I. -I./Include&amp;nbsp; -DPy_BUILD_CORE -o Modules/config.o Modules/config.c&lt;BR /&gt;gcc -pthread -c -fno-strict-aliasing -DNDEBUG -g -O3 -Wall -Wstrict-prototypes -I. -I./Include&amp;nbsp; -DPy_BUILD_CORE -DPYTHONPATH='":plat-linux3:lib-tk"' \&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;-DPREFIX='"/usr/local"' \&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;-DEXEC_PREFIX='"/usr/local"' \&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;-DVERSION='"2.4"' \&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;-DVPATH='""' \&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;-o Modules/getpath.o ./Modules/getpath.c&lt;BR /&gt;/usr/bin/ld: Parser/tokenizer_pgen.o: Relocations in generic ELF (EM: 40)&lt;BR /&gt;/usr/bin/ld: Parser/tokenizer_pgen.o: Relocations in generic ELF (EM: 40)&lt;BR /&gt;/usr/bin/ld: Parser/tokenizer_pgen.o: Relocations in generic ELF (EM: 40)&lt;BR /&gt;/usr/bin/ld: Parser/tokenizer_pgen.o: Relocations in generic ELF (EM: 40)&lt;BR /&gt;/usr/bin/ld: Parser/tokenizer_pgen.o: Relocations in generic ELF (EM: 40)&lt;BR /&gt;/usr/bin/ld: Parser/tokenizer_pgen.o: Relocations in generic ELF (EM: 40)&lt;BR /&gt;/usr/bin/ld: Parser/tokenizer_pgen.o: Relocations in generic ELF (EM: 40)&lt;BR /&gt;Parser/tokenizer_pgen.o: could not read symbols: File in wrong format&lt;BR /&gt;collect2: ld returned 1 exit status&lt;BR /&gt;make: *** [Parser/pgen] Error 1&lt;BR /&gt;make: *** Waiting for unfinished jobs....&lt;BR /&gt;./Modules/getpath.c: In function 'copy_absolute':&lt;BR /&gt;./Modules/getpath.c:230: warning: ignoring return value of 'getcwd', declared with attribute warn_unused_result&lt;BR /&gt;error: Bad exit status from /home/robb/ARM_board/L2.6.35_11.09.01_ER_source/ltib/tmp/rpm-tmp.85951 (%build)&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;RPM build errors:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Bad exit status from /home/robb/ARM_board/L2.6.35_11.09.01_ER_source/ltib/tmp/rpm-tmp.85951 (%build)&lt;BR /&gt;Build time for python: 20 seconds&lt;BR /&gt;&lt;BR /&gt;Failed building python&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 May 2012 19:35:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/quot-FSL-gnome-release-package-quot-build-fails-at-python-build/m-p/158838#M2841</guid>
      <dc:creator>Robb1z</dc:creator>
      <dc:date>2012-05-02T19:35:02Z</dc:date>
    </item>
    <item>
      <title>Re: "FSL gnome release package" build fails at python build stage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/quot-FSL-gnome-release-package-quot-build-fails-at-python-build/m-p/158839#M2842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi I had the same problem, I never knew why it failed.&lt;BR /&gt;The solution is to go to the folder were Python was being build and do a 'make clean', then you can run ltib again and see it compile it without problems.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 May 2012 21:21:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/quot-FSL-gnome-release-package-quot-build-fails-at-python-build/m-p/158839#M2842</guid>
      <dc:creator>JorgeMuaﾱoz</dc:creator>
      <dc:date>2012-05-02T21:21:47Z</dc:date>
    </item>
    <item>
      <title>Re: "FSL gnome release package" build fails at python build stage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/quot-FSL-gnome-release-package-quot-build-fails-at-python-build/m-p/158840#M2843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That did it...&lt;/P&gt;&lt;P&gt;Would love to know what that means because I came across it again while cross-compiling some custom applications and a 'make clean' didn't solve it... but I'll settle for a workaround for now!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks Jorge.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 May 2012 15:55:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/quot-FSL-gnome-release-package-quot-build-fails-at-python-build/m-p/158840#M2843</guid>
      <dc:creator>Robb1z</dc:creator>
      <dc:date>2012-05-03T15:55:09Z</dc:date>
    </item>
    <item>
      <title>Re: "FSL gnome release package" build fails at python build stage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/quot-FSL-gnome-release-package-quot-build-fails-at-python-build/m-p/158841#M2844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2013 05:28:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/quot-FSL-gnome-release-package-quot-build-fails-at-python-build/m-p/158841#M2844</guid>
      <dc:creator>zhiyancao</dc:creator>
      <dc:date>2013-03-20T05:28:32Z</dc:date>
    </item>
    <item>
      <title>Re: "FSL gnome release package" build fails at python build stage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/quot-FSL-gnome-release-package-quot-build-fails-at-python-build/m-p/158842#M2845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just tried to reproduce the problem executing the above command but the issue was not present; I believe you found it when just running './ltib'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;./ltib -m prep -p python &amp;amp;&amp;amp; ./ltib -m scbuild -p python&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure why the &lt;EM&gt;make clean&lt;/EM&gt; solves the issues. Perhaps adding this extra command on the python spec can avoid this, not sure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2013 20:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/quot-FSL-gnome-release-package-quot-build-fails-at-python-build/m-p/158842#M2845</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-03-21T20:53:48Z</dc:date>
    </item>
  </channel>
</rss>