<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMX28 and SocketCAN</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX28-and-SocketCAN/m-p/268309#M28371</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been trying without success to get the Libsocketcan working with the i.MX28.&amp;nbsp; I'm using the 2.6.35.3 kernel and libsocketcan-0.0.8 (tried 0.0.9 also).&amp;nbsp; Compile fails saying IFLA_LINK_INFO, IFLA_INFO_KIND, IFLA_INFO_DATA and IFLA_INFO_MAX are undefined, while they are indeed in the if_link.h header.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there another kernel version I should be using with the i.MX28, or is there another way to get socketcan support working in 2.6.35.3?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you everyone.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Feb 2013 23:04:37 GMT</pubDate>
    <dc:creator>roryhansen</dc:creator>
    <dc:date>2013-02-21T23:04:37Z</dc:date>
    <item>
      <title>MX28 and SocketCAN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX28-and-SocketCAN/m-p/268309#M28371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been trying without success to get the Libsocketcan working with the i.MX28.&amp;nbsp; I'm using the 2.6.35.3 kernel and libsocketcan-0.0.8 (tried 0.0.9 also).&amp;nbsp; Compile fails saying IFLA_LINK_INFO, IFLA_INFO_KIND, IFLA_INFO_DATA and IFLA_INFO_MAX are undefined, while they are indeed in the if_link.h header.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there another kernel version I should be using with the i.MX28, or is there another way to get socketcan support working in 2.6.35.3?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you everyone.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2013 23:04:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX28-and-SocketCAN/m-p/268309#M28371</guid>
      <dc:creator>roryhansen</dc:creator>
      <dc:date>2013-02-21T23:04:37Z</dc:date>
    </item>
    <item>
      <title>Re: MX28 and SocketCAN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX28-and-SocketCAN/m-p/268310#M28372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In imx28evk_defconfig file, you can see that CONFIG_CAN_BCM, CONFIG_CAN_DEV and CONFIG_CAN_VCAN are disabled by default.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CONFIG_CAN=y&lt;/P&gt;&lt;P&gt;CONFIG_CAN_RAW=y&lt;/P&gt;&lt;P&gt;# CONFIG_CAN_BCM is not set&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#&lt;/P&gt;&lt;P&gt;# CAN Device Drivers&lt;/P&gt;&lt;P&gt;#&lt;/P&gt;&lt;P&gt;# CONFIG_CAN_VCAN is not set&lt;/P&gt;&lt;P&gt;# CONFIG_CAN_DEV is not set&lt;/P&gt;&lt;P&gt;# CONFIG_CAN_DEBUG_DEVICES is not set&lt;/P&gt;&lt;P&gt;CONFIG_CAN_FLEXCAN=m&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can run ./ltib -m config , then choose configure kernel.&lt;/P&gt;&lt;P&gt;In kernel configure menu, Networking support -&amp;gt; Can bus subsystem support, to enable them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Grace&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Apr 2013 08:26:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX28-and-SocketCAN/m-p/268310#M28372</guid>
      <dc:creator>GraceH</dc:creator>
      <dc:date>2013-04-03T08:26:15Z</dc:date>
    </item>
    <item>
      <title>Re: MX28 and SocketCAN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX28-and-SocketCAN/m-p/268311#M28373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With the original 10.12.01 kernel release, SocketCAN was largely not working.&amp;nbsp; This was corrected in the latest 1.1.0_130130 release.&amp;nbsp; SocketCAN now works.&amp;nbsp; Note that when compiling, the "-f" option is often still required to get everything built correctly for it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Apr 2013 18:06:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX28-and-SocketCAN/m-p/268311#M28373</guid>
      <dc:creator>roryhansen</dc:creator>
      <dc:date>2013-04-05T18:06:42Z</dc:date>
    </item>
    <item>
      <title>Re: MX28 and SocketCAN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX28-and-SocketCAN/m-p/268312#M28374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Rory&lt;/P&gt;&lt;P&gt;If your issue had been resolved please click Correct Answer.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Apr 2013 09:23:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX28-and-SocketCAN/m-p/268312#M28374</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2013-04-22T09:23:11Z</dc:date>
    </item>
  </channel>
</rss>