<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUsing a custom GStreamer plugin on imx233</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-a-custom-GStreamer-plugin-on-imx233/m-p/158771#M2837</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, has anyone managed to create a gstreamer plugin using the template kit and built it so that it works on a freescale board (specifically the imx233)? My plugin builds fine for windows but won't come up on the board with gst-inspect saying:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(gst-inspect-0.10:714): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libspadecoder.so': /usr/lib/gstreamer-0.10/libspadecoder.so: cannot open shared object file: No such file or directory&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(And yes, the files mentioned there do exist at those paths).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried changing a couple of things having looked at the freescale plugin package and how that builds, but I'm not great with how the configure/make files operate and so far nothing I've tried has changed the above message.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 May 2012 14:51:27 GMT</pubDate>
    <dc:creator>TB</dc:creator>
    <dc:date>2012-05-04T14:51:27Z</dc:date>
    <item>
      <title>Using a custom GStreamer plugin on imx233</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-a-custom-GStreamer-plugin-on-imx233/m-p/158771#M2837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, has anyone managed to create a gstreamer plugin using the template kit and built it so that it works on a freescale board (specifically the imx233)? My plugin builds fine for windows but won't come up on the board with gst-inspect saying:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(gst-inspect-0.10:714): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libspadecoder.so': /usr/lib/gstreamer-0.10/libspadecoder.so: cannot open shared object file: No such file or directory&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(And yes, the files mentioned there do exist at those paths).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried changing a couple of things having looked at the freescale plugin package and how that builds, but I'm not great with how the configure/make files operate and so far nothing I've tried has changed the above message.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 May 2012 14:51:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-a-custom-GStreamer-plugin-on-imx233/m-p/158771#M2837</guid>
      <dc:creator>TB</dc:creator>
      <dc:date>2012-05-04T14:51:27Z</dc:date>
    </item>
  </channel>
</rss>