<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 HDMI video with NFS</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-video-with-NFS/m-p/268105#M28303</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to test some GUI, so I need to connect the device to a video.&lt;/P&gt;&lt;P&gt;I was able to let it work booting from SD with these parameters in u-boot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait video=mxcfb0:dev=hdmi,1920x1200M@60,if=RGB24&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried putting the &lt;EM&gt;video&lt;/EM&gt; part in bootargs_nfs, but it isn't working. I've read in another post that in NFS the HDMI device became &lt;EM&gt;mxcfb1&lt;/EM&gt;, but hadn't luck with ith either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any hints?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;MIX&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Dec 2013 11:08:58 GMT</pubDate>
    <dc:creator>il_mix</dc:creator>
    <dc:date>2013-12-18T11:08:58Z</dc:date>
    <item>
      <title>HDMI video with NFS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-video-with-NFS/m-p/268105#M28303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to test some GUI, so I need to connect the device to a video.&lt;/P&gt;&lt;P&gt;I was able to let it work booting from SD with these parameters in u-boot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait video=mxcfb0:dev=hdmi,1920x1200M@60,if=RGB24&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried putting the &lt;EM&gt;video&lt;/EM&gt; part in bootargs_nfs, but it isn't working. I've read in another post that in NFS the HDMI device became &lt;EM&gt;mxcfb1&lt;/EM&gt;, but hadn't luck with ith either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any hints?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;MIX&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Dec 2013 11:08:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-video-with-NFS/m-p/268105#M28303</guid>
      <dc:creator>il_mix</dc:creator>
      <dc:date>2013-12-18T11:08:58Z</dc:date>
    </item>
    <item>
      <title>Re: HDMI video with NFS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-video-with-NFS/m-p/268106#M28304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Massimo,&lt;/P&gt;&lt;P&gt;When you built BSP in LTIB , the &lt;STRONG&gt;Target Image Generation&lt;/STRONG&gt; you need to chose "NFS ONLY". It means that the uImage you download to your board is the one generated under NFS Target image.&lt;/P&gt;&lt;P&gt;Hope this can help you~~&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2013 05:57:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-video-with-NFS/m-p/268106#M28304</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2013-12-19T05:57:16Z</dc:date>
    </item>
  </channel>
</rss>