<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx-lib build error using LTIB and a local kernel source in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx-lib-build-error-using-LTIB-and-a-local-kernel-source/m-p/158710#M2830</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi again,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the i.MX535 on a Karos based dev board. I have successfully built the kernel using the source supplied from Karos along with LTIB. Great!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now when I add imx-lib to the packages to be built I get the following errors &lt;A href="http://www.pastebin.org/Btb1mN58" target="_blank"&gt;www.pastebin.org/Btb1mN58&lt;/A&gt;&amp;nbsp;Taking note of lines 84 &amp;amp; 85&amp;nbsp;these files are present in the directory described. Also I was aware that the mxc folder was missing from the drivers folder in my local source so, this might be&amp;nbsp;naive, but I copied the mxc driver folder from the freescale BSP into my kernel folder.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;No change?I take it it is not as straightforward as that? Are there other things I should e looking at? Any tips would be great.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Wayne&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Jun 2011 14:54:38 GMT</pubDate>
    <dc:creator>wayne_ng</dc:creator>
    <dc:date>2011-06-27T14:54:38Z</dc:date>
    <item>
      <title>imx-lib build error using LTIB and a local kernel source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-lib-build-error-using-LTIB-and-a-local-kernel-source/m-p/158710#M2830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi again,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the i.MX535 on a Karos based dev board. I have successfully built the kernel using the source supplied from Karos along with LTIB. Great!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now when I add imx-lib to the packages to be built I get the following errors &lt;A href="http://www.pastebin.org/Btb1mN58" target="_blank"&gt;www.pastebin.org/Btb1mN58&lt;/A&gt;&amp;nbsp;Taking note of lines 84 &amp;amp; 85&amp;nbsp;these files are present in the directory described. Also I was aware that the mxc folder was missing from the drivers folder in my local source so, this might be&amp;nbsp;naive, but I copied the mxc driver folder from the freescale BSP into my kernel folder.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;No change?I take it it is not as straightforward as that? Are there other things I should e looking at? Any tips would be great.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Wayne&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jun 2011 14:54:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-lib-build-error-using-LTIB-and-a-local-kernel-source/m-p/158710#M2830</guid>
      <dc:creator>wayne_ng</dc:creator>
      <dc:date>2011-06-27T14:54:38Z</dc:date>
    </item>
  </channel>
</rss>