<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: VGA &amp; LVDS screens together in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/VGA-LVDS-screens-together/m-p/267861#M28258</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Another observation is that&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;if parents' clocks are forced in ldb and tve drivers,&lt;/LI&gt;&lt;LI&gt;and if &lt;SPAN style="text-decoration: line-through;"&gt;the last instruction of mxcfb_blank is not executed (that is mxc_fbi-&amp;gt;cur_blank = blank;)&lt;/SPAN&gt; mxcfb_blank returns 1 when LVDS is unblank with di1_primary kernel option&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;then both display are correct.&lt;/P&gt;&lt;P&gt;But :&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;It sounds like a very bad situation-specific fix&lt;/LI&gt;&lt;LI&gt;The application do not work anymore anyway [it works on LVDS when started with di0_primary, but VGA is broken]&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT : This morning I realize that it is not the last instruction, but return statement that leads to this behavior.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 May 2013 15:09:06 GMT</pubDate>
    <dc:creator>FTO</dc:creator>
    <dc:date>2013-05-31T15:09:06Z</dc:date>
    <item>
      <title>VGA &amp; LVDS screens together</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VGA-LVDS-screens-together/m-p/267858#M28255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We want to display data on two screens at the same time on Linux, one connected to a LVDS display, and one connected to a VGA screen, with our custom iMX53 board. But we do not succeed yet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Displays have different timings, so we think we need to use the two DI separately.&lt;BR /&gt;VGA is necessarily linked to DI1, so we choose to use LVDS1 (where is linked our second display in hardware) in dual mode with DI0 source.&lt;/P&gt;&lt;P&gt;It seems to be the only way to display DI0 to LVDS1 and LVDS0 signals are not connected anyway.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;We use VGA-XGA video mode for VGA display and a custom video mode for the LVDS display :&lt;/P&gt;&lt;PRE&gt;{
&amp;nbsp; /* 640x480 @ 60 Hz 25M pixel clk */
&amp;nbsp; "PRIMEVIEW-PD050VL1", 60, 640, 480, 40000,
&amp;nbsp; 46, 18,
&amp;nbsp; 33, 10,
&amp;nbsp; 96, 2,
&amp;nbsp; 0, // sync
&amp;nbsp; FB_VMODE_NONINTERLACED, // vmode
&amp;nbsp; FB_MODE_IS_DETAILED, // flag
}&lt;/PRE&gt;&lt;P&gt;Timing parameters are based on screen datasheet, but not 100% sure what sync, vmode and flag should be.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With this and the following kernel command line&lt;/P&gt;&lt;PRE&gt;console=ttymxc0,115200 consoleblank=0 video=mxcdi1fb:GBR24,VGA-XGA vga di0_primary video=mxcdi0fb:RGB666,PRIMEVIEW-PD050VL1,bpp=32 ldb=dual,di=0,ch0_map=SPWG,ch1_map=SPWG&lt;/PRE&gt;&lt;P&gt;and after unblanking VGA, we can observe that&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;LVDS displays an stretched Tux (larger width only) on 1/3 of the screen width. Remaining 2/3 are junk.&lt;/LI&gt;&lt;LI&gt;VGA displays a strange Tux, like if some little vertical bands have been cut and other parts &lt;SPAN lang="en"&gt;glued back together. Really difficult to describe.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;When drawing a &lt;SPAN lang="en"&gt;checkerboard&lt;/SPAN&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN lang="en"&gt;LVDS displays &lt;/SPAN&gt;an stretched &lt;SPAN lang="en"&gt;checkerboard &lt;/SPAN&gt;(larger width only) on 1/3 of the screen width. I see 8 squares plus half one (actually rectangles) instead of 64 in x direction, and 48 as expected in y direction. Remaining 2/3 are junk.&lt;/LI&gt;&lt;LI&gt;VGA displays a &lt;SPAN lang="en"&gt;checkerboard with variable &lt;/SPAN&gt;squares width (actually rectangles).&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Moreover, if we use ldb=off instead of dual mode, VGA is just fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wish to precise that the application writes correct data on fb0 and fb1, the question is &lt;EM&gt;NOT&lt;/EM&gt; about it. Also w&lt;SPAN style="font-weight: normal;"&gt;e use &lt;EM&gt;NEITHER&lt;/EM&gt; gstreamer &lt;EM&gt;NOR&lt;/EM&gt; X-server at all. Data are drawn directly to framebuffers memory through IPU ioctls. The problem is the same with direct write to /dev/fb0 node.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-weight: normal;"&gt;The question is really about displaying the two framebuffers themselves on our two displays simultaneously.&lt;/P&gt;&lt;P style="font-weight: normal;"&gt;&lt;/P&gt;&lt;P style="font-weight: normal;"&gt;&lt;/P&gt;&lt;P style="font-weight: normal;"&gt;Every documentation we read always return us to the same kernel command lines &amp;amp; co. So we have tried MANY combinations : di0_primary/di1_primary and turn on the other screen, add video mode also to ldb.c, try other video modes, try timings from PhytecBSP with the same LVDS, change LVDS cable, change LVDS screen, and so on...&lt;/P&gt;&lt;P style="font-weight: normal;"&gt;&lt;/P&gt;&lt;P style="font-weight: normal;"&gt;&lt;/P&gt;&lt;P style="font-weight: normal;"&gt;Has anyone ever succeeded in this VGA/LVDS mix ?&lt;/P&gt;&lt;P style="font-weight: normal;"&gt;Do you have an idea how to do it well ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 May 2013 13:29:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VGA-LVDS-screens-together/m-p/267858#M28255</guid>
      <dc:creator>FTO</dc:creator>
      <dc:date>2013-05-31T13:29:18Z</dc:date>
    </item>
    <item>
      <title>Re: VGA &amp; LVDS screens together</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VGA-LVDS-screens-together/m-p/267859#M28256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin-bottom: 0cm; font-weight: normal; page-break-before: always;"&gt;Here some context :&lt;/P&gt;&lt;P style="margin-bottom: 0cm; font-weight: normal;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: 0cm;"&gt;&lt;STRONG&gt;The board&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="margin-bottom: 0cm;"&gt;We designed a board based on an iMX53. Its basic operation is to transfer video from CSI to both VGA connector and LVDS display at the same time, along with some information.&lt;/P&gt;&lt;P style="margin-bottom: 0cm;"&gt;The VGA connector is linked to the TVE signals of the IMX and LVDS display is linked to LVDS1 outputs of the IMX.&lt;/P&gt;&lt;P style="margin-bottom: 0cm;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: 0cm;"&gt;We observed similar results on QSB with LVDS0. Although we tried it, few tests have been made on this platform which is not the final product.&lt;/P&gt;&lt;P style="margin-bottom: 0cm;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: 0cm;"&gt;&lt;STRONG&gt;Kernel&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="margin-bottom: 0cm;"&gt;The kernel used is based on imx-rel_imx_2.6.35_11.09.01&lt;/P&gt;&lt;P style="margin-bottom: 0cm;"&gt;We have a custom board file, mainly a mix of SMD &amp;amp; LOCO board file.&lt;/P&gt;&lt;P style="margin-bottom: 0cm;"&gt;We have a driver for a chip that is made for 2.6.35 kernel version, wich interracts with V4L2 input&lt;/P&gt;&lt;P style="margin-bottom: 0cm;"&gt;&lt;SPAN lang="en-US"&gt;This patch &lt;A class="western" href="http://repository.timesys.com/buildsources/k/kernel/kernel-2.6.35/linux-2.6.35-mxc-ipu3-dual-display.patch"&gt;http://repository.timesys.com/buildsources/k/kernel/kernel-2.6.35/linux-2.6.35-mxc-ipu3-dual-display.patch&lt;/A&gt; is applied, because of this page &lt;A class="western" href="https://linuxlink.timesys.com/docs/gsg/i.MX53START"&gt;https://linuxlink.timesys.com/docs/gsg/i.MX53START&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 May 2013 13:30:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VGA-LVDS-screens-together/m-p/267859#M28256</guid>
      <dc:creator>FTO</dc:creator>
      <dc:date>2013-05-31T13:30:05Z</dc:date>
    </item>
    <item>
      <title>Re: VGA &amp; LVDS screens together</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VGA-LVDS-screens-together/m-p/267860#M28257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have also noticed that LVDS display is fully correct when we apply the following sequence in userspace :&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;fbset -g 640 480 640 1400 32 -fb /dev/fb1&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;Here the LVDS displays an horizontally stretched &lt;SPAN lang="en"&gt;checkerboard&lt;/SPAN&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;fbset -g 640 480 640 1400 32 -fb /dev/fb0&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;Now the LVDS displays correctly&lt;/P&gt;&lt;P&gt;Both steps are necessary and of course VGA do not work anymore.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en-US"&gt;Based on this observation, I &lt;/SPAN&gt;dived&lt;SPAN lang="en-US"&gt; into the kernel code and saw that di0 and di1 share the same “parent clock” which seems to be modified by of drivers with different values.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en-US"&gt;Thus I tried to force it with one fix value in both drivers.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en-US"&gt;Furthermore, I had to divide LVDS pixclock by two compared to the screen specifications.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en-US"&gt;Now, when the system is started with di0_primary keyword, the LVDS is correct, but VGA screen complains about timings as during the “trick” presented above.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en-US"&gt;When the system is started with di1_primary keyword, the VGA is correct.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en-US"&gt;In both cases, when the second screen is turned on, the VGA complains about timings and LVDS is correct.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 May 2013 13:33:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VGA-LVDS-screens-together/m-p/267860#M28257</guid>
      <dc:creator>FTO</dc:creator>
      <dc:date>2013-05-31T13:33:51Z</dc:date>
    </item>
    <item>
      <title>Re: VGA &amp; LVDS screens together</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VGA-LVDS-screens-together/m-p/267861#M28258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Another observation is that&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;if parents' clocks are forced in ldb and tve drivers,&lt;/LI&gt;&lt;LI&gt;and if &lt;SPAN style="text-decoration: line-through;"&gt;the last instruction of mxcfb_blank is not executed (that is mxc_fbi-&amp;gt;cur_blank = blank;)&lt;/SPAN&gt; mxcfb_blank returns 1 when LVDS is unblank with di1_primary kernel option&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;then both display are correct.&lt;/P&gt;&lt;P&gt;But :&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;It sounds like a very bad situation-specific fix&lt;/LI&gt;&lt;LI&gt;The application do not work anymore anyway [it works on LVDS when started with di0_primary, but VGA is broken]&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT : This morning I realize that it is not the last instruction, but return statement that leads to this behavior.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 May 2013 15:09:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VGA-LVDS-screens-together/m-p/267861#M28258</guid>
      <dc:creator>FTO</dc:creator>
      <dc:date>2013-05-31T15:09:06Z</dc:date>
    </item>
    <item>
      <title>Re: VGA &amp; LVDS screens together</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VGA-LVDS-screens-together/m-p/267862#M28259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;These problems look related with "ipu_di1_clk" and FB format, according to your experientment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For FB format, I am not sure if you did modify "fb_data" structure in your board description source. The definition order of fb_data implies how DI maps. You&amp;nbsp; may check your definition.&lt;/P&gt;&lt;P&gt;//"arch/arm/mach-mx5/mx53_ard.c"&lt;/P&gt;&lt;P&gt;static struct mxc_fb_platform_data fb_data[] = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .interface_pix_fmt = IPU_PIX_FMT_RGB666,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .mode_str = "XGA",&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .mode = video_modes,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .num_modes = ARRAY_SIZE(video_modes),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; },&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .interface_pix_fmt = IPU_PIX_FMT_GBR24,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .mode_str = "1024x768M-16@60",&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .mode = video_modes,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .num_modes = ARRAY_SIZE(video_modes),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; },&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For "ipu_di1_clk", ldb driver appears to only support one by one mapping between ldb channel and di channel. LDB dual mode changes di0 and di1 clocks, and route ldb both channels to one di channel.&lt;/P&gt;&lt;P&gt;Suggest you add extra mode into ldb driver for your lvds1-to-di0 configuration, like "ldb=signale,di=0".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jun 2013 04:37:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VGA-LVDS-screens-together/m-p/267862#M28259</guid>
      <dc:creator>max_tsai</dc:creator>
      <dc:date>2013-06-10T04:37:17Z</dc:date>
    </item>
  </channel>
</rss>