<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: can't connect to the camera in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/can-t-connect-to-the-camera/m-p/266458#M27820</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Saurabh,&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;Yes, you are correct. I did go through the Android Advanced User Guide which came with the android release package and found that it has a separate section for USB Camera support which talks about the modifications you suggested and plus few others as well.&lt;/P&gt;&lt;P&gt;I will update the status once I have tried it out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Sumit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 01 Mar 2014 06:40:05 GMT</pubDate>
    <dc:creator>sumitsinha</dc:creator>
    <dc:date>2014-03-01T06:40:05Z</dc:date>
    <item>
      <title>can't connect to the camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/can-t-connect-to-the-camera/m-p/266454#M27816</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on MCIMX6DL-SDP board which has android 4.0.4 running on it. The Android O.S. came pre - installed along with the board in the NOR flash and I am using NAND boot. The OS build number is R13.4-beta. When I connect a logitech usb camera to the board, I can see the following messages getting displayed on my minicom console:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;uvcvideo: Found UVC 1.00 device &amp;lt;unnamed&amp;gt; (046d:0825)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;input: UVC Camera (046d:0825) as /devices/platform/fsl-ehci.0/usb1/1-1/1-1:1.0/8&lt;/P&gt;&lt;P&gt;3:3:1: cannot get freq at ep 0x86 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, I do see a video node appearing in the 'dev' directory, every time I connect the camera to the board, displayed as "video2". Hence, I assume that the external camera is getting detected. However, When I try to launch the built in Camera app, it says "Can't connect to camera". Also, I can see the following error on my minicom console:&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: slave not found!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The logcat -v time messages which I receive at the time of launching the camera app are as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;01-01 00:00:03.300 I/imx6.gralloc( 2203): disp_mode is D:1024x768p-60&lt;/P&gt;&lt;P&gt;01-01 00:00:03.300 I/AudioFlinger( 2206): Loaded primary audio interface from LEGACY Audio HW HAL (audio)&lt;/P&gt;&lt;P&gt;01-01 00:00:03.300 I/AudioFlinger( 2206): Using 'LEGACY Audio HW HAL' (audio.primary) as the primary audio interface&lt;/P&gt;&lt;P&gt;01-01 00:00:03.300 I/CameraService( 2206): CameraService started (pid=2206)&lt;/P&gt;&lt;P&gt;01-01 00:00:03.310 I/FslCameraHAL( 2206): Face Back Camera is ov5640_mipi, orient is 0&lt;/P&gt;&lt;P&gt;01-01 00:00:03.310 I/FslCameraHAL( 2206): Face Front Camera is ov5642, orient is 0&lt;/P&gt;&lt;P&gt;01-01 00:00:03.320 W/audio_hw_primary( 2206): open output stream devices 2, format 0, channels 0, sample_rate 0&lt;/P&gt;&lt;P&gt;01-01 00:00:03.320 I/AudioFlinger( 2206): AudioFlinger's thread 0xc9488 ready to run&lt;/P&gt;&lt;P&gt;01-01 00:00:03.320 W/AudioFlinger( 2206): Thread AudioOut_1 cannot connect to the power manager service&lt;/P&gt;&lt;P&gt;01-01 00:00:03.320 W/AudioFlinger( 2206): Thread AudioOut_1 cannot connect to the power manager service&lt;/P&gt;&lt;P&gt;01-01 00:00:03.320 W/audio_hw_primary( 2206): out_set_parameters routing=2, ret 1&lt;/P&gt;&lt;P&gt;01-01 00:00:03.320 I/AudioPolicyService( 2206): Loaded audio policy from LEGACY Audio Policy HAL (audio_policy)&lt;/P&gt;&lt;P&gt;01-01 00:00:03.330 W/imx6.gralloc( 2203): 32bpp setting of Framebuffer catched!&lt;/P&gt;&lt;P&gt;01-01 00:00:03.380 W/imx6.gralloc( 2203): using (fd=12)&lt;/P&gt;&lt;P&gt;01-01 00:00:03.380 W/imx6.gralloc( 2203): id&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = DISP3 BG - DI1&lt;/P&gt;&lt;P&gt;01-01 00:00:03.380 W/imx6.gralloc( 2203): xres&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 1024 px&lt;/P&gt;&lt;P&gt;01-01 00:00:03.380 W/imx6.gralloc( 2203): yres&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 768 px&lt;/P&gt;&lt;P&gt;01-01 00:00:03.380 W/imx6.gralloc( 2203): xres_virtual = 1024 px&lt;/P&gt;&lt;P&gt;01-01 00:00:03.380 W/imx6.gralloc( 2203): yres_virtual = 2304 px&lt;/P&gt;&lt;P&gt;01-01 00:00:03.380 W/imx6.gralloc( 2203): bpp&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 32&lt;/P&gt;&lt;P&gt;01-01 00:00:03.380 W/imx6.gralloc( 2203): r&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 16:8&lt;/P&gt;&lt;P&gt;01-01 00:00:03.380 W/imx6.gralloc( 2203): g&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; 8:8&lt;/P&gt;&lt;P&gt;01-01 00:00:03.380 W/imx6.gralloc( 2203): b&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; 0:8&lt;/P&gt;&lt;P&gt;01-01 00:00:03.380 W/imx6.gralloc( 2203): width&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 163 mm (159.568100 dpi)&lt;/P&gt;&lt;P&gt;01-01 00:00:03.380 W/imx6.gralloc( 2203): height&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 122 mm (159.895081 dpi)&lt;/P&gt;&lt;P&gt;01-01 00:00:03.380 W/imx6.gralloc( 2203): refresh rate = 60.00 Hz&lt;/P&gt;&lt;P&gt;01-01 00:00:03.440 D/libEGL&amp;nbsp; ( 2203): loaded /system/lib/egl/libGLES_android.so&lt;/P&gt;&lt;P&gt;01-01 00:00:03.450 D/libEGL&amp;nbsp; ( 2203): loaded /system/lib/egl/libEGL_VIVANTE.so&lt;/P&gt;&lt;P&gt;01-01 00:00:03.480 D/libEGL&amp;nbsp; ( 2203): loaded /system/lib/egl/libGLESv1_CM_VIVANTE.so&lt;/P&gt;&lt;P&gt;01-01 00:00:03.510 D/libEGL&amp;nbsp; ( 2203): loaded /system/lib/egl/libGLESv2_VIVANTE.so&lt;/P&gt;&lt;P&gt;01-01 00:00:03.520 W/SurfaceFlinger( 2203): ro.sf.lcd_density not defined, using 160 dpi by default.&lt;/P&gt;&lt;P&gt;01-01 00:00:03.530 I/SurfaceFlinger( 2203): EGL informations:&lt;/P&gt;&lt;P&gt;01-01 00:00:03.530 I/SurfaceFlinger( 2203): # of configs : 45&lt;/P&gt;&lt;P&gt;01-01 00:00:03.530 I/SurfaceFlinger( 2203): vendor&amp;nbsp;&amp;nbsp;&amp;nbsp; : Vivante Corporation&lt;/P&gt;&lt;P&gt;01-01 00:00:03.530 I/SurfaceFlinger( 2203): version&amp;nbsp;&amp;nbsp; : 1.4&lt;/P&gt;&lt;P&gt;01-01 00:00:03.530 I/SurfaceFlinger( 2203): extensions: EGL_KHR_reusable_sync EGL_KHR_fence_sync EGL_KHR_image_base EGL_KHR_image_pixmap EGL_KHR_image EGL_KHR_gl_textue&lt;/P&gt;&lt;P&gt;01-01 00:00:03.530 I/SurfaceFlinger( 2203): Client API: OpenGL_ES OpenVG&lt;/P&gt;&lt;P&gt;01-01 00:00:03.530 I/SurfaceFlinger( 2203): EGLSurface: 8-8-8-8, config=0xd&lt;/P&gt;&lt;P&gt;01-01 00:00:03.530 I/SurfaceFlinger( 2203): OpenGL informations:&lt;/P&gt;&lt;P&gt;01-01 00:00:03.530 I/SurfaceFlinger( 2203): vendor&amp;nbsp;&amp;nbsp;&amp;nbsp; : Vivante Corporation&lt;/P&gt;&lt;P&gt;01-01 00:00:03.530 I/SurfaceFlinger( 2203): renderer&amp;nbsp; : GC880 Graphics Engine&lt;/P&gt;&lt;P&gt;01-01 00:00:03.530 I/SurfaceFlinger( 2203): version&amp;nbsp;&amp;nbsp; : OpenGL ES-CM 1.1&lt;/P&gt;&lt;P&gt;01-01 00:00:03.530 I/SurfaceFlinger( 2203): extensions: GL_OES_blend_equation_separate GL_OES_blend_func_separate GL_OES_blend_subtract GL_OES_byte_coordinates GL_OES_!&lt;/P&gt;&lt;P&gt; GL_OES_packed_depth_stencil GL_EERROR: v4l2 capture: slave not found!&lt;/P&gt;&lt;P&gt;XT_texture_format_BGRA8888 GL_IMG_read_format GL_IMG_user_clip_plane GL_APPLE_texture_2D_limited_npot GL_EXT_texture_lod_bias GL_EXT_blend_minmax GL_EXT_read_format_bg8&lt;/P&gt;&lt;P&gt;01-01 00:00:03.530 I/SurfaceFlinger( 2203): GL_MAX_TEXTURE_SIZE = 8192&lt;/P&gt;&lt;P&gt;01-01 00:00:03.530 I/SurfaceFlinger( 2203): GL_MAX_VIEWPORT_DIMS = 2048 x 2048&lt;/P&gt;&lt;P&gt;01-01 00:00:03.530 I/SurfaceFlinger( 2203): flags = 00090000&lt;/P&gt;&lt;P&gt;01-01 00:00:03.560 I/v_hwc&amp;nbsp;&amp;nbsp; ( 2203): Vivante HWComposer v2.2&lt;/P&gt;&lt;P&gt;01-01 00:00:03.560 I/v_hwc&amp;nbsp;&amp;nbsp; ( 2203): Device:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x1b4fb90&lt;/P&gt;&lt;P&gt;01-01 00:00:03.560 I/v_hwc&amp;nbsp;&amp;nbsp; ( 2203): Separated 2D:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; YES&lt;/P&gt;&lt;P&gt;01-01 00:00:03.560 I/v_hwc&amp;nbsp;&amp;nbsp; ( 2203): 2D PE20:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; YES&lt;/P&gt;&lt;P&gt;01-01 00:00:03.560 I/v_hwc&amp;nbsp;&amp;nbsp; ( 2203): Filter-stretch blit:&amp;nbsp; YES&lt;/P&gt;&lt;P&gt;01-01 00:00:03.560 I/v_hwc&amp;nbsp;&amp;nbsp; ( 2203): 2D dither enabled :&amp;nbsp;&amp;nbsp; YES&lt;/P&gt;&lt;P&gt;01-01 00:00:03.560 I/v_hwc&amp;nbsp;&amp;nbsp; ( 2203): Multi-source blit:&amp;nbsp;&amp;nbsp;&amp;nbsp; NO&lt;/P&gt;&lt;P&gt;01-01 00:00:03.560 I/v_hwc&amp;nbsp;&amp;nbsp; ( 2203): Multi-source blit Ex: NO&lt;/P&gt;&lt;P&gt;01-01 00:00:03.560 I/v_hwc&amp;nbsp;&amp;nbsp; ( 2203): OPF/YUV blit/Tiling : NO&lt;/P&gt;&lt;P&gt;01-01 00:00:03.650 D/libEGL&amp;nbsp; ( 2286): loaded /system/lib/egl/libGLES_android.so&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I need to apply some patch and rebuild the android kernel in order to get the external camera working..?&lt;/P&gt;&lt;P&gt;Can anybody help me getting this issue resolved. I am working on an android video calling application and hence, need the usb camera to work on the development platform.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Sumit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Feb 2014 09:49:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/can-t-connect-to-the-camera/m-p/266454#M27816</guid>
      <dc:creator>sumitsinha</dc:creator>
      <dc:date>2014-02-28T09:49:39Z</dc:date>
    </item>
    <item>
      <title>Re: can't connect to the camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/can-t-connect-to-the-camera/m-p/266455#M27817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Sumit&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to modified the init.rc file to add a support for the UVC camera. After that you can able to used USB camera.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Feb 2014 09:57:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/can-t-connect-to-the-camera/m-p/266455#M27817</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-02-28T09:57:59Z</dc:date>
    </item>
    <item>
      <title>Re: can't connect to the camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/can-t-connect-to-the-camera/m-p/266456#M27818</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Saurabh,&lt;/P&gt;&lt;P&gt;Thanks for the reply. &lt;/P&gt;&lt;P&gt;Could you please elaborate a bit on your answer. &lt;/P&gt;&lt;P&gt;I do see the init.rc file. However, I am not sure what modifications need to be done in order to get the uvc camera working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Sumit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Feb 2014 10:38:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/can-t-connect-to-the-camera/m-p/266456#M27818</guid>
      <dc:creator>sumitsinha</dc:creator>
      <dc:date>2014-02-28T10:38:50Z</dc:date>
    </item>
    <item>
      <title>Re: can't connect to the camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/can-t-connect-to-the-camera/m-p/266457#M27819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Sumit&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;open&amp;nbsp; device\fsl\"you device folder"\init.c.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For imx6q this path will be device\fsl\sabresd_6dq\init.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;replace&amp;nbsp; ov5640_mipi by uvc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;setprop back_camera_name uvc&lt;/P&gt;&lt;P&gt;setprop back_camera_orient 0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Feb 2014 11:17:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/can-t-connect-to-the-camera/m-p/266457#M27819</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-02-28T11:17:10Z</dc:date>
    </item>
    <item>
      <title>Re: can't connect to the camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/can-t-connect-to-the-camera/m-p/266458#M27820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Saurabh,&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;Yes, you are correct. I did go through the Android Advanced User Guide which came with the android release package and found that it has a separate section for USB Camera support which talks about the modifications you suggested and plus few others as well.&lt;/P&gt;&lt;P&gt;I will update the status once I have tried it out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Sumit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Mar 2014 06:40:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/can-t-connect-to-the-camera/m-p/266458#M27820</guid>
      <dc:creator>sumitsinha</dc:creator>
      <dc:date>2014-03-01T06:40:05Z</dc:date>
    </item>
  </channel>
</rss>