<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: several questions about IPU's DI in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/several-questions-about-IPU-s-DI/m-p/266116#M27697</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For Q1: &lt;BR /&gt;DISP0_CNTRST was not used in current BSP, this pin was designed to control the backlight, but in current BSP, the PWM pin was used for backlight.&lt;BR /&gt;DISP0_DRDY is DE(Display Data Enable)&lt;BR /&gt;DISP0_PIN2 is used as HSYNC, DISP0_PIN3 as vsync, DISP0_PIN15 as DISP0_DRDY. For VSYNC, HSYNC and DRDY, they are configable, but in current BSP, they are hardcoded to PIN2, PIN3 and PIN15. For how to change the DI PIN number, you can reference to &lt;A _jive_internal="true" href="https://community.nxp.com/thread/279078"&gt;https://community.freescale.com/thread/279078&lt;/A&gt;.&lt;BR /&gt;By the way, if you are not familiar with IPU, we don't suggest you to modify the display DI pin usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Q2:&lt;BR /&gt;Yes, the dual display use case is OK, the two DIs can work at the same time. It can support two parallel RGB LCD panels; or one LCD + one HDMI; or one LCD + one LVDS; or one HDMI + one LVDS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Q3:&lt;BR /&gt;The DI is also the source for HDMI and LVDS. For dual display case, it was answered in Q2.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Sep 2013 06:25:03 GMT</pubDate>
    <dc:creator>qiang_li-mpu_se</dc:creator>
    <dc:date>2013-09-09T06:25:03Z</dc:date>
    <item>
      <title>several questions about IPU's DI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/several-questions-about-IPU-s-DI/m-p/266115#M27696</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,I like this forum!&lt;/P&gt;&lt;P&gt;here are some questions about IPU's DI:&lt;/P&gt;&lt;P&gt;1:According to the Sabre&amp;nbsp; reference design ,thers is one parallel RGB displasy interface including&amp;nbsp; DISP0_DATA(23..0), DISP0_CLK,DISP0_HSYNC,DISP0_VSYNC,DISP0_CNTRST,DISP0_DRDY.What's the meaning of DISP0_CNTRST and DISP0_DRDY?Should&amp;nbsp; I use&amp;nbsp; DISP0_DRDY as&amp;nbsp; data_en?and what does&amp;nbsp; DISP0_CNTRST mean? can i make the pin DI0_PIN4 which mapped to DISP0_CNTRST unconnected?&lt;/P&gt;&lt;P&gt;DISP0_PIN2 is used as HSYNC,DISP0_PIN3 as vsync, DISP0_PIN15 as DISP0_DRDY, why these pins should be conntected like this? is PIN2 mapped to Hsync in imx6q?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.Is it possibel to make two channel display work at the same time? for example,connect the IPU1's two DI to external display devices, Are there any other choices? Can hdmi and lvds interface work at the same time, not in&amp;nbsp; the time sharing mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3,what is the soruce of HDMI and LVDS interface? is it IPU's DI? if the answer is YES,then is it impossible to use LVDS or HDMI&amp;nbsp; and DI''s parallel RGB at the same time?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jul 2013 06:38:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/several-questions-about-IPU-s-DI/m-p/266115#M27696</guid>
      <dc:creator>gaoweilin</dc:creator>
      <dc:date>2013-07-11T06:38:44Z</dc:date>
    </item>
    <item>
      <title>Re: several questions about IPU's DI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/several-questions-about-IPU-s-DI/m-p/266116#M27697</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For Q1: &lt;BR /&gt;DISP0_CNTRST was not used in current BSP, this pin was designed to control the backlight, but in current BSP, the PWM pin was used for backlight.&lt;BR /&gt;DISP0_DRDY is DE(Display Data Enable)&lt;BR /&gt;DISP0_PIN2 is used as HSYNC, DISP0_PIN3 as vsync, DISP0_PIN15 as DISP0_DRDY. For VSYNC, HSYNC and DRDY, they are configable, but in current BSP, they are hardcoded to PIN2, PIN3 and PIN15. For how to change the DI PIN number, you can reference to &lt;A _jive_internal="true" href="https://community.nxp.com/thread/279078"&gt;https://community.freescale.com/thread/279078&lt;/A&gt;.&lt;BR /&gt;By the way, if you are not familiar with IPU, we don't suggest you to modify the display DI pin usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Q2:&lt;BR /&gt;Yes, the dual display use case is OK, the two DIs can work at the same time. It can support two parallel RGB LCD panels; or one LCD + one HDMI; or one LCD + one LVDS; or one HDMI + one LVDS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Q3:&lt;BR /&gt;The DI is also the source for HDMI and LVDS. For dual display case, it was answered in Q2.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2013 06:25:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/several-questions-about-IPU-s-DI/m-p/266116#M27697</guid>
      <dc:creator>qiang_li-mpu_se</dc:creator>
      <dc:date>2013-09-09T06:25:03Z</dc:date>
    </item>
  </channel>
</rss>