<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: dual camera work at the same time</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/dual-camera-work-at-the-same-time/m-p/265431#M27520</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Henri, were you able to achieve side by side display?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 May 2015 19:33:48 GMT</pubDate>
    <dc:creator>nmak</dc:creator>
    <dc:date>2015-05-22T19:33:48Z</dc:date>
    <item>
      <title>dual camera work at the same time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/dual-camera-work-at-the-same-time/m-p/265426#M27515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&amp;nbsp; guys&lt;/P&gt;&lt;P&gt;&amp;nbsp; i read the imx53 rm .it says &lt;/P&gt;&lt;P&gt;Several sensors can be connected to each of the CSIs. Simultaneous functionality&lt;/P&gt;&lt;P&gt;(sending data) is supported as follows:&lt;/P&gt;&lt;P&gt;• Two sensors can send data independently, each through a different port.&lt;/P&gt;&lt;P&gt;• Only one of the streams can be transferred to the VDIC or IC for on-the-fly&lt;/P&gt;&lt;P&gt;processing, while the other one is sent directly to system memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i do not understand what does on the fly processing&amp;nbsp; and sent directly to system menmory means&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;does it mean&amp;nbsp; when two sensor work at the same time&amp;nbsp; the preview image&amp;nbsp; one is sent to the lcd display device&amp;nbsp;&amp;nbsp; the other is sent to memory&lt;/P&gt;&lt;P&gt; can i&amp;nbsp; save both of them at the same time&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Forion&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2013 02:06:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/dual-camera-work-at-the-same-time/m-p/265426#M27515</guid>
      <dc:creator>ff</dc:creator>
      <dc:date>2013-02-20T02:06:48Z</dc:date>
    </item>
    <item>
      <title>Re: dual camera work at the same time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/dual-camera-work-at-the-same-time/m-p/265427#M27516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm also very interested to get this working. I have modified mxc_v4l2_capture driver in kernel 2.6.35 to support both CSI's, and they work OK when running separately (CSI0 as overlay and CSI1 as capture). But dual playback does not work, I get "IPU Error - IPU_INT_STAT_10 = 0x01000000" and "0x00000002". I've tried to run capture also in "bypass IC" mode but even then I couldn't get it working.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Feb 2013 08:07:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/dual-camera-work-at-the-same-time/m-p/265427#M27516</guid>
      <dc:creator>henri_bragge</dc:creator>
      <dc:date>2013-02-25T08:07:26Z</dc:date>
    </item>
    <item>
      <title>Re: dual camera work at the same time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/dual-camera-work-at-the-same-time/m-p/265428#M27517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; For iMX53 BSP, it only supports one V4L2 output device and only one ouput can be used at the same time, so you will fail to preview the two camera at the same time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can try to render the two preview with ipu lib and screenlayer lib, the sample code can be found at the unit test package such as "imx-test-11.09.01.tar.gz", the mxc_ipudev_test.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; For iMX6 BSP, it supports more V4l2 output device to support multi-camera.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Feb 2013 02:11:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/dual-camera-work-at-the-same-time/m-p/265428#M27517</guid>
      <dc:creator>qiang_li-mpu_se</dc:creator>
      <dc:date>2013-02-28T02:11:04Z</dc:date>
    </item>
    <item>
      <title>Re: dual camera work at the same time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/dual-camera-work-at-the-same-time/m-p/265429#M27518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for helpful answer. I've not gotten to the output part yet, because I cannot even capture yet. I tried CSI-&amp;gt;MEM path for CSI0/1 simultaneously, and I can only get frames (/interrupts) from both if I do not register any synchronous framebuffers. If I register, then I can only get frames from one CSI at a time. So possibly some framebuffer resources (DP/DC/DMFC) are conflicting with dual CSI-&amp;gt;MEM path (or I need one framebuffer per CSI), any ideas how I could overcome that?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Mar 2013 08:42:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/dual-camera-work-at-the-same-time/m-p/265429#M27518</guid>
      <dc:creator>henri_bragge</dc:creator>
      <dc:date>2013-03-01T08:42:53Z</dc:date>
    </item>
    <item>
      <title>Re: dual camera work at the same time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/dual-camera-work-at-the-same-time/m-p/265430#M27519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was able to overcome the capture problem (I had two bugs: local_buf_num was global instead of per-CSI in mxc_v4l2_capture.c and CSI_MEM1/IRQ1 was used instead of CSI_MEM2/IRQ2 for CSI1 in ipu_csi_enc.c).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Next I would need to somehow show them side by side. Any idea if I could use DP for combining or if I need to accomplish that in SW? Guess I need to check the ipu and screenlayer libs you mentioned.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Mar 2013 07:27:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/dual-camera-work-at-the-same-time/m-p/265430#M27519</guid>
      <dc:creator>henri_bragge</dc:creator>
      <dc:date>2013-03-05T07:27:50Z</dc:date>
    </item>
    <item>
      <title>Re: dual camera work at the same time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/dual-camera-work-at-the-same-time/m-p/265431#M27520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Henri, were you able to achieve side by side display?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2015 19:33:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/dual-camera-work-at-the-same-time/m-p/265431#M27520</guid>
      <dc:creator>nmak</dc:creator>
      <dc:date>2015-05-22T19:33:48Z</dc:date>
    </item>
  </channel>
</rss>