<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX53 display</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-display/m-p/265363#M27503</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am doing a project will use &lt;SPAN class="seohtagbold"&gt;MCIMX537CVV8B, display will use KOE RGB TX09D40VM3CBA. The LCD dot clk type is 5.6MHz. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="seohtagbold"&gt;I want to know if the CPU could generate the required clock for LCD or need external frequency divider?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="seohtagbold"&gt;Could LCD signal Hsync Vsync DOTCLK connect to CPU directly or need external CPLD? if have any timing sequency issue?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="seohtagbold"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="seohtagbold"&gt;Thanks!&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="seohtagbold"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="seohtagbold"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 05 Oct 2013 11:08:33 GMT</pubDate>
    <dc:creator>lilyliu</dc:creator>
    <dc:date>2013-10-05T11:08:33Z</dc:date>
    <item>
      <title>iMX53 display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-display/m-p/265363#M27503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am doing a project will use &lt;SPAN class="seohtagbold"&gt;MCIMX537CVV8B, display will use KOE RGB TX09D40VM3CBA. The LCD dot clk type is 5.6MHz. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="seohtagbold"&gt;I want to know if the CPU could generate the required clock for LCD or need external frequency divider?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="seohtagbold"&gt;Could LCD signal Hsync Vsync DOTCLK connect to CPU directly or need external CPLD? if have any timing sequency issue?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="seohtagbold"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="seohtagbold"&gt;Thanks!&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="seohtagbold"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="seohtagbold"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Oct 2013 11:08:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX53-display/m-p/265363#M27503</guid>
      <dc:creator>lilyliu</dc:creator>
      <dc:date>2013-10-05T11:08:33Z</dc:date>
    </item>
    <item>
      <title>Re: iMX53 display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-display/m-p/265364#M27504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is a normal RGB interface LCD panel, MX53 can support it directly without external Timing controller (CPLD).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2013 07:02:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX53-display/m-p/265364#M27504</guid>
      <dc:creator>aven_tsao</dc:creator>
      <dc:date>2013-12-09T07:02:03Z</dc:date>
    </item>
  </channel>
</rss>