<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMMPF0100 how to enter OFF mode</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-how-to-enter-OFF-mode/m-p/265258#M27485</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We've developed a custom board with IMX6D and MMPF0100 (default version) and are running a yocto custom build. We have a problem with power off mode, we can't enter it. We're not interested in sleep or standby etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The datasheet for MMPF0100 states that if PWRON is set low and SWxOMODE bits are not set, OFF mode should be entered, however the voltages (SW1-4 and VGEN1-6) won't shut off so I assume sleep is entered. However I am seeing some weird behavior in SW2, namely it alternates between 1.8V and 2.2V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The power button is connected to the CPU and I see no difference between "shutdown -h 0" and just asserting the power button for &amp;gt;4s.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Aug 2013 07:26:40 GMT</pubDate>
    <dc:creator>peterhygren</dc:creator>
    <dc:date>2013-08-20T07:26:40Z</dc:date>
    <item>
      <title>MMPF0100 how to enter OFF mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-how-to-enter-OFF-mode/m-p/265258#M27485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We've developed a custom board with IMX6D and MMPF0100 (default version) and are running a yocto custom build. We have a problem with power off mode, we can't enter it. We're not interested in sleep or standby etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The datasheet for MMPF0100 states that if PWRON is set low and SWxOMODE bits are not set, OFF mode should be entered, however the voltages (SW1-4 and VGEN1-6) won't shut off so I assume sleep is entered. However I am seeing some weird behavior in SW2, namely it alternates between 1.8V and 2.2V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The power button is connected to the CPU and I see no difference between "shutdown -h 0" and just asserting the power button for &amp;gt;4s.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Aug 2013 07:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-how-to-enter-OFF-mode/m-p/265258#M27485</guid>
      <dc:creator>peterhygren</dc:creator>
      <dc:date>2013-08-20T07:26:40Z</dc:date>
    </item>
  </channel>
</rss>