<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMX6 encoding SXGA</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX6-encoding-SXGA/m-p/264455#M27240</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could someone tell me if encoding an SXGA via CSI port is possible at 60 fps? I saw another post that indicated that it would not be possible at that frame rate, but running the VPU at 266 MHZ. What about running it at 350 MHZ? Could it be possible then to encode that resolution at 60 fps?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Feb 2014 15:18:07 GMT</pubDate>
    <dc:creator>timothybean</dc:creator>
    <dc:date>2014-02-27T15:18:07Z</dc:date>
    <item>
      <title>MX6 encoding SXGA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6-encoding-SXGA/m-p/264455#M27240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could someone tell me if encoding an SXGA via CSI port is possible at 60 fps? I saw another post that indicated that it would not be possible at that frame rate, but running the VPU at 266 MHZ. What about running it at 350 MHZ? Could it be possible then to encode that resolution at 60 fps?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2014 15:18:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6-encoding-SXGA/m-p/264455#M27240</guid>
      <dc:creator>timothybean</dc:creator>
      <dc:date>2014-02-27T15:18:07Z</dc:date>
    </item>
    <item>
      <title>Re: MX6 encoding SXGA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6-encoding-SXGA/m-p/264456#M27241</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;it depends what data format you use, if the number of cycles needed to send a single pixel is one, yes mx6 IPU can support it, for more detailed information, you can refer to the chapter 37.1.2.1.1 Camera Ports of Reference Manual, the formula is:&lt;/P&gt;&lt;P&gt;F = FH * FW * FPS * BI * DF&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Mar 2014 09:10:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6-encoding-SXGA/m-p/264456#M27241</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2014-03-05T09:10:11Z</dc:date>
    </item>
  </channel>
</rss>