<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックI.Mx SDRAM interfacing</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-Mx-SDRAM-interfacing/m-p/158216#M2718</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the MX53SUG.pdf the explanation for DDR_INPUT field in the IOMUX chapter is this,&lt;/P&gt;&lt;P&gt;"DDR_INPUT (1 bit ddr_input control)—Needed when interfacing DDR memories."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But nowhere it is mentioned whether or not to enable this bit? And to which pins this should be enabled?&lt;/P&gt;&lt;P&gt;Any ideas on what is the CMOS input mode and Differential input mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 May 2012 06:40:52 GMT</pubDate>
    <dc:creator>positron</dc:creator>
    <dc:date>2012-05-02T06:40:52Z</dc:date>
    <item>
      <title>I.Mx SDRAM interfacing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-Mx-SDRAM-interfacing/m-p/158216#M2718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the MX53SUG.pdf the explanation for DDR_INPUT field in the IOMUX chapter is this,&lt;/P&gt;&lt;P&gt;"DDR_INPUT (1 bit ddr_input control)—Needed when interfacing DDR memories."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But nowhere it is mentioned whether or not to enable this bit? And to which pins this should be enabled?&lt;/P&gt;&lt;P&gt;Any ideas on what is the CMOS input mode and Differential input mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 May 2012 06:40:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-Mx-SDRAM-interfacing/m-p/158216#M2718</guid>
      <dc:creator>positron</dc:creator>
      <dc:date>2012-05-02T06:40:52Z</dc:date>
    </item>
  </channel>
</rss>