<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Intermittent Boot problems on SD booting IMX53 QSB-R board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Intermittent-Boot-problems-on-SD-booting-IMX53-QSB-R-board/m-p/158153#M2709</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have seen something similar with i.MX53 SABRE-AI board. Sometimes (like 1/2 or 1/3 of times) when I plug in the power cable, power leds turn on but I get no output on U-boot whatsoever (when booting from SD). Booting from NAND works every time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 May 2012 13:36:13 GMT</pubDate>
    <dc:creator>HenriBragge</dc:creator>
    <dc:date>2012-05-02T13:36:13Z</dc:date>
    <item>
      <title>Intermittent Boot problems on SD booting IMX53 QSB-R board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Intermittent-Boot-problems-on-SD-booting-IMX53-QSB-R-board/m-p/158152#M2708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Folks,&lt;/P&gt;&lt;P&gt;I have been working through an issue with the imx53&amp;nbsp;kernel boot sequence.&amp;nbsp; The following occurs.&amp;nbsp; I have an IMX53-QSB-R board (Several in fact) that when the power has been off for more than a few minutes the kernel will fail to mount the&amp;nbsp;sdcard &amp;nbsp;file system.&amp;nbsp; The power on&amp;nbsp;boot sequence is:&amp;nbsp; U-boot starts and loads the&amp;nbsp;kernel successfully from the SD card.&amp;nbsp; The kernel begins to load drivers&amp;nbsp;and then&amp;nbsp;when it gets to&amp;nbsp;mounting the android file systems&amp;nbsp;the mounts&amp;nbsp;fail&amp;nbsp;with a mmc0:&amp;nbsp;error -110 initialising mmc card.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If&amp;nbsp;I cycle the power one more time&amp;nbsp;everything boots just&amp;nbsp;fine.&amp;nbsp; I have some imx53 boards that&amp;nbsp;boot fine every time and I&amp;nbsp;have some that&amp;nbsp;exhibit the&amp;nbsp;this strange behavior.&amp;nbsp; I am using the latest adeno Android bsp.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I dug down into the mmc driver and&amp;nbsp;the timeout&amp;nbsp;seems to be occuring when the&amp;nbsp;cid command is being sent to the mmc interface&amp;nbsp;at probing.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone have any ideas on this one. I have searched and searched and I have not found&amp;nbsp;solutions.&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;P&gt;Jeff&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2012 21:24:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Intermittent-Boot-problems-on-SD-booting-IMX53-QSB-R-board/m-p/158152#M2708</guid>
      <dc:creator>JeffBallif</dc:creator>
      <dc:date>2012-04-30T21:24:02Z</dc:date>
    </item>
    <item>
      <title>Re: Intermittent Boot problems on SD booting IMX53 QSB-R board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Intermittent-Boot-problems-on-SD-booting-IMX53-QSB-R-board/m-p/158153#M2709</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have seen something similar with i.MX53 SABRE-AI board. Sometimes (like 1/2 or 1/3 of times) when I plug in the power cable, power leds turn on but I get no output on U-boot whatsoever (when booting from SD). Booting from NAND works every time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 May 2012 13:36:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Intermittent-Boot-problems-on-SD-booting-IMX53-QSB-R-board/m-p/158153#M2709</guid>
      <dc:creator>HenriBragge</dc:creator>
      <dc:date>2012-05-02T13:36:13Z</dc:date>
    </item>
    <item>
      <title>Re: Intermittent Boot problems on SD booting IMX53 QSB-R board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Intermittent-Boot-problems-on-SD-booting-IMX53-QSB-R-board/m-p/158154#M2710</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Henri,&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;More data on the intermittent boot up.&amp;nbsp; U-boot boots from the SD card everytime just fine on all of my quick start boards. *( I currently have 20 of them running).&amp;nbsp; I have never seen U-boot fail.&amp;nbsp; After a lot more investigation it seems that the problem only occurs where there is some data on Partition 6 of the SD card.&amp;nbsp; The same machine with a very small amount of data on the SD card will boot everytime. But once I add about 3Meg of data to the card in seperate files the mmc card will not be recognized in the the linux/Android boot process and the boot will fail.&lt;/P&gt;&lt;P&gt;When the failure happens the services in&amp;nbsp;init.rc will not start.&amp;nbsp;The files can't be found.&amp;nbsp;From the boot log it looks like there is a race condition in the boot process.&amp;nbsp; The mmc timeout error always happens after init.rc tries to open files on the SD card.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 May 2012 16:08:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Intermittent-Boot-problems-on-SD-booting-IMX53-QSB-R-board/m-p/158154#M2710</guid>
      <dc:creator>JeffBallif</dc:creator>
      <dc:date>2012-05-02T16:08:02Z</dc:date>
    </item>
  </channel>
</rss>