<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6Q : using OpenGL 2 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-using-OpenGL-2/m-p/263942#M27056</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On Xorg log file I have the folowing traces :&lt;/P&gt;&lt;P&gt;drmOpenDevice : node name is /dev/dri/card0&lt;/P&gt;&lt;P&gt;[drm] failed to load kernel module "vivante"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no directory "/dev/dri". According to Ubuntu Software Center the installed vivante driver is "gpu-viv-ubt0 12.11.01.oneiric.MX6DQ.post GA.RC3"&lt;/P&gt;&lt;P&gt;What I have to install to allow running GL2 applications.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Apr 2013 13:50:57 GMT</pubDate>
    <dc:creator>mimeline</dc:creator>
    <dc:date>2013-04-18T13:50:57Z</dc:date>
    <item>
      <title>i.MX6Q : using OpenGL 2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-using-OpenGL-2/m-p/263940#M27054</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How can I launch my OpenGL 2 application ? I have a GLException at the OpenGL context creation. The GL2 seems to be unavailable.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Apr 2013 11:42:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-using-OpenGL-2/m-p/263940#M27054</guid>
      <dc:creator>mimeline</dc:creator>
      <dc:date>2013-04-12T11:42:13Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q : using OpenGL 2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-using-OpenGL-2/m-p/263941#M27055</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can run glxgears, before that chek whether the DRI is setup correctly&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/320024#320024"&gt;https://community.freescale.com/message/320024#320024&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Apr 2013 13:59:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-using-OpenGL-2/m-p/263941#M27055</guid>
      <dc:creator>PrabhuSundarara</dc:creator>
      <dc:date>2013-04-12T13:59:12Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q : using OpenGL 2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-using-OpenGL-2/m-p/263942#M27056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On Xorg log file I have the folowing traces :&lt;/P&gt;&lt;P&gt;drmOpenDevice : node name is /dev/dri/card0&lt;/P&gt;&lt;P&gt;[drm] failed to load kernel module "vivante"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no directory "/dev/dri". According to Ubuntu Software Center the installed vivante driver is "gpu-viv-ubt0 12.11.01.oneiric.MX6DQ.post GA.RC3"&lt;/P&gt;&lt;P&gt;What I have to install to allow running GL2 applications.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Apr 2013 13:50:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-using-OpenGL-2/m-p/263942#M27056</guid>
      <dc:creator>mimeline</dc:creator>
      <dc:date>2013-04-18T13:50:57Z</dc:date>
    </item>
  </channel>
</rss>