<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX6Solo Linux patch for development board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Solo-Linux-patch-for-development-board/m-p/263796#M27032</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using the iMX6Solo/DualLite SABRE development board for smart devices. At the moment I am aiming for a system with iMX6Solo and not DualLite. On your homepage there exists a patch that is used to disable one core, thus emulating a iMX6Solo. I do get a little bit puzzled by this patch however since it seems like it reduces max RAM memory size to 512 MB. Is this the maximum RAM size for a iMX6Solo system? If not, why is it reduced to 512Mb in this patch?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Emil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Apr 2013 08:32:09 GMT</pubDate>
    <dc:creator>emil</dc:creator>
    <dc:date>2013-04-12T08:32:09Z</dc:date>
    <item>
      <title>iMX6Solo Linux patch for development board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Solo-Linux-patch-for-development-board/m-p/263796#M27032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using the iMX6Solo/DualLite SABRE development board for smart devices. At the moment I am aiming for a system with iMX6Solo and not DualLite. On your homepage there exists a patch that is used to disable one core, thus emulating a iMX6Solo. I do get a little bit puzzled by this patch however since it seems like it reduces max RAM memory size to 512 MB. Is this the maximum RAM size for a iMX6Solo system? If not, why is it reduced to 512Mb in this patch?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Emil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Apr 2013 08:32:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Solo-Linux-patch-for-development-board/m-p/263796#M27032</guid>
      <dc:creator>emil</dc:creator>
      <dc:date>2013-04-12T08:32:09Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Solo Linux patch for development board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Solo-Linux-patch-for-development-board/m-p/263797#M27033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Emil,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6DualLite and Solo SABRE SD share the same HW evaluation board.&lt;/P&gt;&lt;P&gt;i.MX6 Dualite has up to &lt;STRONG&gt;64-bit&lt;/STRONG&gt; DDR interface and i.MX6 Solo has up to &lt;STRONG&gt;32-bit&lt;/STRONG&gt; DDR interface.&lt;/P&gt;&lt;P&gt;If you emulate an i.MX6 Solo on a Dualite SABRE SD board, you'll be forced to use half of the DDR packages of the board as you'll only have a 32-bit DDR interface (instead of 64-bit) consequently you'll divide the memory size of the board by 2.&lt;/P&gt;&lt;P&gt;Anyway 512MB is not the max DDR size of i.MX6 Solo (4GB max).&lt;/P&gt;&lt;P&gt;Application note AN4397 explains that: &lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4397.pdf?fpsp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4397.pdf?fpsp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bixente&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Apr 2013 10:00:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Solo-Linux-patch-for-development-board/m-p/263797#M27033</guid>
      <dc:creator>Aubineau_FAE</dc:creator>
      <dc:date>2013-04-12T10:00:43Z</dc:date>
    </item>
  </channel>
</rss>