<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6Q Sabre SD kernel boot crash in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Sabre-SD-kernel-boot-crash/m-p/263547#M26980</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just tried with the NFS filesystem provided in the ga_image package and both my kernel and the official kernel works fine, as long as I use the u-boot image provided with the 4.2.2-1.1.0-ga_image package. If I use the u-boot on the original SD Card (R13.4.1 ICS) I get the abort soon in the kernel boot as explained in my first post.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So there is at least two differences between the two u-boot versions:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Some initializations are different, thus the newe kernels can't boot from a board initialized by the older u-boot&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The new u-boot REFUSES to save the "botcmd" environment variable: I can change and save the content of ANY variable EXCEPT bootcmd&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I think that is VERY unconvenient! I will look at the u-boot source code to try to understand what happens;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I wonder if the variable is saved correctly but overwritten at u-boot start...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The kernel stop I noticed after the "Freeing init memory: 244K" message seems to be caused by the root filesystem; however I still have to understand what as different between the released NFS image and the one I constructed, but I have some ideas about that an shoud be able to solve that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will post again when everything works and I was able to correct the u-boot behavior.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 24 Aug 2013 11:25:54 GMT</pubDate>
    <dc:creator>BernardDAUTREVA</dc:creator>
    <dc:date>2013-08-24T11:25:54Z</dc:date>
    <item>
      <title>i.MX6Q Sabre SD kernel boot crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Sabre-SD-kernel-boot-crash/m-p/263543#M26976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a problem with the latest Android JB distribution (jb4.2.2_1.1.0-ga) compiled on Ubuntu 12.04.&lt;/P&gt;&lt;P&gt;I can compiled everything without problem, but when I try to boot the Linux kernel, it crashes and resets the board with an audible "click".&lt;/P&gt;&lt;P&gt;The Android ICS version provided on teh SD-card, of course, works flawlessly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note however that I got the same behaviour (kernel boot aborting with a "click") when i Use a 5V-1A powersupply instead of the 5V-5A supply provided with the board; I then check and see that the board is using up to about 2A when the kernel is booting, probably when switching on the various peripherals, but I can't reproduce it right now (I don't have the proper poser supply here).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope someone will have ideas on how I could at least work around this. I've heard someone talking about suppressing kernel power management but&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1) I don't see how (there is very few PM-related config options in menuconfig)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2) I'm afraid this could break havoc in Android...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the log of the kernel boot:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;## Booting kernel from Legacy Image at 10800000 ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; Linux-3.0.35-06126-g0f2d6ad-dirt&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; ARM Linux Kernel Image (uncompressed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 4766036 Bytes =&amp;nbsp; 4.5 MB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Load Address: 10008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 10008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Loading Kernel Image ... OK&lt;/P&gt;&lt;P&gt;OK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Uncompressing Linux... done, booting the kernel.&lt;/P&gt;&lt;P&gt;Initializing cgroup subsys cpu&lt;/P&gt;&lt;P&gt;Linux version 3.0.35-06126-g0f2d6ad-dirty (dautrevaux@coLinux) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #21 SMP PREEMPT Mon Aug 19 18:06:26 CEST 2013&lt;/P&gt;&lt;P&gt;CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d&lt;/P&gt;&lt;P&gt;CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;/P&gt;&lt;P&gt;Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board&lt;/P&gt;&lt;P&gt;Ignoring unrecognised tag 0x54410008&lt;/P&gt;&lt;P&gt;Memory policy: ECC disabled, Data cache writealloc&lt;/P&gt;&lt;P&gt;CPU identified as i.MX6Q, silicon rev 1.2&lt;/P&gt;&lt;P&gt;PERCPU: Embedded 7 pages/cpu @c1325000 s6592 r8192 d13888 u32768&lt;/P&gt;&lt;P&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 208128&lt;/P&gt;&lt;P&gt;Kernel command line: init=/init androidboot.console=ttymxc0 console=ttymxc0,115200n8 ip=192.168.233.128:192.168.233.1:192.168.233.1:255.255.255.0:sabresd_6dq:eth0:off fbmem=10M vmalloc=400M root=/dev/nfs nfsroot=192.168.233.1:/tftpboot/rootfs-sabresd_6dq&lt;/P&gt;&lt;P&gt;PID hash table entries: 2048 (order: 1, 8192 bytes)&lt;/P&gt;&lt;P&gt;Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;/P&gt;&lt;P&gt;Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;/P&gt;&lt;P&gt;Memory: 767MB 54MB = 821MB total&lt;/P&gt;&lt;P&gt;Memory: 820576k/820576k available, 228000k reserved, 431104K highmem&lt;/P&gt;&lt;P&gt;Virtual kernel memory layout:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vector&amp;nbsp; : 0xffff0000 - 0xffff1000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 4 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fixmap&amp;nbsp; : 0xfff00000 - 0xfffe0000&amp;nbsp;&amp;nbsp; ( 896 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0xfbe00000 - 0xffe00000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 64 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmalloc : 0xd9800000 - 0xf2000000&amp;nbsp;&amp;nbsp; ( 392 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; lowmem&amp;nbsp; : 0xc0000000 - 0xd9000000&amp;nbsp;&amp;nbsp; ( 400 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pkmap&amp;nbsp;&amp;nbsp; : 0xbfe00000 - 0xc0000000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 2 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; modules : 0xbf000000 - 0xbfe00000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 14 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .init : 0xc0008000 - 0xc0045000&amp;nbsp;&amp;nbsp; ( 244 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0xc0045000 - 0xc08fa938&amp;nbsp;&amp;nbsp; (8919 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0xc08fc000 - 0xc0993be0&amp;nbsp;&amp;nbsp; ( 607 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bss : 0xc0993c04 - 0xc0b1b948&amp;nbsp;&amp;nbsp; (1568 kB)&lt;/P&gt;&lt;P&gt;Preemptible hierarchical RCU implementation.&lt;/P&gt;&lt;P&gt;NR_IRQS:624&lt;/P&gt;&lt;P&gt;MXC GPIO hardware&lt;/P&gt;&lt;P&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms&lt;/P&gt;&lt;P&gt;arm_max_freq=1GHz&lt;/P&gt;&lt;P&gt;MXC_Early serial console at MMIO 0x2020000 (options '115200n8')&lt;/P&gt;&lt;P&gt;bootconsole [ttymxc0] enabled&lt;/P&gt;&lt;P&gt;Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)&lt;/P&gt;&lt;P&gt;pid_max: default: 32768 minimum: 301&lt;/P&gt;&lt;P&gt;Mount-cache hash table entries: 512&lt;/P&gt;&lt;P&gt;Initializing cgroup subsys debug&lt;/P&gt;&lt;P&gt;Initializing cgroup subsys cpuacct&lt;/P&gt;&lt;P&gt;Initializing cgroup subsys freezer&lt;/P&gt;&lt;P&gt;CPU: Testing write buffer coherency: ok&lt;/P&gt;&lt;P&gt;hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available&lt;/P&gt;&lt;P&gt;CPU1: Booted secondary processor&lt;/P&gt;&lt;P&gt;CPU2: Booted secondary processor&lt;/P&gt;&lt;P&gt;CPU3: Booted secondary processor&lt;/P&gt;&lt;P&gt;Brought up 4 CPUs&lt;/P&gt;&lt;P&gt;SMP: Total of 4 processors activated (6324.22 BogoMIPS).&lt;/P&gt;&lt;P&gt;print_constraints: dummy:&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 16&lt;/P&gt;&lt;P&gt;print_constraints: vddpu: 725 &amp;lt;--&amp;gt; 1300 mV at 1100 mV fast normal&lt;/P&gt;&lt;P&gt;print_constraints: vddcore: 725 &amp;lt;--&amp;gt; 1300 mV at 1100 mV fast normal&lt;/P&gt;&lt;P&gt;print_constraints: vddsoc: 725 &amp;lt;--&amp;gt; 1300 mV at 1200 mV fast normal&lt;/P&gt;&lt;P&gt;print_constraints: vdd2p5: 2000 &amp;lt;--&amp;gt; 2775 mV at 2400 mV fast normal&lt;/P&gt;&lt;P&gt;print_constraints: vdd1p1: 800 &amp;lt;--&amp;gt; 1400 mV at 1100 mV fast normal&lt;/P&gt;&lt;P&gt;print_constraints: vdd3p0: 2625 &amp;lt;--&amp;gt; 3400 mV at 3000 mV fast normal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2009.08-00602-g3f71ed9 (Nov 26 2012 - 17:31:49)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6 family TO1.2 at 792 MHz&lt;/P&gt;&lt;P&gt;Temperature:&amp;nbsp;&amp;nbsp; 53 C, calibration data 0x5884c57d&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Aug 2013 16:13:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Sabre-SD-kernel-boot-crash/m-p/263543#M26976</guid>
      <dc:creator>BernardDAUTREVA</dc:creator>
      <dc:date>2013-08-19T16:13:24Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q Sabre SD kernel boot crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Sabre-SD-kernel-boot-crash/m-p/263544#M26977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just test with the already compiled uImage provided in the image_bundle tarball and I get the same result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder if this could be a compatibility problem between u-boot and the Linux kernel, as I still use the u-boot of the ICS 13.4.1 release. I will test with the proper u-boot later today but I need firts to get my SD-card reader... (I usually work only through the network, loading the kernel through TFTP and the root filesystem through NFS).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bernard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Aug 2013 11:37:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Sabre-SD-kernel-boot-crash/m-p/263544#M26977</guid>
      <dc:creator>BernardDAUTREVA</dc:creator>
      <dc:date>2013-08-20T11:37:03Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q Sabre SD kernel boot crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Sabre-SD-kernel-boot-crash/m-p/263545#M26978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bernard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The u-boot should not be a problem here since it is the same from previous versions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not sure that I got the situation here, can you confirm:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- You are able to boot using FSL's android SD Card with the 5v 5a power supply.&lt;/P&gt;&lt;P&gt;- You are not able to boot using FSL's android SD Card with the 5v 5a power supply.&lt;/P&gt;&lt;P&gt;- You are not able to boot your compiled card with any of the power supplies.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is this correct?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2013 17:41:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Sabre-SD-kernel-boot-crash/m-p/263545#M26978</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2013-08-22T17:41:57Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q Sabre SD kernel boot crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Sabre-SD-kernel-boot-crash/m-p/263546#M26979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is approximately correct:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to boot using FSL's android SD Card with the 5V 5A power supply&lt;/P&gt;&lt;P&gt;I am able to boot using FSL's android SD Card with the 5V 2A power supply&lt;/P&gt;&lt;P&gt;I am not able to start the board with the 5V 1A power supply (sometimes it seems to start but crash when booting the board)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However that is not too much of a problem as I have only a few 1A power supplies and mainly 2A or 5A power supplies. The behavior I get with my compiled kernel was just reminding me of the same kind of problem when a not powerful enough board was connected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My real problem is that when I recompile the kernel and try to boot it after loading the uImage through TFTP it crashes with the messages above, just after printing the constraints for regulator vdd3p0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I got the kernel from git://git.freescale.com/imx/linux-2.6-imx.git, tag jb4.2.2_1.1.0-ga&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I compile it as instructed using the gcc compiler provided by Google in the AOSP 4.2.2 release&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I configure it as imx6_android_defconfig&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I then today was able to burn the u-boot I recompiled from the sources during the Android buildn in an SD card that I partitionned as instructed and now the kernel is able to boot almost to the end! so there is indeed a dependency to the u-boot version used that should be different between the ICS (R13.4.1) that was on the original SD Card and the one I just recompile.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My kernel was not able to boot completly however and crashes silently just after the "Freeing init memory: 244K" message (he was just before that able to mount the root filesystem on NFS).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect here a problem in the declaration of some functions and structures as _devinit or _initdata in arch/arm/mach-mx6/pcie.c as when compiling th ekernel manually (can't see the message in a full android build...) I get a section mismatch in this file... However solving this conflict (by removing _init tags to a few functions and data) does not change anything...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also have a proble wiith u-boot (only able to save the environment once) but it is probably better that I report it in a second message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the log I get when booting my kernel: (note it stops at the same point if I burn everything on teh SD card and boot with the default u-boot setup)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;.## Booting kernel from Legacy Image at 10800000 ...&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; Linux-3.0.35-06126-g0f2d6ad&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; ARM Linux Kernel Image (uncompressed)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 4766136 Bytes =&amp;nbsp; 4.5 MB&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Load Address: 10008000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 10008000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Loading Kernel Image ... OK&lt;BR /&gt;OK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Uncompressing Linux... done, booting the kernel.&lt;BR /&gt;Initializing cgroup subsys cpu&lt;BR /&gt;Linux version 3.0.35-06126-g0f2d6ad (dautrevaux@coLinux) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #2 SMP PREEMPT Fri Aug 23 19:03:02 CEST 2013&lt;BR /&gt;CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d&lt;BR /&gt;CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board&lt;BR /&gt;Ignoring unrecognised tag 0x54410008&lt;BR /&gt;Memory policy: ECC disabled, Data cache writealloc&lt;BR /&gt;CPU identified as i.MX6Q, silicon rev 1.2&lt;BR /&gt;PERCPU: Embedded 7 pages/cpu @c1323000 s6592 r8192 d13888 u32768&lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 208128&lt;BR /&gt;Kernel command line: init=/init androidboot.console=ttymxc0 androidboot.hardware=freescale console=ttymxc0,115200n8 ip=192.168.233.128:192.168.233.1:192.168.233.1:255.255.255.0:sabresd_6dq:eth0:off fbmem=10M vmalloc=400M root=/dev/nfs nfsroot=192.168.233.1:/tftpboot/rootfs-sabresd_6dq&lt;BR /&gt;PID hash table entries: 2048 (order: 1, 8192 bytes)&lt;BR /&gt;Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;BR /&gt;Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;BR /&gt;Memory: 767MB 54MB = 821MB total&lt;BR /&gt;Memory: 820584k/820584k available, 227992k reserved, 431104K highmem&lt;BR /&gt;Virtual kernel memory layout:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vector&amp;nbsp; : 0xffff0000 - 0xffff1000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 4 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fixmap&amp;nbsp; : 0xfff00000 - 0xfffe0000&amp;nbsp;&amp;nbsp; ( 896 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0xfbe00000 - 0xffe00000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 64 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmalloc : 0xd9800000 - 0xf2000000&amp;nbsp;&amp;nbsp; ( 392 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; lowmem&amp;nbsp; : 0xc0000000 - 0xd9000000&amp;nbsp;&amp;nbsp; ( 400 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pkmap&amp;nbsp;&amp;nbsp; : 0xbfe00000 - 0xc0000000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 2 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; modules : 0xbf000000 - 0xbfe00000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 14 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .init : 0xc0008000 - 0xc0045000&amp;nbsp;&amp;nbsp; ( 244 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0xc0045000 - 0xc08f9928&amp;nbsp;&amp;nbsp; (8915 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0xc08fa000 - 0xc0991bc0&amp;nbsp;&amp;nbsp; ( 607 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bss : 0xc0991be4 - 0xc0b19928&amp;nbsp;&amp;nbsp; (1568 kB)&lt;BR /&gt;Preemptible hierarchical RCU implementation.&lt;BR /&gt;NR_IRQS:624&lt;BR /&gt;MXC GPIO hardware&lt;BR /&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms&lt;BR /&gt;arm_max_freq=1GHz&lt;BR /&gt;MXC_Early serial console at MMIO 0x2020000 (options '115200n8')&lt;BR /&gt;bootconsole [ttymxc0] enabled&lt;BR /&gt;Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)&lt;BR /&gt;pid_max: default: 32768 minimum: 301&lt;BR /&gt;Mount-cache hash table entries: 512&lt;BR /&gt;Initializing cgroup subsys debug&lt;BR /&gt;Initializing cgroup subsys cpuacct&lt;BR /&gt;Initializing cgroup subsys freezer&lt;BR /&gt;CPU: Testing write buffer coherency: ok&lt;BR /&gt;hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available&lt;BR /&gt;CPU1: Booted secondary processor&lt;BR /&gt;CPU2: Booted secondary processor&lt;BR /&gt;CPU3: Booted secondary processor&lt;BR /&gt;Brought up 4 CPUs&lt;BR /&gt;SMP: Total of 4 processors activated (6324.22 BogoMIPS).&lt;BR /&gt;print_constraints: dummy:&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;print_constraints: vddpu: 725 &amp;lt;--&amp;gt; 1300 mV at 700 mV fast normal&lt;BR /&gt;print_constraints: vddcore: 725 &amp;lt;--&amp;gt; 1300 mV at 1100 mV fast normal&lt;BR /&gt;print_constraints: vddsoc: 725 &amp;lt;--&amp;gt; 1300 mV at 1200 mV fast normal&lt;BR /&gt;print_constraints: vdd2p5: 2000 &amp;lt;--&amp;gt; 2775 mV at 2400 mV fast normal&lt;BR /&gt;print_constraints: vdd1p1: 800 &amp;lt;--&amp;gt; 1400 mV at 1100 mV fast normal&lt;BR /&gt;print_constraints: vdd3p0: 2625 &amp;lt;--&amp;gt; 3400 mV at 3000 mV fast normal&lt;BR /&gt;ram_console: got buffer at 3ff00000, size 100000&lt;BR /&gt;ram_console: uncorrectable error in header&lt;BR /&gt;ram_console: no valid data in buffer (sig = 0x010a0350)&lt;BR /&gt;console [ram-1] enabled&lt;BR /&gt;No AHCI save PWR: PDDQ enabled&lt;BR /&gt;hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.&lt;BR /&gt;hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.&lt;BR /&gt;hw-breakpoint: maximum watchpoint size is 4 bytes.&lt;BR /&gt;L310 cache controller enabled&lt;BR /&gt;l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B&lt;BR /&gt;bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;BR /&gt;mxs-dma mxs-dma-apbh: initialized&lt;BR /&gt;print_constraints: SPKVDD: 4200 mV&lt;BR /&gt;print_constraints: vmmc: 3300 mV&lt;BR /&gt;vgaarb: loaded&lt;BR /&gt;SCSI subsystem initialized&lt;BR /&gt;spi_imx imx6q-ecspi.0: probed&lt;BR /&gt;usbcore: registered new interface driver usbfs&lt;BR /&gt;usbcore: registered new interface driver hub&lt;BR /&gt;usbcore: registered new device driver usb&lt;BR /&gt;Freescale USB OTG Driver loaded, $Revision: 1.55 $&lt;BR /&gt;mc_pfuze 1-0008: ID: 0,Full lay: 1 ,Metal lay: 1&lt;BR /&gt;mc_pfuze 1-0008: FAB: 0 ,FIN: 0&lt;BR /&gt;print_constraints: PFUZE100_SW1A: 300 &amp;lt;--&amp;gt; 1875 mV at 1300 mV&lt;BR /&gt;print_constraints: PFUZE100_SW1B: 300 &amp;lt;--&amp;gt; 1875 mV at 300 mV&lt;BR /&gt;print_constraints: PFUZE100_SW1C: 300 &amp;lt;--&amp;gt; 1875 mV at 1300 mV&lt;BR /&gt;print_constraints: PFUZE100_SW2: 800 &amp;lt;--&amp;gt; 3950 mV at 3300 mV&lt;BR /&gt;print_constraints: PFUZE100_SW3A: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV&lt;BR /&gt;print_constraints: PFUZE100_SW3B: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV&lt;BR /&gt;print_constraints: PFUZE100_SW4: 800 &amp;lt;--&amp;gt; 3950 mV at 3150 mV&lt;BR /&gt;print_constraints: PFUZE100_SWBST: 5000 &amp;lt;--&amp;gt; 5150 mV at 5000 mV&lt;BR /&gt;print_constraints: PFUZE100_VSNVS: 1200 &amp;lt;--&amp;gt; 3000 mV at 1800 mV&lt;BR /&gt;print_constraints: PFUZE100_VREFDDR: at 750 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN1: 800 &amp;lt;--&amp;gt; 1550 mV at 1500 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN2: 800 &amp;lt;--&amp;gt; 1550 mV at 1500 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN3: 1800 &amp;lt;--&amp;gt; 3300 mV at 2800 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN4: 1800 &amp;lt;--&amp;gt; 3300 mV at 1800 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN5: 1800 &amp;lt;--&amp;gt; 3300 mV at 3000 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN6: 1800 &amp;lt;--&amp;gt; 3300 mV at 3300 mV&lt;BR /&gt;imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)&lt;BR /&gt;imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)&lt;BR /&gt;mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed&lt;BR /&gt;mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a&lt;BR /&gt;MIPI CSI2 driver module loaded&lt;BR /&gt;Advanced Linux Sound Architecture Driver Version 1.0.24.&lt;BR /&gt;Bluetooth: Core ver 2.16&lt;BR /&gt;NET: Registered protocol family 31&lt;BR /&gt;Bluetooth: HCI device and connection manager initialized&lt;BR /&gt;Bluetooth: HCI socket layer initialized&lt;BR /&gt;Bluetooth: L2CAP socket layer initialized&lt;BR /&gt;Bluetooth: SCO socket layer initialized&lt;BR /&gt;max17135_regulator_init abort: EPDC not enabled&lt;BR /&gt;max17135 2-0048: PMIC MAX17135 for eInk display&lt;BR /&gt;i2c-core: driver [max17135] using legacy suspend method&lt;BR /&gt;i2c-core: driver [max17135] using legacy resume method&lt;BR /&gt;Switching to clocksource mxc_timer1&lt;BR /&gt;NET: Registered protocol family 2&lt;BR /&gt;IP route cache hash table entries: 16384 (order: 4, 65536 bytes)&lt;BR /&gt;TCP established hash table entries: 65536 (order: 7, 524288 bytes)&lt;BR /&gt;TCP bind hash table entries: 65536 (order: 7, 786432 bytes)&lt;BR /&gt;TCP: Hash tables configured (established 65536 bind 65536)&lt;BR /&gt;TCP reno registered&lt;BR /&gt;UDP hash table entries: 256 (order: 1, 8192 bytes)&lt;BR /&gt;UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)&lt;BR /&gt;NET: Registered protocol family 1&lt;BR /&gt;RPC: Registered named UNIX socket transport module.&lt;BR /&gt;RPC: Registered udp transport module.&lt;BR /&gt;RPC: Registered tcp transport module.&lt;BR /&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;PCI: CLS 0 bytes, default 32&lt;BR /&gt;PMU: registered new PMU device of type 0&lt;BR /&gt;Static Power Management for Freescale i.MX6&lt;BR /&gt;wait mode is enabled for i.MX6&lt;BR /&gt;cpaddr = d9880000 suspend_iram_base=d9934000&lt;BR /&gt;PM driver module loaded&lt;BR /&gt;link up failed, DB_R0:0x00e2f100, DB_R1:0x08200000!&lt;BR /&gt;IMX PCIe port: link down with power supply 1!&lt;BR /&gt;IMX usb wakeup probe&lt;BR /&gt;the wakeup pdata is 0xd65f0f60&lt;BR /&gt;add wake up source irq 75&lt;BR /&gt;IMX usb wakeup probe&lt;BR /&gt;the wakeup pdata is 0xd65f0ce0&lt;BR /&gt;cpu regulator mode:ldo_bypass&lt;BR /&gt;_regulator_get: get() with no identifier&lt;BR /&gt;mx6_cpu_regulator_init: failed to get pu regulator&lt;BR /&gt;i.MXC CPU frequency driver&lt;BR /&gt;highmem bounce pool size: 64 pages&lt;BR /&gt;ashmem: initialized&lt;BR /&gt;NTFS driver 2.1.30 [Flags: R/O].&lt;BR /&gt;JFFS2 version 2.2. (NAND) Â© 2001-2006 Red Hat, Inc.&lt;BR /&gt;fuse init (API version 7.16)&lt;BR /&gt;msgmni has been set to 760&lt;BR /&gt;NET: Registered protocol family 38&lt;BR /&gt;cryptodev: driver loaded.&lt;BR /&gt;io scheduler noop registered&lt;BR /&gt;io scheduler deadline registered&lt;BR /&gt;io scheduler cfq registered (default)&lt;BR /&gt;mxc_mipi_dsi mxc_mipi_dsi: i.MX MIPI DSI driver probed&lt;BR /&gt;MIPI DSI driver module loaded&lt;BR /&gt;mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb&lt;BR /&gt;_regulator_get: get() with no identifier&lt;BR /&gt;imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)&lt;BR /&gt;mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver hdmi&lt;BR /&gt;mxc_hdmi mxc_hdmi: Detected HDMI controller 0x13:0xa:0xa0:0xc1&lt;BR /&gt;fbcvt: 1920x1080@60: CVT Name - 2.073M9&lt;BR /&gt;mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver ldb&lt;BR /&gt;imx-sdma imx-sdma: loaded firmware 1.1&lt;BR /&gt;imx-sdma imx-sdma: initialized&lt;BR /&gt;Serial: IMX driver&lt;BR /&gt;imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX&lt;BR /&gt;imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX&lt;BR /&gt;console [ttymxc0] enabled, bootconsole disabled&lt;BR /&gt;console [ttymxc0] enabled, bootconsole disabled&lt;BR /&gt;loop: module loaded&lt;BR /&gt;m25p80 spi0.0: found m25p32, expected sst25vf016b&lt;BR /&gt;m25p80 spi0.0: m25p32 (4096 Kbytes)&lt;BR /&gt;Creating 2 MTD partitions on "m25p80":&lt;BR /&gt;0x000000000000-0x000000100000 : "bootloader"&lt;BR /&gt;0x000000100000-0x000000400000 : "kernel"&lt;BR /&gt;GPMI NAND driver registered. (IMX)&lt;BR /&gt;vcan: Virtual CAN interface driver&lt;BR /&gt;CAN device driver interface&lt;BR /&gt;flexcan netdevice driver&lt;BR /&gt;FEC Ethernet Driver&lt;BR /&gt;fec_enet_mii_bus: probed&lt;BR /&gt;PPP generic driver version 2.4.2&lt;BR /&gt;PPP Deflate Compression module registered&lt;BR /&gt;PPP BSD Compression module registered&lt;BR /&gt;PPP MPPE Compression module registered&lt;BR /&gt;NET: Registered protocol family 24&lt;BR /&gt;PPTP driver version 0.8.5&lt;BR /&gt;tun: Universal TUN/TAP device driver, 1.6&lt;BR /&gt;&lt;SPAN&gt;tun: (C) 1999-2004 Max Krasnyansky &amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:maxk@qualcomm.com"&gt;maxk@qualcomm.com&lt;/A&gt;&lt;SPAN&gt;&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;BR /&gt;fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller&lt;BR /&gt;fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1&lt;BR /&gt;fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000&lt;BR /&gt;fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00&lt;BR /&gt;hub 1-0:1.0: USB hub found&lt;BR /&gt;hub 1-0:1.0: 1 port detected&lt;BR /&gt;add wake up source irq 72&lt;BR /&gt;fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller&lt;BR /&gt;fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2&lt;BR /&gt;fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200&lt;BR /&gt;fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00&lt;BR /&gt;hub 2-0:1.0: USB hub found&lt;BR /&gt;hub 2-0:1.0: 1 port detected&lt;BR /&gt;usbcore: registered new interface driver cdc_acm&lt;BR /&gt;cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters&lt;BR /&gt;Initializing USB Mass Storage driver...&lt;BR /&gt;usbcore: registered new interface driver usb-storage&lt;BR /&gt;USB Mass Storage support registered.&lt;BR /&gt;usbcore: registered new interface driver usbserial&lt;BR /&gt;usbserial: USB Serial Driver core&lt;BR /&gt;USB Serial support registered for GSM modem (1-port)&lt;BR /&gt;usbcore: registered new interface driver option&lt;BR /&gt;option: v0.7.2:USB Driver for GSM modems&lt;BR /&gt;USB Serial support registered for Qualcomm USB modem&lt;BR /&gt;usbcore: registered new interface driver qcserial&lt;BR /&gt;ARC USBOTG Device Controller driver (1 August 2005)&lt;BR /&gt;android_usb gadget: Mass Storage Function, version: 2009/09/11&lt;BR /&gt;android_usb gadget: Number of LUNs=1&lt;BR /&gt; lun0: LUN: removable file: (no medium)&lt;BR /&gt;Gadget Android: controller 'fsl-usb2-udc' not recognized&lt;BR /&gt;android_usb gadget: android_usb ready&lt;BR /&gt;Suspend udc for OTG auto detect&lt;BR /&gt;USB Host suspend begins&lt;BR /&gt;will suspend roothub and its children&lt;BR /&gt;ehci_fsl_bus_suspend begins, DR&lt;BR /&gt;ehci_fsl_bus_suspend ends, DR&lt;BR /&gt;host suspend ends&lt;BR /&gt;USB Gadget resume begins&lt;BR /&gt;fsl_udc_resume, Wait for wakeup thread finishes&lt;BR /&gt;dr_controller_run: udc out low power mode&lt;BR /&gt;USB Gadget resume ends&lt;BR /&gt;fsl-usb2-udc: bind to driver android_usb&lt;BR /&gt;mousedev: PS/2 mouse device common for all mice&lt;BR /&gt;input: gpio-keys as /devices/platform/gpio-keys/input/input0&lt;BR /&gt;input: max11801_ts as /devices/platform/imx-i2c.1/i2c-1/1-0048/input/input1&lt;BR /&gt;egalax_ts 1-0004: egalax_ts: failed to read firmware version&lt;BR /&gt;egalax_ts: probe of 1-0004 failed with error -5&lt;BR /&gt;input: eGalax Touch Screen as /devices/platform/imx-i2c.2/i2c-2/2-0004/input/input2&lt;BR /&gt;android_work: did not send uevent (0 0&amp;nbsp;&amp;nbsp; (null))&lt;BR /&gt;android_work: sent uevent USB_STATE=CONNECTED&lt;BR /&gt;android_work: sent uevent USB_STATE=DISCONNECTED&lt;BR /&gt;android_work: sent uevent USB_STATE=CONNECTED&lt;BR /&gt;android_work: sent uevent USB_STATE=DISCONNECTED&lt;BR /&gt;android_work: sent uevent USB_STATE=CONNECTED&lt;BR /&gt;android_work: sent uevent USB_STATE=DISCONNECTED&lt;BR /&gt;android_work: sent uevent USB_STATE=CONNECTED&lt;BR /&gt;android_work: sent uevent USB_STATE=DISCONNECTED&lt;BR /&gt;android_work: sent uevent USB_STATE=CONNECTED&lt;BR /&gt;android_work: sent uevent USB_STATE=DISCONNECTED&lt;BR /&gt;elan - Read Hello Packet Failed&lt;BR /&gt;elan-touch: probe of 2-0010 failed with error -22&lt;BR /&gt;input: isl29023 light sensor as /devices/virtual/input/input3&lt;BR /&gt;isl29023 2-0044: driver version 1.0 enabled&lt;BR /&gt;i2c-core: driver [isl29023] using legacy suspend method&lt;BR /&gt;i2c-core: driver [isl29023] using legacy resume method&lt;BR /&gt;using rtc device, snvs_rtc, for alarms&lt;BR /&gt;snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0&lt;BR /&gt;i2c /dev entries driver&lt;BR /&gt;Linux video capture interface: v2.00&lt;BR /&gt;android_work: sent uevent USB_STATE=CONNECTED&lt;BR /&gt;android_work: sent uevent USB_STATE=DISCONNECTED&lt;BR /&gt;android_work: sent uevent USB_STATE=CONNECTED&lt;BR /&gt;android_work: sent uevent USB_STATE=DISCONNECTED&lt;BR /&gt;camera ov5642 is found&lt;BR /&gt;USB Gadget resume begins&lt;BR /&gt;fsl_udc_resume, Wait for wakeup thread finishes&lt;BR /&gt;android_work: sent uevent USB_STATE=CONNECTED&lt;BR /&gt;camera ov5640_mipi is found&lt;BR /&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16&lt;BR /&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17&lt;BR /&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18&lt;BR /&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19&lt;BR /&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20&lt;BR /&gt;usbcore: registered new interface driver uvcvideo&lt;BR /&gt;USB Video Class driver (v1.1.0)&lt;BR /&gt;mag3110 2-000e: check mag3110 chip ID&lt;BR /&gt;input: mag3110 as /devices/virtual/input/input4&lt;BR /&gt;mag3110 2-000e: mag3110 is probed&lt;BR /&gt;i2c-core: driver [mag3110] using legacy suspend method&lt;BR /&gt;i2c-core: driver [mag3110] using legacy resume method&lt;BR /&gt;input: mma845x as /devices/virtual/input/input5&lt;BR /&gt;imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)&lt;BR /&gt;device-mapper: uevent: version 1.0.3&lt;BR /&gt;&lt;SPAN&gt;device-mapper: ioctl: 4.20.0-ioctl (2011-02-02) initialised: &lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:dm-devel@redhat.com"&gt;dm-devel@redhat.com&lt;/A&gt;&lt;BR /&gt;Bluetooth: Virtual HCI driver ver 1.3&lt;BR /&gt;Bluetooth: HCI UART driver ver 2.2&lt;BR /&gt;Bluetooth: HCIATH3K protocol initialized&lt;BR /&gt;Bluetooth: Generic Bluetooth USB driver ver 0.6&lt;BR /&gt;usbcore: registered new interface driver btusb&lt;BR /&gt;sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;mmc0: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA&lt;BR /&gt;mmc1: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA&lt;BR /&gt;mmc2: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA&lt;BR /&gt;mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed&lt;BR /&gt;VPU initialized&lt;BR /&gt;mxc_asrc registered&lt;BR /&gt;revserved_memory_account:viv_gpu registerd&lt;BR /&gt;Thermal calibration data is 0x5884c57d&lt;BR /&gt;Thermal sensor with ratio = 183&lt;BR /&gt;Anatop Thermal registered as thermal_zone0&lt;BR /&gt;anatop_thermal_probe: default cooling device is cpufreq!&lt;BR /&gt;Registered led device: chg_now_led&lt;BR /&gt;usbcore: registered new interface driver usbhid&lt;BR /&gt;usbhid: USB HID core driver&lt;BR /&gt;logger: created 256K log 'log_main'&lt;BR /&gt;logger: created 256K log 'log_events'&lt;BR /&gt;logger: created 256K log 'log_radio'&lt;BR /&gt;logger: created 256K log 'log_system'&lt;BR /&gt;usbcore: registered new interface driver snd-usb-audio&lt;BR /&gt;mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio&lt;BR /&gt;Cirrus Logic CS42888 ALSA SoC Codec Driver&lt;BR /&gt;i2c-core: driver [cs42888] using legacy suspend method&lt;BR /&gt;i2c-core: driver [cs42888] using legacy resume method&lt;BR /&gt;mmc0: new high speed DDR MMC card at address 0001&lt;BR /&gt;mmcblk0: mmc0:0001 SEM08G 7.39 GiB&lt;BR /&gt;mmcblk0boot0: mmc0:0001 SEM08G partition 1 2.00 MiB&lt;BR /&gt;mmcblk0boot1: mmc0:0001 SEM08G partition 2 2.00 MiB&lt;BR /&gt; mmcblk0: unknown partition table&lt;BR /&gt; mmcblk0boot1: unknown partition table&lt;BR /&gt; mmcblk0boot0: unknown partition table&lt;BR /&gt;wm8962 0-001a: customer id 0 revision D&lt;BR /&gt;input: WM8962 Beep Generator as /devices/platform/imx-i2c.0/i2c-0/0-001a/input/input6&lt;BR /&gt;asoc: wm8962 &amp;lt;-&amp;gt; imx-ssi.1 mapping ok&lt;BR /&gt;input: wm8962-audio DMIC as /devices/platform/soc-audio.5/sound/card0/input7&lt;BR /&gt;input: wm8962-audio Headphone Jack as /devices/platform/soc-audio.5/sound/card0/input8&lt;BR /&gt;imx_3stack asoc driver&lt;BR /&gt;asoc: mxc-hdmi-soc &amp;lt;-&amp;gt; imx-hdmi-soc-dai.0 mapping ok&lt;BR /&gt;ALSA device list:&lt;BR /&gt;&amp;nbsp; #0: wm8962-audio&lt;BR /&gt;&amp;nbsp; #1: imx-hdmi-soc&lt;BR /&gt;oprofile: using arm/armv7-ca9&lt;BR /&gt;GACT probability NOT on&lt;BR /&gt;Mirror/redirect action on&lt;BR /&gt;u32 classifier&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Actions configured&lt;BR /&gt;Netfilter messages via NETLINK v0.30.&lt;BR /&gt;nf_conntrack version 0.5.0 (12821 buckets, 51284 max)&lt;BR /&gt;mmc1: new high speed SDHC card at address 0002&lt;BR /&gt;mmcblk1: mmc1:0002 00000 7.41 GiB&lt;BR /&gt;ctnetlink v0.93: registering with nfnetlink.&lt;BR /&gt; mmcblk1: p1 p2 p3 &amp;lt; p5 p6 p7 p8 p9 &amp;gt; p4&lt;BR /&gt;NF_TPROXY: Transparent proxy support initialized, version 4.1.0&lt;BR /&gt;NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.&lt;BR /&gt;xt_time: kernel timezone is -0000&lt;BR /&gt;IPv4 over IPv4 tunneling driver&lt;BR /&gt;GRE over IPv4 demultiplexor driver&lt;BR /&gt;ip_tables: (C) 2000-2006 Netfilter Core Team&lt;BR /&gt;arp_tables: (C) 2002 David S. Miller&lt;BR /&gt;TCP cubic registered&lt;BR /&gt;NET: Registered protocol family 10&lt;BR /&gt;Mobile IPv6&lt;BR /&gt;ip6_tables: (C) 2000-2006 Netfilter Core Team&lt;BR /&gt;IPv6 over IPv4 tunneling driver&lt;BR /&gt;NET: Registered protocol family 17&lt;BR /&gt;NET: Registered protocol family 15&lt;BR /&gt;can: controller area network core (rev 20090105 abi 8)&lt;BR /&gt;NET: Registered protocol family 29&lt;BR /&gt;can: raw protocol (rev 20090105)&lt;BR /&gt;can: broadcast manager protocol (rev 20090105 t)&lt;BR /&gt;Bluetooth: RFCOMM TTY layer initialized&lt;BR /&gt;Bluetooth: RFCOMM socket layer initialized&lt;BR /&gt;Bluetooth: RFCOMM ver 1.11&lt;BR /&gt;Bluetooth: BNEP (Ethernet Emulation) ver 1.3&lt;BR /&gt;Bluetooth: BNEP filters: protocol multicast&lt;BR /&gt;Bluetooth: HIDP (Human Interface Emulation) ver 1.2&lt;BR /&gt;L2TP core driver, V2.0&lt;BR /&gt;PPPoL2TP kernel driver, V2.0&lt;BR /&gt;L2TP IP encapsulation support (L2TPv3)&lt;BR /&gt;L2TP netlink interface&lt;BR /&gt;L2TP ethernet pseudowire support (L2TPv3)&lt;BR /&gt;lib80211: common routines for IEEE802.11 drivers&lt;BR /&gt;lib80211_crypt: registered algorithm 'NULL'&lt;BR /&gt;lib80211_crypt: registered algorithm 'WEP'&lt;BR /&gt;lib80211_crypt: registered algorithm 'CCMP'&lt;BR /&gt;lib80211_crypt: registered algorithm 'TKIP'&lt;BR /&gt;VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4&lt;BR /&gt;Bus freq driver module loaded&lt;BR /&gt;Bus freq driver Enabled&lt;BR /&gt;mxc_dvfs_core_probe&lt;BR /&gt;DVFS driver module loaded&lt;BR /&gt;regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on&lt;BR /&gt;regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on&lt;BR /&gt;regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on&lt;BR /&gt;regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on&lt;BR /&gt;snvs_rtc snvs_rtc.0: setting system clock to 1970-01-02 00:59:59 UTC (89999)&lt;BR /&gt;eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=1:01, irq=-1)&lt;BR /&gt;ADDRCONF(NETDEV_UP): eth0: link is not ready&lt;BR /&gt;ehci_fsl_bus_suspend begins, Host 1&lt;BR /&gt;ehci_fsl_bus_suspend ends, Host 1&lt;BR /&gt;PHY: 1:01 - Link is Up - 100/Full&lt;BR /&gt;ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready&lt;BR /&gt;IP-Config: Complete:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; device=eth0, addr=192.168.233.128, mask=255.255.255.0, gw=192.168.233.1,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; host=sabresd_6dq, domain=, nis-domain=(none),&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bootserver=192.168.233.1, rootserver=192.168.233.1, rootpath=&lt;BR /&gt;VFS: Mounted root (nfs filesystem) on device 0:12.&lt;BR /&gt;Freeing init memory: 244K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Aug 2013 17:14:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Sabre-SD-kernel-boot-crash/m-p/263546#M26979</guid>
      <dc:creator>BernardDAUTREVA</dc:creator>
      <dc:date>2013-08-23T17:14:18Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q Sabre SD kernel boot crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Sabre-SD-kernel-boot-crash/m-p/263547#M26980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just tried with the NFS filesystem provided in the ga_image package and both my kernel and the official kernel works fine, as long as I use the u-boot image provided with the 4.2.2-1.1.0-ga_image package. If I use the u-boot on the original SD Card (R13.4.1 ICS) I get the abort soon in the kernel boot as explained in my first post.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So there is at least two differences between the two u-boot versions:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Some initializations are different, thus the newe kernels can't boot from a board initialized by the older u-boot&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The new u-boot REFUSES to save the "botcmd" environment variable: I can change and save the content of ANY variable EXCEPT bootcmd&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I think that is VERY unconvenient! I will look at the u-boot source code to try to understand what happens;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I wonder if the variable is saved correctly but overwritten at u-boot start...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The kernel stop I noticed after the "Freeing init memory: 244K" message seems to be caused by the root filesystem; however I still have to understand what as different between the released NFS image and the one I constructed, but I have some ideas about that an shoud be able to solve that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will post again when everything works and I was able to correct the u-boot behavior.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Aug 2013 11:25:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Sabre-SD-kernel-boot-crash/m-p/263547#M26980</guid>
      <dc:creator>BernardDAUTREVA</dc:creator>
      <dc:date>2013-08-24T11:25:54Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q Sabre SD kernel boot crash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Sabre-SD-kernel-boot-crash/m-p/263548#M26981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bernard, has this issue been solved? What is the root cause? We encounter the same issue on our i.MX6 board. Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Oct 2013 06:55:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Sabre-SD-kernel-boot-crash/m-p/263548#M26981</guid>
      <dc:creator>Pao_portalinks</dc:creator>
      <dc:date>2013-10-10T06:55:31Z</dc:date>
    </item>
  </channel>
</rss>