<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx.233 VDDIO_DRAM in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx-233-VDDIO-DRAM/m-p/262688#M26682</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running the imx233 chip but have problems with the 2.5V VDDIO_DRAM.&amp;nbsp; All the other voltages are there (5Vsupply, 3.3V, 1.8V, 1.2V) except 2.5V for my DDR memory.&amp;nbsp; Is there something I need to do to enable the 2.5V regulator output on the IMX 233 chip?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Jul 2013 17:49:33 GMT</pubDate>
    <dc:creator>cnguyenterasci</dc:creator>
    <dc:date>2013-07-09T17:49:33Z</dc:date>
    <item>
      <title>imx.233 VDDIO_DRAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-233-VDDIO-DRAM/m-p/262688#M26682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running the imx233 chip but have problems with the 2.5V VDDIO_DRAM.&amp;nbsp; All the other voltages are there (5Vsupply, 3.3V, 1.8V, 1.2V) except 2.5V for my DDR memory.&amp;nbsp; Is there something I need to do to enable the 2.5V regulator output on the IMX 233 chip?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jul 2013 17:49:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-233-VDDIO-DRAM/m-p/262688#M26682</guid>
      <dc:creator>cnguyenterasci</dc:creator>
      <dc:date>2013-07-09T17:49:33Z</dc:date>
    </item>
    <item>
      <title>Re: imx.233 VDDIO_DRAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-233-VDDIO-DRAM/m-p/262689#M26683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Calvin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; You may need to enable this 2P5 regulator manually, as it is disable by default. See below code:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // DDR1,VDDM = 2.5V&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Clear pulldown as it isn't needed for internal linear regulator&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; HW_POWER_VDDMEMCTRL_CLR(BM_POWER_VDDMEMCTRL_PULLDOWN_ACTIVE);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; HW_POWER_VDDMEMCTRL.B.TRG = 0x10; // ~2.5v&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; HW_POWER_VDDMEMCTRL_SET(BM_POWER_VDDMEMCTRL_ENABLE_ILIMIT);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; HW_POWER_VDDMEMCTRL_SET(BM_POWER_VDDMEMCTRL_ENABLE_LINREG);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Wait 10ms for 2p5 capacitor to fully charge&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; XLDRStall(20000);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; HW_POWER_VDDMEMCTRL_CLR(BM_POWER_VDDMEMCTRL_ENABLE_ILIMIT);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jul 2013 03:20:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-233-VDDIO-DRAM/m-p/262689#M26683</guid>
      <dc:creator>AnsonHuang</dc:creator>
      <dc:date>2013-07-10T03:20:26Z</dc:date>
    </item>
  </channel>
</rss>