<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic JTAG Debugging - Connecting to i.MX53, i.MX51 TO2, i.MX37, i.MX31, and i.MX25 using RVDS 3.1 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/JTAG-Debugging-Connecting-to-i-MX53-i-MX51-TO2-i-MX37-i-MX31-and/m-p/157871#M2662</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Connecting to i.MX53, i.MX51 TO2, i.MX37, i.MX31 and i.MX25&amp;nbsp;using RVDS 3.1&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;STRONG&gt;RVI update:&lt;/STRONG&gt;&lt;BR /&gt;In order to connect to i.MX51 TO2 RVI updates are required.&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;Patches must be applied in this order:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;ARM-RVI-3.1.0-754-base.rvi&lt;/LI&gt;&lt;LI&gt;ARM_RVI-3.1.3-776-patch.rvi&lt;/LI&gt;&lt;LI&gt;ARM-RVI-3.2.0-850-base.rvi&lt;/LI&gt;&lt;LI&gt;ARM-RVI-3.2.6-875-Engineer-patch.rvi&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Note - Check ARM's website for patches&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR class="atl-forced-newline" /&gt;Note: after the update ETMBUF is not listed as a registered option. Use an unregistered device of IR length 4 in place of ETMBUF.&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;i.MX53&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Same as i.MX51 TO2 except Coresight base address is 0xC0008000&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN style="color: #000000; "&gt;&lt;STRONG&gt;i.MX50&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Same as i.MX53 -&amp;gt; Coresight base address is 0xC0008000&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;i.MX51 TO2&lt;/STRONG&gt;&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Connect RVICE to MX51 board using short JTAG parallel cable.&amp;nbsp; LVDS probe cannot be used.&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;Configure the scan chain with the following connections (TDI =&amp;gt; Unknown =&amp;gt; Unknown =&amp;gt; ARMCS-DP =&amp;gt; Cortex-A8)&lt;UL&gt;&lt;LI&gt;Add Device=&amp;gt;Custom Device=&amp;gt;UNKNOWN=&amp;gt;IR Length = 5&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Custom Device=&amp;gt;UNKNOWN=&amp;gt;IR Length = 4&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Registered Device=&amp;gt;CoreSight=&amp;gt;ARMCS-DP&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Registered Device=&amp;gt;Cortex=&amp;gt;Cortex-A8&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;Update the CoreSight base address as follows:&lt;UL&gt;&lt;LI&gt;Right Click on Cortex-A8 Device&lt;/LI&gt;&lt;LI&gt;Select Configuration&lt;/LI&gt;&lt;LI&gt;Set CoreSight base address = 0xE0008000&lt;/LI&gt;&lt;LI&gt;Save the configuration&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN class="image-wrap"&gt;&lt;IMG height="427" src="http://wiki.freescale.net/download/attachments/14260451/worddavc1f53298886db4ea194c98e3ecbec864.png?version=1&amp;amp;modificationDate=1226345368000" width="540" /&gt;&lt;/SPAN&gt;&lt;BR /&gt;Save and Close.&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;STRONG&gt;i.MX37&lt;/STRONG&gt;&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;After updating RVICE&amp;nbsp;to version 3.1 (needed to work with MX51), you'll need to add a new configuration as below to talk to MX37.&lt;BR /&gt;In order to connect to i.MX37 TO2 RVI updates are required.&amp;nbsp;&lt;A class="external-link" href="http://compass.freescale.net/go/179841424" rel="nofollow"&gt;http://compass.freescale.net/go/179841424&lt;/A&gt;&lt;BR class="atl-forced-newline" /&gt;Patches must be applied in this order:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;ARM-RVI-1.6.0-581-base.rvi&lt;/LI&gt;&lt;LI&gt;ARM_RVI-1.6.1-583-patch.rvi&lt;/LI&gt;&lt;LI&gt;Metrowerks-RVI-1.1.0-172-patch-MWZAS1.rvi&lt;/LI&gt;&lt;/OL&gt;&lt;UL&gt;&lt;LI&gt;Configure the scan chain with the following connections (TDI =&amp;gt;&amp;nbsp;ETMBUF =&amp;gt; ARM1176JZF-S =&amp;gt;&amp;nbsp;StarCORE140 =&amp;gt;&amp;nbsp;SDMA =&amp;gt; SJC)&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;&lt;UL&gt;&lt;LI&gt;Add Device=&amp;gt;ETMBUF&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;ARM1176JZF-S&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;StarCORE140&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;SDMA&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;SJC&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;SPAN class="image-wrap"&gt;&lt;IMG src="http://wiki.freescale.net/download/attachments/14260451/mx37-rvi-config.PNG?version=1&amp;amp;modificationDate=1246999898000" /&gt;&lt;/SPAN&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Save and Close.&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;i.MX31 and i.MX35&lt;/STRONG&gt;&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;You will also need to add a new configuration as below to talk to MX31.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Configure the scan chain with the following connections (TDI =&amp;gt; Unknown =&amp;gt; Unknown =&amp;gt; ARM1136JF-S =&amp;gt; ETMBUF)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;UL&gt;&lt;LI&gt;Add Device=&amp;gt;Custom Device=&amp;gt;UNKNOWN=&amp;gt;IR Length = 4&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Custom Device=&amp;gt;UNKNOWN=&amp;gt;IR Length = 5&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Registered Device=&amp;gt;ARM1136JF-S&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Registered Device=&amp;gt;ETMBUF (IR Length = 4)&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;SPAN class="image-wrap"&gt;&lt;IMG height="429" src="http://wiki.freescale.net/download/attachments/14260451/worddavfc2bd02e71758e283f9ce345ad42e11c.png?version=1&amp;amp;modificationDate=1226522490000" width="575" /&gt;&lt;/SPAN&gt;&lt;BR /&gt;Save and Close&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;STRONG&gt;i.MX25&lt;/STRONG&gt;&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;You will also need to add a new configuration as below to talk to MX25.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Configure the scan chain with the following connections (TDI =&amp;gt; Unknown =&amp;gt; Unknown =&amp;gt; ARM926EJ-S =&amp;gt; ETMBUF)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;UL&gt;&lt;LI&gt;Add Device=&amp;gt;Custom Device=&amp;gt;UNKNOWN=&amp;gt;IR Length = 5&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Custom Device=&amp;gt;UNKNOWN=&amp;gt;IR Length = 4&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Registered Device=&amp;gt; ARM926EJ-S&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Registered Device=&amp;gt;ETMBUF (IR Length = 4)&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;SPAN class="image-wrap"&gt;&lt;IMG height="410" src="http://wiki.freescale.net/download/attachments/14260451/worddava9385cf2aeaede0b9dec82787618359e.png?version=1&amp;amp;modificationDate=1226601778000" width="575" /&gt;&lt;/SPAN&gt;&lt;BR /&gt;Save and Close.&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;i.MX23 &amp;amp; i.MX28&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;For i.MX23, &amp;nbsp;uncheck the "Use Adaptive Clock if detected" option and set the JTAG Clock Speed to 400 KHz. &amp;nbsp;After that&amp;nbsp;you can use the Auto Configure Scan Chain option. &amp;nbsp;Only one TAP should show up which is the ARM926ej-s. &amp;nbsp;Now you can save this configuration for later use.&amp;nbsp;&lt;SPAN class="image-wrap"&gt;&lt;IMG src="http://wiki.freescale.net/download/attachments/14260451/i.MX23+RVIconfig.JPG?version=1&amp;amp;modificationDate=1267716735000" /&gt;&lt;/SPAN&gt;&lt;BR class="atl-forced-newline" /&gt;You should now be able to connect to i.MX53, i.MX51, i.MX37, i.MX31, i.MX28, i.MX25, and i.MX23.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2011 19:00:23 GMT</pubDate>
    <dc:creator>J_Eastlack</dc:creator>
    <dc:date>2011-06-15T19:00:23Z</dc:date>
    <item>
      <title>JTAG Debugging - Connecting to i.MX53, i.MX51 TO2, i.MX37, i.MX31, and i.MX25 using RVDS 3.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/JTAG-Debugging-Connecting-to-i-MX53-i-MX51-TO2-i-MX37-i-MX31-and/m-p/157871#M2662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Connecting to i.MX53, i.MX51 TO2, i.MX37, i.MX31 and i.MX25&amp;nbsp;using RVDS 3.1&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;STRONG&gt;RVI update:&lt;/STRONG&gt;&lt;BR /&gt;In order to connect to i.MX51 TO2 RVI updates are required.&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;Patches must be applied in this order:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;ARM-RVI-3.1.0-754-base.rvi&lt;/LI&gt;&lt;LI&gt;ARM_RVI-3.1.3-776-patch.rvi&lt;/LI&gt;&lt;LI&gt;ARM-RVI-3.2.0-850-base.rvi&lt;/LI&gt;&lt;LI&gt;ARM-RVI-3.2.6-875-Engineer-patch.rvi&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Note - Check ARM's website for patches&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR class="atl-forced-newline" /&gt;Note: after the update ETMBUF is not listed as a registered option. Use an unregistered device of IR length 4 in place of ETMBUF.&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;i.MX53&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Same as i.MX51 TO2 except Coresight base address is 0xC0008000&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN style="color: #000000; "&gt;&lt;STRONG&gt;i.MX50&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Same as i.MX53 -&amp;gt; Coresight base address is 0xC0008000&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;i.MX51 TO2&lt;/STRONG&gt;&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Connect RVICE to MX51 board using short JTAG parallel cable.&amp;nbsp; LVDS probe cannot be used.&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;Configure the scan chain with the following connections (TDI =&amp;gt; Unknown =&amp;gt; Unknown =&amp;gt; ARMCS-DP =&amp;gt; Cortex-A8)&lt;UL&gt;&lt;LI&gt;Add Device=&amp;gt;Custom Device=&amp;gt;UNKNOWN=&amp;gt;IR Length = 5&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Custom Device=&amp;gt;UNKNOWN=&amp;gt;IR Length = 4&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Registered Device=&amp;gt;CoreSight=&amp;gt;ARMCS-DP&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Registered Device=&amp;gt;Cortex=&amp;gt;Cortex-A8&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;Update the CoreSight base address as follows:&lt;UL&gt;&lt;LI&gt;Right Click on Cortex-A8 Device&lt;/LI&gt;&lt;LI&gt;Select Configuration&lt;/LI&gt;&lt;LI&gt;Set CoreSight base address = 0xE0008000&lt;/LI&gt;&lt;LI&gt;Save the configuration&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN class="image-wrap"&gt;&lt;IMG height="427" src="http://wiki.freescale.net/download/attachments/14260451/worddavc1f53298886db4ea194c98e3ecbec864.png?version=1&amp;amp;modificationDate=1226345368000" width="540" /&gt;&lt;/SPAN&gt;&lt;BR /&gt;Save and Close.&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;STRONG&gt;i.MX37&lt;/STRONG&gt;&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;After updating RVICE&amp;nbsp;to version 3.1 (needed to work with MX51), you'll need to add a new configuration as below to talk to MX37.&lt;BR /&gt;In order to connect to i.MX37 TO2 RVI updates are required.&amp;nbsp;&lt;A class="external-link" href="http://compass.freescale.net/go/179841424" rel="nofollow"&gt;http://compass.freescale.net/go/179841424&lt;/A&gt;&lt;BR class="atl-forced-newline" /&gt;Patches must be applied in this order:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;ARM-RVI-1.6.0-581-base.rvi&lt;/LI&gt;&lt;LI&gt;ARM_RVI-1.6.1-583-patch.rvi&lt;/LI&gt;&lt;LI&gt;Metrowerks-RVI-1.1.0-172-patch-MWZAS1.rvi&lt;/LI&gt;&lt;/OL&gt;&lt;UL&gt;&lt;LI&gt;Configure the scan chain with the following connections (TDI =&amp;gt;&amp;nbsp;ETMBUF =&amp;gt; ARM1176JZF-S =&amp;gt;&amp;nbsp;StarCORE140 =&amp;gt;&amp;nbsp;SDMA =&amp;gt; SJC)&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;&lt;UL&gt;&lt;LI&gt;Add Device=&amp;gt;ETMBUF&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;ARM1176JZF-S&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;StarCORE140&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;SDMA&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;SJC&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;SPAN class="image-wrap"&gt;&lt;IMG src="http://wiki.freescale.net/download/attachments/14260451/mx37-rvi-config.PNG?version=1&amp;amp;modificationDate=1246999898000" /&gt;&lt;/SPAN&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Save and Close.&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;i.MX31 and i.MX35&lt;/STRONG&gt;&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;You will also need to add a new configuration as below to talk to MX31.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Configure the scan chain with the following connections (TDI =&amp;gt; Unknown =&amp;gt; Unknown =&amp;gt; ARM1136JF-S =&amp;gt; ETMBUF)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;UL&gt;&lt;LI&gt;Add Device=&amp;gt;Custom Device=&amp;gt;UNKNOWN=&amp;gt;IR Length = 4&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Custom Device=&amp;gt;UNKNOWN=&amp;gt;IR Length = 5&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Registered Device=&amp;gt;ARM1136JF-S&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Registered Device=&amp;gt;ETMBUF (IR Length = 4)&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;SPAN class="image-wrap"&gt;&lt;IMG height="429" src="http://wiki.freescale.net/download/attachments/14260451/worddavfc2bd02e71758e283f9ce345ad42e11c.png?version=1&amp;amp;modificationDate=1226522490000" width="575" /&gt;&lt;/SPAN&gt;&lt;BR /&gt;Save and Close&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;STRONG&gt;i.MX25&lt;/STRONG&gt;&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;You will also need to add a new configuration as below to talk to MX25.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Configure the scan chain with the following connections (TDI =&amp;gt; Unknown =&amp;gt; Unknown =&amp;gt; ARM926EJ-S =&amp;gt; ETMBUF)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;UL&gt;&lt;LI&gt;Add Device=&amp;gt;Custom Device=&amp;gt;UNKNOWN=&amp;gt;IR Length = 5&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Custom Device=&amp;gt;UNKNOWN=&amp;gt;IR Length = 4&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Registered Device=&amp;gt; ARM926EJ-S&lt;/LI&gt;&lt;LI&gt;Add Device=&amp;gt;Registered Device=&amp;gt;ETMBUF (IR Length = 4)&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR class="atl-forced-newline" /&gt;&lt;SPAN class="image-wrap"&gt;&lt;IMG height="410" src="http://wiki.freescale.net/download/attachments/14260451/worddava9385cf2aeaede0b9dec82787618359e.png?version=1&amp;amp;modificationDate=1226601778000" width="575" /&gt;&lt;/SPAN&gt;&lt;BR /&gt;Save and Close.&amp;nbsp;&lt;BR class="atl-forced-newline" /&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;i.MX23 &amp;amp; i.MX28&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;For i.MX23, &amp;nbsp;uncheck the "Use Adaptive Clock if detected" option and set the JTAG Clock Speed to 400 KHz. &amp;nbsp;After that&amp;nbsp;you can use the Auto Configure Scan Chain option. &amp;nbsp;Only one TAP should show up which is the ARM926ej-s. &amp;nbsp;Now you can save this configuration for later use.&amp;nbsp;&lt;SPAN class="image-wrap"&gt;&lt;IMG src="http://wiki.freescale.net/download/attachments/14260451/i.MX23+RVIconfig.JPG?version=1&amp;amp;modificationDate=1267716735000" /&gt;&lt;/SPAN&gt;&lt;BR class="atl-forced-newline" /&gt;You should now be able to connect to i.MX53, i.MX51, i.MX37, i.MX31, i.MX28, i.MX25, and i.MX23.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2011 19:00:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/JTAG-Debugging-Connecting-to-i-MX53-i-MX51-TO2-i-MX37-i-MX31-and/m-p/157871#M2662</guid>
      <dc:creator>J_Eastlack</dc:creator>
      <dc:date>2011-06-15T19:00:23Z</dc:date>
    </item>
  </channel>
</rss>