<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMx53 I2C slave patch</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Mx53-I2C-slave-patch/m-p/262477#M26590</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hardware connection&lt;/P&gt;&lt;P&gt;In mx53 SMD, connect R85 to R138, connect R86 to R139.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;mx53_i2c_slave.patch is the patch to support I2C slave in Mx53 SMD, it can be applied to R10.3.2 and 1109.&lt;/P&gt;&lt;P&gt;I2C2 is master, I2C3 is slave.&lt;/P&gt;&lt;P&gt;In menuconfig, select Device Drivers&amp;nbsp; ---&amp;gt; [*] I2C Slave support&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;mxc_i2c_slave_test.c is the test code, it can be built by below command&lt;/P&gt;&lt;P&gt;/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-none-linux-gnueabi-gcc -lpthread mxc_i2c_slave_test.c -o mxc_i2c_slave_test&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the test fail, please check if I2C2_SCL, I2C2_SDA, I2C3_SCL, I2C3_SDA are pulled up to 3.3V, they may be pulled down by the original I2C3 slave device in the board.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336378"&gt;mx53_i2c_slave.patch.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336378"&gt;mxc_i2c_slave_test.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Jul 2013 02:29:24 GMT</pubDate>
    <dc:creator>shaojun_wang</dc:creator>
    <dc:date>2013-07-10T02:29:24Z</dc:date>
    <item>
      <title>Mx53 I2C slave patch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mx53-I2C-slave-patch/m-p/262477#M26590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hardware connection&lt;/P&gt;&lt;P&gt;In mx53 SMD, connect R85 to R138, connect R86 to R139.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;mx53_i2c_slave.patch is the patch to support I2C slave in Mx53 SMD, it can be applied to R10.3.2 and 1109.&lt;/P&gt;&lt;P&gt;I2C2 is master, I2C3 is slave.&lt;/P&gt;&lt;P&gt;In menuconfig, select Device Drivers&amp;nbsp; ---&amp;gt; [*] I2C Slave support&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;mxc_i2c_slave_test.c is the test code, it can be built by below command&lt;/P&gt;&lt;P&gt;/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-none-linux-gnueabi-gcc -lpthread mxc_i2c_slave_test.c -o mxc_i2c_slave_test&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the test fail, please check if I2C2_SCL, I2C2_SDA, I2C3_SCL, I2C3_SDA are pulled up to 3.3V, they may be pulled down by the original I2C3 slave device in the board.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336378"&gt;mx53_i2c_slave.patch.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336378"&gt;mxc_i2c_slave_test.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jul 2013 02:29:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mx53-I2C-slave-patch/m-p/262477#M26590</guid>
      <dc:creator>shaojun_wang</dc:creator>
      <dc:date>2013-07-10T02:29:24Z</dc:date>
    </item>
  </channel>
</rss>