<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6 SDMA Function in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SDMA-Function/m-p/261977#M26392</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Koichi-san,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you asking&lt;/P&gt;&lt;P&gt;(1) Does SDMA support scatter/gather function?&lt;/P&gt;&lt;P&gt;(2) Does SDMA support transfer biween memory and SDIO?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If (1) is the case, Assuming the "scatter/gather" means &lt;/P&gt;&lt;P&gt;similar function in eDMA, SDMA seems to have superior function(s).&lt;/P&gt;&lt;P&gt;Please refer to the chapter of SDMA in RM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If (2) is the case, most probably the answer is yes,&lt;/P&gt;&lt;P&gt;but I think that you need to describe what you'd like to&lt;/P&gt;&lt;P&gt;accomplish more specifically to get appropriate answer(s).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;4-Feb-2014&lt;/P&gt;&lt;P&gt;Motoo Tanaka&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Feb 2014 07:10:05 GMT</pubDate>
    <dc:creator>Rhyme</dc:creator>
    <dc:date>2014-02-04T07:10:05Z</dc:date>
    <item>
      <title>iMX6 SDMA Function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SDMA-Function/m-p/261976#M26391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sirs,&lt;BR /&gt;I would like to use the scatter/gather function between SDIO and memorys.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does iMX6 SDMA support&amp;nbsp; scatter/gather function between SDIO and memorys ?&lt;BR /&gt;Or ,do I have to use the internal DMA ( in uSDHC module) ?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;If Yes, does the Linux BSP support above function ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Koichi Sakagami&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2014 10:21:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SDMA-Function/m-p/261976#M26391</guid>
      <dc:creator>koichisakagami</dc:creator>
      <dc:date>2014-01-28T10:21:36Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 SDMA Function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SDMA-Function/m-p/261977#M26392</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Koichi-san,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you asking&lt;/P&gt;&lt;P&gt;(1) Does SDMA support scatter/gather function?&lt;/P&gt;&lt;P&gt;(2) Does SDMA support transfer biween memory and SDIO?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If (1) is the case, Assuming the "scatter/gather" means &lt;/P&gt;&lt;P&gt;similar function in eDMA, SDMA seems to have superior function(s).&lt;/P&gt;&lt;P&gt;Please refer to the chapter of SDMA in RM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If (2) is the case, most probably the answer is yes,&lt;/P&gt;&lt;P&gt;but I think that you need to describe what you'd like to&lt;/P&gt;&lt;P&gt;accomplish more specifically to get appropriate answer(s).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;4-Feb-2014&lt;/P&gt;&lt;P&gt;Motoo Tanaka&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Feb 2014 07:10:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SDMA-Function/m-p/261977#M26392</guid>
      <dc:creator>Rhyme</dc:creator>
      <dc:date>2014-02-04T07:10:05Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 SDMA Function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SDMA-Function/m-p/261978#M26393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Tanaka-san,&lt;/P&gt;&lt;P&gt;Thank you for reply.&lt;/P&gt;&lt;P&gt;It is (2) that I would like to ask.&lt;/P&gt;&lt;P&gt;I understood. I post the questions more specifically.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Koichi sakagami&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Feb 2014 00:09:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SDMA-Function/m-p/261978#M26393</guid>
      <dc:creator>koichisakagami</dc:creator>
      <dc:date>2014-02-05T00:09:12Z</dc:date>
    </item>
  </channel>
</rss>