<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Unable to handle kernel paging request at virtual address</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-handle-kernel-paging-request-at-virtual-address/m-p/261860#M26344</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is like that it is about the temperature after let the IMX6Q cool this problem like have solved . : )&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Jul 2013 02:11:54 GMT</pubDate>
    <dc:creator>steven1758</dc:creator>
    <dc:date>2013-07-31T02:11:54Z</dc:date>
    <item>
      <title>Unable to handle kernel paging request at virtual address</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-handle-kernel-paging-request-at-virtual-address/m-p/261859#M26343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am using the imx-android-13.4.1 code. after burn to my board ,It will suddenly &lt;/P&gt;&lt;P&gt;give the Unable to handle kernel paging request at virtual address error then crash. :&amp;nbsp; (&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the information:&lt;/P&gt;&lt;P&gt;active wake lock PowerManagerService&lt;/P&gt;&lt;P&gt;request_suspend_state: wakeup (3-&amp;gt;0) at 178405733691 (2013-07-09 10:09:59.364397999 UTC)&lt;/P&gt;&lt;P&gt;PHY: 1:05 - Link is Up - 1000/Full&lt;/P&gt;&lt;P&gt;mmc0: Starting deferred resume&lt;/P&gt;&lt;P&gt;mmc0: Deferred resume completed&lt;/P&gt;&lt;P&gt;Unable to handle kernel paging request at virtual address 9fed28f0&lt;/P&gt;&lt;P&gt;pgd = c0004000&lt;/P&gt;&lt;P&gt;[9fed28f0] *pgd=00000000&lt;/P&gt;&lt;P&gt;Internal error: Oops: 805 [#1] PREEMPT SMP&lt;/P&gt;&lt;P&gt;Modules linked in:&lt;/P&gt;&lt;P&gt;CPU: 1&amp;nbsp;&amp;nbsp;&amp;nbsp; Not tainted&amp;nbsp; (3.0.35-05524-g8513494-dirty #5)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice will be appreciate .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jul 2013 10:35:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-handle-kernel-paging-request-at-virtual-address/m-p/261859#M26343</guid>
      <dc:creator>steven1758</dc:creator>
      <dc:date>2013-07-09T10:35:02Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to handle kernel paging request at virtual address</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-handle-kernel-paging-request-at-virtual-address/m-p/261860#M26344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is like that it is about the temperature after let the IMX6Q cool this problem like have solved . : )&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jul 2013 02:11:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-handle-kernel-paging-request-at-virtual-address/m-p/261860#M26344</guid>
      <dc:creator>steven1758</dc:creator>
      <dc:date>2013-07-31T02:11:54Z</dc:date>
    </item>
  </channel>
</rss>