<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Clone display without using LVDS in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Clone-display-without-using-LVDS/m-p/261656#M26295</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the following setting for bootargs has lvds0 with fb0 and hdmi with fb2.&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666' video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24'&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then you can output the same content into fb2 &amp;amp; fb0, and both displays can show the same content.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Feb 2014 07:15:14 GMT</pubDate>
    <dc:creator>max_tsai</dc:creator>
    <dc:date>2014-02-21T07:15:14Z</dc:date>
    <item>
      <title>Clone display without using LVDS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Clone-display-without-using-LVDS/m-p/261655#M26294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I heard&amp;nbsp; LinuxBSP for iMX6QSDB didn't support clone display (except LDVS0&amp;amp;1).&lt;/P&gt;&lt;P&gt;However I would like to display primary fb on both hdmi and lcd.&lt;/P&gt;&lt;P&gt;Is it possible? If yes, how can I configure video bootargs of uboot?&lt;/P&gt;&lt;P&gt;If it is difficult, which source file need to modify?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2014 10:24:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Clone-display-without-using-LVDS/m-p/261655#M26294</guid>
      <dc:creator>torus1000</dc:creator>
      <dc:date>2014-01-28T10:24:55Z</dc:date>
    </item>
    <item>
      <title>Re: Clone display without using LVDS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Clone-display-without-using-LVDS/m-p/261656#M26295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the following setting for bootargs has lvds0 with fb0 and hdmi with fb2.&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666' video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24'&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then you can output the same content into fb2 &amp;amp; fb0, and both displays can show the same content.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Feb 2014 07:15:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Clone-display-without-using-LVDS/m-p/261656#M26295</guid>
      <dc:creator>max_tsai</dc:creator>
      <dc:date>2014-02-21T07:15:14Z</dc:date>
    </item>
  </channel>
</rss>