<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MX53 CSI/IDMAC config for Aptina 12-bit grayscale camera?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX53-CSI-IDMAC-config-for-Aptina-12-bit-grayscale-camera/m-p/261557#M26276</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think you also need set BPP to 16 bits per pixel in CPMEM. &lt;BR /&gt;For generic mode, when you set 16 bits data width in CSI, it will capture 16 bits each clock. And when use CPMEM to save them to memory, with your setting, 12 bits will be saved each time, but the captured data has 4 bits unused data, it will also be saved to memory, so there will be 4 bits shift.&lt;BR /&gt;And if you wants to save the 12 bits gray data to memory bits[0~11], I think you should connect the data pins to CSI_DATA15 ~ CSI_DATA4. &lt;BR /&gt;Otherwize, when convert from 16bits to 12bits, LSB will be dropped, so the 12 bits data will always kept in memory bits[4-15].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Jun 2013 03:28:11 GMT</pubDate>
    <dc:creator>qiang_li-mpu_se</dc:creator>
    <dc:date>2013-06-03T03:28:11Z</dc:date>
    <item>
      <title>MX53 CSI/IDMAC config for Aptina 12-bit grayscale camera?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX53-CSI-IDMAC-config-for-Aptina-12-bit-grayscale-camera/m-p/261556#M26275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm having a problem configuring the MX53 CSI/IDMAC properly for a 12-bit Aptina camera - the data values are showing up in memory in bits 4-15 rather than 0-11. Here's the scenario:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MT9P031M 12-bit mono camera&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; parallel data connected to data 8-19&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CSI0_SENS_CONF:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; protocol: gated&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; format: generic&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; data width: 16 bits&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; data dest: IDMAC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPMEM (interleaved):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BPP: 3 (12 bits per pixel)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NPB: 31&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PFS: 6 (generic data)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Compander is disabled&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I put the camera into test mode, generating a walking 1's pattern.&lt;/P&gt;&lt;P&gt;Here are the data values that are put in memory, which are shifted left by 4 bits:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0020&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0040&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0080&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0100&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0200&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0400&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0800&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 8000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0010&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0020&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's my understanding that I should be able to have 12-bit camera data show up in the lower 12 bits of memory - what additional/different settings are needed to do that...?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;--Ed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2013 21:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX53-CSI-IDMAC-config-for-Aptina-12-bit-grayscale-camera/m-p/261556#M26275</guid>
      <dc:creator>EdMenard</dc:creator>
      <dc:date>2013-05-28T21:33:45Z</dc:date>
    </item>
    <item>
      <title>Re: MX53 CSI/IDMAC config for Aptina 12-bit grayscale camera?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX53-CSI-IDMAC-config-for-Aptina-12-bit-grayscale-camera/m-p/261557#M26276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think you also need set BPP to 16 bits per pixel in CPMEM. &lt;BR /&gt;For generic mode, when you set 16 bits data width in CSI, it will capture 16 bits each clock. And when use CPMEM to save them to memory, with your setting, 12 bits will be saved each time, but the captured data has 4 bits unused data, it will also be saved to memory, so there will be 4 bits shift.&lt;BR /&gt;And if you wants to save the 12 bits gray data to memory bits[0~11], I think you should connect the data pins to CSI_DATA15 ~ CSI_DATA4. &lt;BR /&gt;Otherwize, when convert from 16bits to 12bits, LSB will be dropped, so the 12 bits data will always kept in memory bits[4-15].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Jun 2013 03:28:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX53-CSI-IDMAC-config-for-Aptina-12-bit-grayscale-camera/m-p/261557#M26276</guid>
      <dc:creator>qiang_li-mpu_se</dc:creator>
      <dc:date>2013-06-03T03:28:11Z</dc:date>
    </item>
    <item>
      <title>Re: MX53 CSI/IDMAC config for Aptina 12-bit grayscale camera?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX53-CSI-IDMAC-config-for-Aptina-12-bit-grayscale-camera/m-p/261558#M26277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks - that's the conclusion we reached as well.&lt;/P&gt;&lt;P&gt;For now we are shifting the bits down in software - next rev of the hardware we'll connect as you suggest.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Jun 2013 16:00:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX53-CSI-IDMAC-config-for-Aptina-12-bit-grayscale-camera/m-p/261558#M26277</guid>
      <dc:creator>EdMenard</dc:creator>
      <dc:date>2013-06-03T16:00:34Z</dc:date>
    </item>
  </channel>
</rss>