<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6 MfgTool not loading u-boot.bin as expected in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-MfgTool-not-loading-u-boot-bin-as-expected/m-p/260957#M26088</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm sorry for the delayed followup.&amp;nbsp; No, I never managed to get the USB loader to load the FPGA bitfile the way I was trying to do it, but found another way.&amp;nbsp; I simple added another line to the XML config file, and loaded the file to a different address in memory, and from there I was able to do what was needed.&amp;nbsp; Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 May 2013 18:18:12 GMT</pubDate>
    <dc:creator>jamese</dc:creator>
    <dc:date>2013-05-01T18:18:12Z</dc:date>
    <item>
      <title>IMX6 MfgTool not loading u-boot.bin as expected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-MfgTool-not-loading-u-boot-bin-as-expected/m-p/260954#M26085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the MfgTool to load a custom u-boot to our board over USB.&amp;nbsp; The u-boot is basically the one from the SDK, and has the HAB stuff added to it.&amp;nbsp; I had to make the linker changes, and the system seems to work well on the SabreSD eval board, though that was loaded off of an SD card.&amp;nbsp; In the case of the new board, the MfgTool loads the u-boot.bin, but sometime after the main u-boot code, somewhere in the padding that follows, it cuts off the download, so everything after the padding is lost.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a trick to get the MfgTool to load the entire image?&amp;nbsp; The documentation I've found is very light on what it's doing.&amp;nbsp; I'm assuming that the tool is determining the size of the image to load based on something other than file size, but can't find what that is.&amp;nbsp; Any help is appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Apr 2013 19:15:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-MfgTool-not-loading-u-boot-bin-as-expected/m-p/260954#M26085</guid>
      <dc:creator>jamese</dc:creator>
      <dc:date>2013-04-10T19:15:50Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 MfgTool not loading u-boot.bin as expected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-MfgTool-not-loading-u-boot-bin-as-expected/m-p/260955#M26086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,James,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I need more details about your projects ,Could you tell me following :&lt;/P&gt;&lt;P&gt;(1)Which CPU you are using ?&lt;/P&gt;&lt;P&gt;(2)which uSDHC port ?&lt;/P&gt;&lt;P&gt;(3)Can you paste the ucl2.xml file here?&lt;/P&gt;&lt;P&gt;Let me see burning list for your board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Apr 2013 03:08:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-MfgTool-not-loading-u-boot-bin-as-expected/m-p/260955#M26086</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2013-04-16T03:08:19Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 MfgTool not loading u-boot.bin as expected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-MfgTool-not-loading-u-boot-bin-as-expected/m-p/260956#M26087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,James,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Did you resolve your issue ?&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 21 Apr 2013 05:57:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-MfgTool-not-loading-u-boot-bin-as-expected/m-p/260956#M26087</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2013-04-21T05:57:56Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 MfgTool not loading u-boot.bin as expected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-MfgTool-not-loading-u-boot-bin-as-expected/m-p/260957#M26088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm sorry for the delayed followup.&amp;nbsp; No, I never managed to get the USB loader to load the FPGA bitfile the way I was trying to do it, but found another way.&amp;nbsp; I simple added another line to the XML config file, and loaded the file to a different address in memory, and from there I was able to do what was needed.&amp;nbsp; Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 May 2013 18:18:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-MfgTool-not-loading-u-boot-bin-as-expected/m-p/260957#M26088</guid>
      <dc:creator>jamese</dc:creator>
      <dc:date>2013-05-01T18:18:12Z</dc:date>
    </item>
  </channel>
</rss>