<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Looking for a Bare metal executable code for iMX6 using DS-5 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-Bare-metal-executable-code-for-iMX6-using-DS-5/m-p/260679#M26000</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Singh&lt;/P&gt;&lt;P&gt;Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel &lt;/P&gt;&lt;P&gt;free to contact Freescale.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Feb 2014 06:06:16 GMT</pubDate>
    <dc:creator>YixingKong</dc:creator>
    <dc:date>2014-02-18T06:06:16Z</dc:date>
    <item>
      <title>Looking for a Bare metal executable code for iMX6 using DS-5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-Bare-metal-executable-code-for-iMX6-using-DS-5/m-p/260675#M25996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am looking for a bare metal example code for a iMX6Q Sbare lite version board to be used using DS-5. I tried using a RTSM start up codes to initialize the startup.s file for this board, and tried to map the memory in the scatter file , but on building the code crashes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So if you can provide me the initial framework for this, using which i can create my codes, that would be really helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would also like to get a Lauterbach script for same board as well, using which i can simply load the .axf file generated using DS-5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know the needful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Harshit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2013 10:05:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-Bare-metal-executable-code-for-iMX6-using-DS-5/m-p/260675#M25996</guid>
      <dc:creator>harshitsingh</dc:creator>
      <dc:date>2013-05-28T10:05:36Z</dc:date>
    </item>
    <item>
      <title>Re: Looking for a Bare metal executable code for iMX6 using DS-5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-Bare-metal-executable-code-for-iMX6-using-DS-5/m-p/260676#M25997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is a &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6SL&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;Platform SDK&lt;/A&gt; that should provide you the information you are requesting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The tools folder has the Lauterbach scripts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT: It's under the Snippets, Boot Code, .. Tab&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Brett&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2013 13:40:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-Bare-metal-executable-code-for-iMX6-using-DS-5/m-p/260676#M25997</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2013-05-28T13:40:24Z</dc:date>
    </item>
    <item>
      <title>Re: Looking for a Bare metal executable code for iMX6 using DS-5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-Bare-metal-executable-code-for-iMX6-using-DS-5/m-p/260677#M25998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have already gone through this. And it did not helped much as DS-5 folder inside this mainly comprises of the debugger script for accessing the DDR3 memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. I am looking for something which will do the initialization using 'startup.s' file just like we have in the code attached for RTSM Coretile express Cortex-A9, attached along with this thread.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So if you can provide similar kind of code that would suffice my requirement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Also for Lauterbach, i want the .cmm style script for this board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. The SDK Platform is not helping much. Can you provide us the guidelines how to use this files present in the SDK platform to run Using DS-5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly let me know the needful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Harshit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 May 2013 05:01:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-Bare-metal-executable-code-for-iMX6-using-DS-5/m-p/260677#M25998</guid>
      <dc:creator>harshitsingh</dc:creator>
      <dc:date>2013-05-29T05:01:48Z</dc:date>
    </item>
    <item>
      <title>Re: Looking for a Bare metal executable code for iMX6 using DS-5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-Bare-metal-executable-code-for-iMX6-using-DS-5/m-p/260678#M25999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got the lauterbach script (.cmm) file, which i run it before i load a code '.axf' file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But whenever i do that i get an error like 'bus error generated by cpu'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please find the attached code which was build using DS-5 and debugged using Lauterbach.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I request you to kindly let me know is there any initialization problem in the code or something else which i am missing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly let me know your feedback regarding this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Harshit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 May 2013 11:16:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-Bare-metal-executable-code-for-iMX6-using-DS-5/m-p/260678#M25999</guid>
      <dc:creator>harshitsingh</dc:creator>
      <dc:date>2013-05-29T11:16:37Z</dc:date>
    </item>
    <item>
      <title>Re: Looking for a Bare metal executable code for iMX6 using DS-5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-Bare-metal-executable-code-for-iMX6-using-DS-5/m-p/260679#M26000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Singh&lt;/P&gt;&lt;P&gt;Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel &lt;/P&gt;&lt;P&gt;free to contact Freescale.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2014 06:06:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-Bare-metal-executable-code-for-iMX6-using-DS-5/m-p/260679#M26000</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-18T06:06:16Z</dc:date>
    </item>
    <item>
      <title>Re: Looking for a Bare metal executable code for iMX6 using DS-5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-Bare-metal-executable-code-for-iMX6-using-DS-5/m-p/260680#M26001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Singh&lt;/P&gt;&lt;P&gt;This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this &lt;/P&gt;&lt;P&gt;discussion, or create another discussion.&lt;BR /&gt;Thanks,&lt;BR /&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Feb 2014 06:19:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-Bare-metal-executable-code-for-iMX6-using-DS-5/m-p/260680#M26001</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-25T06:19:43Z</dc:date>
    </item>
  </channel>
</rss>