<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: u-boot NFS problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-NFS-problem/m-p/260624#M25981</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tested the device on another PC where it previously worked, and NFS is still working. So u-boot configuration is ok; the problem is in TFTP/NFS configuration on PC side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;MIX&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Dec 2013 11:05:06 GMT</pubDate>
    <dc:creator>il_mix</dc:creator>
    <dc:date>2013-12-18T11:05:06Z</dc:date>
    <item>
      <title>u-boot NFS problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-NFS-problem/m-p/260622#M25979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a SABRE IMX6Q, that was correctly working with NFS.&lt;/P&gt;&lt;P&gt;Now I messed up the u-boot parameters, and I'm not able to let it work again.&lt;/P&gt;&lt;P&gt;Here is the output of the 'pr' command in u-boot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;baudrate=115200&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;boot_fdt=try&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bootargs=console=ttymxc0,115200 root=/dev/nfs ip=10.0.10.216:10.0.10.108:10.0.10&lt;/EM&gt;&lt;EM&gt;.1:255.255.255.0:sabresd:eth0:off:nfsroot=${serverip}:{nfsroot},v3,tcp&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bootcmd=mmc dev ${mmcdev};if mmc rescan; then if run loadbootscript; then run bo&lt;/EM&gt;&lt;EM&gt;otscript; else if run loaduimage; then run mmcboot; else run netboot; fi; fi; el&lt;/EM&gt;&lt;EM&gt;se run netboot; fi&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bootdelay=1&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bootfile=uImage&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bootscript=echo Running bootscript from mmc ...; source&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;console=ttymxc0&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;ethact=FEC&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;ethaddr=00:04:9f:02:b2:f0&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;ethprime=FEC&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;fdt_addr=0x11000000&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;fdt_file=imx6q-sabresd.dtb&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;fdt_high=0xffffffff&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;get_cmd=tftp&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;initrd_high=0xffffffff&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;ip_dyn=no&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;ipaddr=10.0.10.216&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;loadaddr=0x12000000&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;loaduimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${uimage}&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot}&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || tes&lt;/EM&gt;&lt;EM&gt;t ${boot_fdt} = try; then if run loadfdt; then bootm ${loadaddr} - ${fdt_addr}; &lt;/EM&gt;&lt;EM&gt;else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; &lt;/EM&gt;&lt;EM&gt;fi; fi; else bootm; fi;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;mmcdev=1&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;mmcpart=1&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;mmcroot=/dev/mmcblk1p2 rootwait rw&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;netargs=${bootargs}&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then se&lt;/EM&gt;&lt;EM&gt;tenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${uimage}; if test $&lt;/EM&gt;&lt;EM&gt;{boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt&lt;/EM&gt;&lt;EM&gt;_file}; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; th&lt;/EM&gt;&lt;EM&gt;en bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;nfsroot=/home/cristofolini/tftp&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;script=boot.scr&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;serverip=10.0.10.108&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;uimage=uImage&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;update_sd_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else seten&lt;/EM&gt;&lt;EM&gt;v get_cmd tftp; fi; if mmc dev ${mmcdev}; then if ${get_cmd} ${update_sd_firmwar&lt;/EM&gt;&lt;EM&gt;e_filename}; then setexpr fw_sz ${filesize} / 0x200; setexpr fw_sz ${fw_sz} + 1;&lt;/EM&gt;&lt;EM&gt; mmc write ${loadaddr} 0x2 ${fw_sz}; fi; fi&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Environment size: 2098/8188 bytes &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uBoot isn't able to locate uImage.&lt;/P&gt;&lt;P&gt;uImage is copied in my tftp directory, the one listed in /etc/default/atftpd.&lt;/P&gt;&lt;P&gt;Then, the fyle system is in nfsroot=/home/cristofolini/tftp, and the directory is exported in /etc/exports&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I missing something?&lt;/P&gt;&lt;P&gt;Thanks for the support!&lt;/P&gt;&lt;P&gt;MIX&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Dec 2013 12:12:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-NFS-problem/m-p/260622#M25979</guid>
      <dc:creator>il_mix</dc:creator>
      <dc:date>2013-12-13T12:12:04Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot NFS problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-NFS-problem/m-p/260623#M25980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Massimo,&lt;/P&gt;&lt;P&gt;Would you please try copy the uImage to your /home/cristofolini/tftp directory, as you have set nfsroot=/home/cristofolini/tftp .&lt;/P&gt;&lt;P&gt;Hope this can help you ~~&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Dec 2013 02:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-NFS-problem/m-p/260623#M25980</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2013-12-18T02:20:04Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot NFS problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-NFS-problem/m-p/260624#M25981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tested the device on another PC where it previously worked, and NFS is still working. So u-boot configuration is ok; the problem is in TFTP/NFS configuration on PC side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;MIX&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Dec 2013 11:05:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-NFS-problem/m-p/260624#M25981</guid>
      <dc:creator>il_mix</dc:creator>
      <dc:date>2013-12-18T11:05:06Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot NFS problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-NFS-problem/m-p/260625#M25982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Massimo,&lt;/P&gt;&lt;P&gt;My pleasure:smileyhappy:.&amp;nbsp; The TFTP/NFS configuration you can reference the document "Setting_Up_LTIB_host.pdf". Any questions contract with me easily~~&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2013 02:03:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-NFS-problem/m-p/260625#M25982</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2013-12-19T02:03:33Z</dc:date>
    </item>
  </channel>
</rss>