<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックdisplay_data lost on IMX53?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/display-data-lost-on-IMX53/m-p/260147#M25828</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are outputting as RGB24 on the displayport. &lt;/P&gt;&lt;P&gt;However, we see that some LSB's gets lost (actually, not really lost, but getting replaced some of the MSB's)&lt;/P&gt;&lt;P&gt;With walking 1's, it looks like (measured with the scope)&lt;/P&gt;&lt;P&gt;I'm using the linux 2.6.35 kernel from release 9.11 (git). Anyone has any clue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;R:&lt;/P&gt;&lt;P&gt;bit0 : 0x20 -&amp;gt; should be 0x01&lt;/P&gt;&lt;P&gt;bit1: 0x40 -&amp;gt; should be 0x02&lt;/P&gt;&lt;P&gt;bit2: 0x80 -&amp;gt; should be 0x04&lt;/P&gt;&lt;P&gt;bit3: 0x08&lt;/P&gt;&lt;P&gt;bit4: 0x10&lt;/P&gt;&lt;P&gt;bit5: 0x20&lt;/P&gt;&lt;P&gt;bit6: 0x40&lt;/P&gt;&lt;P&gt;bit7: 0x80&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;G:&lt;/P&gt;&lt;P&gt;bit0 : 0x40-&amp;gt; should be 0x01&lt;/P&gt;&lt;P&gt;bit1: 0x80 -&amp;gt; should be 0x02&lt;/P&gt;&lt;P&gt;bit2: 0x04&lt;/P&gt;&lt;P&gt;bit3: 0x08&lt;/P&gt;&lt;P&gt;bit4: 0x10&lt;/P&gt;&lt;P&gt;bit5: 0x20&lt;/P&gt;&lt;P&gt;bit6: 0x40&lt;/P&gt;&lt;P&gt;bit7: 0x80&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;B:&lt;/P&gt;&lt;P&gt;bit0 : 0x20 -&amp;gt; should be 0x01&lt;/P&gt;&lt;P&gt;bit1: 0x40 -&amp;gt; should be 0x02&lt;/P&gt;&lt;P&gt;bit2: 0x80 -&amp;gt; should be 0x04&lt;/P&gt;&lt;P&gt;bit3: 0x08&lt;/P&gt;&lt;P&gt;bit4: 0x10&lt;/P&gt;&lt;P&gt;bit5: 0x20&lt;/P&gt;&lt;P&gt;bit6: 0x40&lt;/P&gt;&lt;P&gt;bit7: 0x80&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Feb 2013 11:22:02 GMT</pubDate>
    <dc:creator>woutervh</dc:creator>
    <dc:date>2013-02-15T11:22:02Z</dc:date>
    <item>
      <title>display_data lost on IMX53?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/display-data-lost-on-IMX53/m-p/260147#M25828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are outputting as RGB24 on the displayport. &lt;/P&gt;&lt;P&gt;However, we see that some LSB's gets lost (actually, not really lost, but getting replaced some of the MSB's)&lt;/P&gt;&lt;P&gt;With walking 1's, it looks like (measured with the scope)&lt;/P&gt;&lt;P&gt;I'm using the linux 2.6.35 kernel from release 9.11 (git). Anyone has any clue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;R:&lt;/P&gt;&lt;P&gt;bit0 : 0x20 -&amp;gt; should be 0x01&lt;/P&gt;&lt;P&gt;bit1: 0x40 -&amp;gt; should be 0x02&lt;/P&gt;&lt;P&gt;bit2: 0x80 -&amp;gt; should be 0x04&lt;/P&gt;&lt;P&gt;bit3: 0x08&lt;/P&gt;&lt;P&gt;bit4: 0x10&lt;/P&gt;&lt;P&gt;bit5: 0x20&lt;/P&gt;&lt;P&gt;bit6: 0x40&lt;/P&gt;&lt;P&gt;bit7: 0x80&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;G:&lt;/P&gt;&lt;P&gt;bit0 : 0x40-&amp;gt; should be 0x01&lt;/P&gt;&lt;P&gt;bit1: 0x80 -&amp;gt; should be 0x02&lt;/P&gt;&lt;P&gt;bit2: 0x04&lt;/P&gt;&lt;P&gt;bit3: 0x08&lt;/P&gt;&lt;P&gt;bit4: 0x10&lt;/P&gt;&lt;P&gt;bit5: 0x20&lt;/P&gt;&lt;P&gt;bit6: 0x40&lt;/P&gt;&lt;P&gt;bit7: 0x80&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;B:&lt;/P&gt;&lt;P&gt;bit0 : 0x20 -&amp;gt; should be 0x01&lt;/P&gt;&lt;P&gt;bit1: 0x40 -&amp;gt; should be 0x02&lt;/P&gt;&lt;P&gt;bit2: 0x80 -&amp;gt; should be 0x04&lt;/P&gt;&lt;P&gt;bit3: 0x08&lt;/P&gt;&lt;P&gt;bit4: 0x10&lt;/P&gt;&lt;P&gt;bit5: 0x20&lt;/P&gt;&lt;P&gt;bit6: 0x40&lt;/P&gt;&lt;P&gt;bit7: 0x80&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 11:22:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/display-data-lost-on-IMX53/m-p/260147#M25828</guid>
      <dc:creator>woutervh</dc:creator>
      <dc:date>2013-02-15T11:22:02Z</dc:date>
    </item>
    <item>
      <title>Re: display_data lost on IMX53?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/display-data-lost-on-IMX53/m-p/260148#M25829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may try to configure framebuffer with 32bpp.&lt;/P&gt;&lt;P&gt;You can add 'bpp=32' appending video_mode of bootup command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can refer to "mx53_start_linux.book" as the below.&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;4. For each of the devices connected with DI, provide a specific video mode in bootup command line&lt;/P&gt;&lt;P&gt;in this format: video=mxcdixfb:DI_pixel_format,&lt;/P&gt;&lt;P&gt;video_mode,bpp=bits_per_pixel_of_frame_buffer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Feb 2013 03:15:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/display-data-lost-on-IMX53/m-p/260148#M25829</guid>
      <dc:creator>max_tsai</dc:creator>
      <dc:date>2013-02-25T03:15:57Z</dc:date>
    </item>
    <item>
      <title>Re: display_data lost on IMX53?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/display-data-lost-on-IMX53/m-p/260149#M25830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Feb 2013 13:07:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/display-data-lost-on-IMX53/m-p/260149#M25830</guid>
      <dc:creator>woutervh</dc:creator>
      <dc:date>2013-02-27T13:07:57Z</dc:date>
    </item>
  </channel>
</rss>